IADC_Init_t Struct Reference
IADC init structure, common for single conversion and scan sequence.
      
       #include <em_iadc.h>
      
     
| Data Fields | |
| bool | iadcClkSuspend0 | 
| Suspend IADC_CLK until PRS0 trigger. | |
| bool | iadcClkSuspend1 | 
| Suspend IADC_CLK until PRS1 trigger. | |
| bool | debugHalt | 
| Halt IADC during debug mode. | |
| IADC_Warmup_t | warmup | 
| IADC warmup mode. | |
| uint8_t | timebase | 
| IADC clock cycles (timebase+1) corresponding to 1us. | |
| uint8_t | srcClkPrescale | 
| User requested source clock divider (prescale+1) which will be used if the calculated prescaler value is less. | |
| uint16_t | timerCycles | 
| Number of ADC_CLK cycles per TIMER event. | |
| uint16_t | greaterThanEqualThres | 
| Digital window comparator greater-than or equal threshold. | |
| uint16_t | lessThanEqualThres | 
| Digital window comparator less-than or equal threshold. | |
IADC init structure, common for single conversion and scan sequence.
Field Documentation
◆ iadcClkSuspend0
| bool IADC_Init_t::iadcClkSuspend0 | 
Suspend IADC_CLK until PRS0 trigger.
◆ iadcClkSuspend1
| bool IADC_Init_t::iadcClkSuspend1 | 
Suspend IADC_CLK until PRS1 trigger.
◆ debugHalt
| bool IADC_Init_t::debugHalt | 
Halt IADC during debug mode.
◆ warmup
| IADC_Warmup_t IADC_Init_t::warmup | 
IADC warmup mode.
◆ timebase
| uint8_t IADC_Init_t::timebase | 
IADC clock cycles (timebase+1) corresponding to 1us.
Used as time reference for IADC delays, e.g. warmup. If the user sets timebase to 0, then IADC_Init() will calculate the timebase using the currently defined CMU clock setting for the IADC.
◆ srcClkPrescale
| uint8_t IADC_Init_t::srcClkPrescale | 
User requested source clock divider (prescale+1) which will be used if the calculated prescaler value is less.
◆ timerCycles
| uint16_t IADC_Init_t::timerCycles | 
Number of ADC_CLK cycles per TIMER event.
◆ greaterThanEqualThres
| uint16_t IADC_Init_t::greaterThanEqualThres | 
Digital window comparator greater-than or equal threshold.
◆ lessThanEqualThres
| uint16_t IADC_Init_t::lessThanEqualThres | 
Digital window comparator less-than or equal threshold.