Signature
Description
Digital Signature Algorithms (ECDSA, EdDSA).
API for using digital signatures with the SE.
Functions | |
sl_status_t | sl_se_ecc_sign (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char *message, size_t message_len, unsigned char *signature, size_t signature_len) |
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message. | |
sl_status_t | sl_se_ecc_verify (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_alg, bool hashed_message, const unsigned char *message, size_t message_len, const unsigned char *signature, size_t signature_len) |
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message. | |
Function Documentation
◆ sl_se_ecc_sign()
sl_status_t sl_se_ecc_sign | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_hash_type_t | hash_alg, |
||
bool | hashed_message, |
||
const unsigned char * | message, |
||
size_t | message_len, |
||
unsigned char * | signature, |
||
size_t | signature_len |
||
) |
This function computes Elliptic-Curve Cryptography (ECC) digital signatures of a message.
- Note
- Edwards-curve Digital Signature Algorithm (EdDSA) generates a message digest using the input message for computing signatures. The input parameters
hash_alg
andhashed_message
do not apply for EdDSA.
P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] hash_alg
Which hashing algorithm to use. [in] hashed_message
The input message is a message digest. [in] message
The message to be used to compute the signature. [in] message_len
The length of message. [out] signature
The computed signature. [in] signature_len
The length of the computed signature.
- Returns
- SL_STATUS_OK when the command was executed successfully, otherwise an appropiate error code (sl_status.h).
◆ sl_se_ecc_verify()
sl_status_t sl_se_ecc_verify | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_hash_type_t | hash_alg, |
||
bool | hashed_message, |
||
const unsigned char * | message, |
||
size_t | message_len, |
||
const unsigned char * | signature, |
||
size_t | signature_len |
||
) |
This function verifies Elliptic-Curve Cryptography (ECC) digital signatures of a message.
- Note
- The input parameters
hash_alg
andhashed_message
do not apply for Edwards-curve Digital Signature Algorithm (EdDSA).
P-521 Elliptic Curve for Elliptic Curve Digital Signature Algorithm (ECDSA) expects a 544 bits (68 bytes) buffer for storing private keys, and a 1088 bits (136 bytes) buffer for storing public keys and signatures. The first 23 bits of d, Qx, Qy, R and S are padding bits to comply word-aligned addressing.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] hash_alg
Which hashing algorithm to use. [in] hashed_message
The input message is a message digest. [in] message
The message to be used to compute signatures. [in] message_len
The length of message. [in] signature
The signature to be verified. [in] signature_len
The length of signature.
- Returns
- SL_STATUS_OK if the signature is successfully verified, otherwise an appropiate error code (sl_status.h).