Utilities
Description
Device initialisation, debug lock, upgrade functionality, user data...
API for managing the Secure Element or Root code on a device. Upload and read device configuration.
Modules | |
Tamper options | |
Tamper configuration options. Levels, signals and filter options. | |
Data Structures | |
struct | sl_se_cert_size_type_t |
Certificate size data structure. | |
struct | sl_se_otp_init_t |
OTP initialization data structure. | |
struct | sl_se_debug_options_t |
Debug lock options. | |
struct | sl_se_debug_status_t |
Debug status. | |
struct | sl_se_status_t |
SE status. | |
Functions | |
sl_status_t | sl_se_check_se_image (sl_se_command_context_t *cmd_ctx, void *image_addr) |
Validate SE firmware image. | |
sl_status_t | sl_se_apply_se_image (sl_se_command_context_t *cmd_ctx, void *image_addr) |
Apply SE firmware image. | |
sl_status_t | sl_se_get_upgrade_status_se_image (sl_se_command_context_t *cmd_ctx, uint32_t *status, uint32_t *prev_version) |
Get upgrade status of SE firmware image. | |
sl_status_t | sl_se_check_host_image (sl_se_command_context_t *cmd_ctx, void *image_addr, uint32_t size) |
Validate Host firmware image. | |
sl_status_t | sl_se_apply_host_image (sl_se_command_context_t *cmd_ctx, void *image_addr, uint32_t size) |
Apply Host firmware image. | |
sl_status_t | sl_se_upgrade_status_clear (sl_se_command_context_t *cmd_ctx) |
Clear Host firmware upgrade status. | |
sl_status_t | sl_se_get_upgrade_status_host_image (sl_se_command_context_t *cmd_ctx, uint32_t *status, uint32_t *prev_version) |
Get upgrade status of Host firmware image. | |
sl_status_t | sl_se_init_otp_key (sl_se_command_context_t *cmd_ctx, sl_se_device_key_type_t key_type, void *key, uint32_t num_bytes) |
Initialize key to be stored in the SE OTP flash. | |
sl_status_t | sl_se_read_pubkey (sl_se_command_context_t *cmd_ctx, sl_se_device_key_type_t key_type, void *key, uint32_t num_bytes) |
Read a public key stored in the SE. | |
sl_status_t | sl_se_init_otp (sl_se_command_context_t *cmd_ctx, sl_se_otp_init_t *otp_init) |
Initialize SE OTP configuration. | |
sl_status_t | sl_se_read_otp (sl_se_command_context_t *cmd_ctx, sl_se_otp_init_t *otp_settings) |
Read SE OTP configuration. | |
sl_status_t | sl_se_get_se_version (sl_se_command_context_t *cmd_ctx, uint32_t *version) |
Read the SE firmware version. | |
sl_status_t | sl_se_get_debug_lock_status (sl_se_command_context_t *cmd_ctx, sl_se_debug_status_t *status) |
Returns the current debug lock configuration. | |
sl_status_t | sl_se_apply_debug_lock (sl_se_command_context_t *cmd_ctx) |
Enables the debug lock for the part. | |
sl_status_t | sl_se_write_user_data (sl_se_command_context_t *cmd_ctx, uint32_t offset, void *data, uint32_t num_bytes) |
Writes data to User Data section in MTP. | |
sl_status_t | sl_se_erase_user_data (sl_se_command_context_t *cmd_ctx) |
Erases User Data section in MTP. | |
sl_status_t | sl_se_get_status (sl_se_command_context_t *cmd_ctx, sl_se_status_t *status) |
Returns the current boot status, versions and system configuration. | |
sl_status_t | sl_se_get_serialnumber (sl_se_command_context_t *cmd_ctx, void *serial) |
Read the serial number of the SE module. | |
sl_status_t | sl_se_get_otp_version (sl_se_command_context_t *cmd_ctx, uint32_t *version) |
Read the OTP firmware version of the SE module. | |
sl_status_t | sl_se_get_reset_cause (sl_se_command_context_t *cmd_ctx, uint32_t *reset_cause) |
Read the EMU->RSTCAUSE after a tamper reset. | |
sl_status_t | sl_se_enable_secure_debug (sl_se_command_context_t *cmd_ctx) |
Enables the secure debug functionality. | |
sl_status_t | sl_se_disable_secure_debug (sl_se_command_context_t *cmd_ctx) |
Disables the secure debug functionality. | |
sl_status_t | sl_se_set_debug_options (sl_se_command_context_t *cmd_ctx, const sl_se_debug_options_t *debug_options) |
Set debug options. | |
sl_status_t | sl_se_erase_device (sl_se_command_context_t *cmd_ctx) |
Performs a device mass erase and debug unlock. | |
sl_status_t | sl_se_disable_device_erase (sl_se_command_context_t *cmd_ctx) |
Disabled device erase functionality. | |
sl_status_t | sl_se_get_challenge (sl_se_command_context_t *cmd_ctx, sl_se_challenge_t challenge) |
Request challenge from SE which can be used to open debug access. | |
sl_status_t | sl_se_roll_challenge (sl_se_command_context_t *cmd_ctx) |
Invalidate current challenge and make a new challenge. | |
sl_status_t | sl_se_open_debug (sl_se_command_context_t *cmd_ctx, void *cert, uint32_t len, const sl_se_debug_options_t *debug_options) |
Unlock debug access using certificate and signed challenge. | |
sl_status_t | sl_se_disable_tamper (sl_se_command_context_t *cmd_ctx, void *cert, uint32_t len, sl_se_tamper_signals_t tamper_signals) |
Temporarily disable tamper configuration using certificate and signed challenge. | |
sl_status_t | sl_se_read_cert_size (sl_se_command_context_t *cmd_ctx, sl_se_cert_size_type_t *cert_size) |
Read size of stored certificates in SE. | |
sl_status_t | sl_se_read_cert (sl_se_command_context_t *cmd_ctx, sl_se_cert_type_t cert_type, void *cert, uint32_t num_bytes) |
Read stored certificates in SE. | |
Macros | |
#define | SL_SE_OTP_INIT_DEFAULT |
Default configuration for OTP initialisation structure. | |
#define | SL_SE_CHALLENGE_SIZE 16 |
SE Challenge size. | |
#define | SL_SE_CERT_KEY_SIZE 64 |
Certificate key size. | |
#define | SL_SE_CERT_SIGN_SIZE 64 |
Certificate signature size. | |
#define | SL_SE_CERT_BATCH 0x01 |
Batch ID certificate. | |
#define | SL_SE_CERT_DEVICE_SE 0x02 |
SE ID certificate. | |
#define | SL_SE_CERT_DEVICE_HOST 0x03 |
Host ID certificate. | |
Typedefs | |
typedef uint8_t | sl_se_tamper_level_t |
SE tamper signal levels. | |
typedef uint32_t | sl_se_tamper_signals_t |
SE tamper signals. | |
typedef uint8_t | sl_se_tamper_filter_period_t |
SE tamper filter timeout period. | |
typedef uint8_t | sl_se_tamper_filter_threshold_t |
Number of tamper counts to trigger the filter signal. | |
typedef uint8_t | sl_se_cert_type_t |
SE certificate types. | |
typedef uint32_t | sl_se_debug_flags_t |
SE Debug lock flags. | |
typedef uint8_t | sl_se_challenge_t[SL_SE_CHALLENGE_SIZE] |
SE challenge storage. | |
Enumerations | |
enum | sl_se_device_key_type_t { SL_SE_KEY_TYPE_IMMUTABLE_BOOT = 0, SL_SE_KEY_TYPE_IMMUTABLE_AUTH, SL_SE_KEY_TYPE_IMMUTABLE_AES_128, SL_SE_KEY_TYPE_IMMUTABLE_ATTESTATION, SL_SE_KEY_TYPE_IMMUTABLE_SE_ATTESTATION } |
OTP key types. | |
Function Documentation
◆ sl_se_check_se_image()
sl_status_t sl_se_check_se_image | ( | sl_se_command_context_t * | cmd_ctx, |
void * | image_addr |
||
) |
Validate SE firmware image.
Validate SE firmware image located at given address. This function is typically used before calling sl_se_apply_se_image.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] image_addr
Pointer to SE image to validate.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_apply_se_image()
sl_status_t sl_se_apply_se_image | ( | sl_se_command_context_t * | cmd_ctx, |
void * | image_addr |
||
) |
Apply SE firmware image.
Apply SE firmware image located at given address.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] image_addr
Pointer to SE image to apply.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_get_upgrade_status_se_image()
sl_status_t sl_se_get_upgrade_status_se_image | ( | sl_se_command_context_t * | cmd_ctx, |
uint32_t * | status, |
||
uint32_t * | prev_version |
||
) |
Get upgrade status of SE firmware image.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] status
Pointer to 32-bit word where to return upgrade status. [in] prev_version
Pointer to 32-bit word where to return previous version.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_check_host_image()
sl_status_t sl_se_check_host_image | ( | sl_se_command_context_t * | cmd_ctx, |
void * | image_addr, |
||
uint32_t | size |
||
) |
Validate Host firmware image.
Validate Host firmware image located at given address. This function is typically used before calling sl_se_apply_host_image.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] image_addr
Pointer to Host image to validate. [in] size
Size of Host image to validate.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_apply_host_image()
sl_status_t sl_se_apply_host_image | ( | sl_se_command_context_t * | cmd_ctx, |
void * | image_addr, |
||
uint32_t | size |
||
) |
Apply Host firmware image.
Apply Host firmware image located at given address.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] image_addr
Pointer to Host image to apply. [in] size
Size of Host image to apply.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_upgrade_status_clear()
sl_status_t sl_se_upgrade_status_clear | ( | sl_se_command_context_t * | cmd_ctx | ) |
Clear Host firmware upgrade status.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Returns
- Return values
-
SL_STATUS_OK
when the Host upgrade status has been cleared, otherwise an error code from sl_status.h if no upgrade has been run and there is nothing to clear.
◆ sl_se_get_upgrade_status_host_image()
sl_status_t sl_se_get_upgrade_status_host_image | ( | sl_se_command_context_t * | cmd_ctx, |
uint32_t * | status, |
||
uint32_t * | prev_version |
||
) |
Get upgrade status of Host firmware image.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] status
Pointer to 32-bit word where to return upgrade status. [in] prev_version
Pointer to 32-bit word where to return previous version.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_init_otp_key()
sl_status_t sl_se_init_otp_key | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_device_key_type_t | key_type, |
||
void * | key, |
||
uint32_t | num_bytes |
||
) |
Initialize key to be stored in the SE OTP flash.
Initialize key stored in the SE. The command can be used to write (sl_se_device_key_type_t):
- SL_SE_KEY_TYPE_IMMUTABLE_BOOT
- SL_SE_KEY_TYPE_IMMUTABLE_AUTH
- SL_SE_KEY_TYPE_IMMUTABLE_AES_128
- Note
- These keys can not be overwritten, so this command can only be issued once per key per part.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_type
ID of key type to initialize. [in] key
Pointer to a buffer that contains the key. Public keys must be word aligned and have a length of 64 bytes. AES-128 keys must be word aligned and have length of 16 bytes. [in] num_bytes
Length of key buffer in bytes (16 or 64 bytes).
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_read_pubkey()
sl_status_t sl_se_read_pubkey | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_device_key_type_t | key_type, |
||
void * | key, |
||
uint32_t | num_bytes |
||
) |
Read a public key stored in the SE.
Read out a public key stored in the SE. The command can be used to read (sl_se_device_key_type_t):
- SL_SE_KEY_TYPE_IMMUTABLE_BOOT
- SL_SE_KEY_TYPE_IMMUTABLE_AUTH
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key_type
ID of key type to read. [out] key
Pointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes. [in] num_bytes
Length of pubkey buffer (64 bytes).
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_init_otp()
sl_status_t sl_se_init_otp | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_otp_init_t * | otp_init |
||
) |
Initialize SE OTP configuration.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] otp_init
Pointer to OTP initialization structure.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed SL_STATUS_ABORT
when the operation is not attempted.
◆ sl_se_read_otp()
sl_status_t sl_se_read_otp | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_otp_init_t * | otp_settings |
||
) |
Read SE OTP configuration.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] otp_settings
Pointer to OTP initialization structure.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_COMMAND
if OTP configuration isn't initialized SL_STATUS_ABORT
when the operation is not attempted.
◆ sl_se_get_se_version()
sl_status_t sl_se_get_se_version | ( | sl_se_command_context_t * | cmd_ctx, |
uint32_t * | version |
||
) |
Read the SE firmware version.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] version
Pointer to uint32_t word where version shall be returned.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_OWNERSHIP
when the ownership is already taken SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_get_debug_lock_status()
sl_status_t sl_se_get_debug_lock_status | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_debug_status_t * | status |
||
) |
Returns the current debug lock configuration.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] status
Pointer to sl_se_debug_status_t structure to be filled out with the current status of the debug configuration.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_apply_debug_lock()
sl_status_t sl_se_apply_debug_lock | ( | sl_se_command_context_t * | cmd_ctx | ) |
Enables the debug lock for the part.
The debug port will be closed and the only way to open it is through device erase (if enabled) or through secure debug unlock (if enabled).
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully
◆ sl_se_write_user_data()
sl_status_t sl_se_write_user_data | ( | sl_se_command_context_t * | cmd_ctx, |
uint32_t | offset, |
||
void * | data, |
||
uint32_t | num_bytes |
||
) |
Writes data to User Data section in MTP.
Write data must be aligned to word size and contain a number of bytes that is divisable by four.
- Note
- It is recommended to erase the flash page before performing a write.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] offset
Offset to the flash word to write to. Must be aligned to words. [in] data
Data to write to flash. [in] num_bytes
Number of bytes to write to flash. NB: Must be divisable by four.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_erase_user_data()
sl_status_t sl_se_erase_user_data | ( | sl_se_command_context_t * | cmd_ctx | ) |
Erases User Data section in MTP.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_get_status()
sl_status_t sl_se_get_status | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_status_t * | status |
||
) |
Returns the current boot status, versions and system configuration.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] status
SE_Status_t containing current SE status.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
upon command completion. Errors are encoded in the different parts of the returned status object. SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_get_serialnumber()
sl_status_t sl_se_get_serialnumber | ( | sl_se_command_context_t * | cmd_ctx, |
void * | serial |
||
) |
Read the serial number of the SE module.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] serial
Pointer to array of size 16 bytes.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_get_otp_version()
sl_status_t sl_se_get_otp_version | ( | sl_se_command_context_t * | cmd_ctx, |
uint32_t * | version |
||
) |
Read the OTP firmware version of the SE module.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] version
Pointer to uint32_t word where version shall be returned.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_get_reset_cause()
sl_status_t sl_se_get_reset_cause | ( | sl_se_command_context_t * | cmd_ctx, |
uint32_t * | reset_cause |
||
) |
Read the EMU->RSTCAUSE after a tamper reset.
This function should be called if EMU->RSTCAUSE has been cleared upon boot.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] reset_cause
Pointer to uint32_t word where reset cause shall be returned.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized
◆ sl_se_enable_secure_debug()
sl_status_t sl_se_enable_secure_debug | ( | sl_se_command_context_t * | cmd_ctx | ) |
Enables the secure debug functionality.
Enables the secure debug functionality that can be used to open a locked debug port through the Get challenge and Open debug commands. This command can only be executed before the debug port is locked, and after a secure debug public key has been installed in the SE.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully
◆ sl_se_disable_secure_debug()
sl_status_t sl_se_disable_secure_debug | ( | sl_se_command_context_t * | cmd_ctx | ) |
Disables the secure debug functionality.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
Disables the secure debug functionality that can be used to open a locked debug port.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully
◆ sl_se_set_debug_options()
sl_status_t sl_se_set_debug_options | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_debug_options_t * | debug_options |
||
) |
Set debug options.
This function makes it possible to configure the Trust-Zone access permissions of the debug interface. For details please refer to sl_se_debug_options_t.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] debug_options
Pointer to debug options structure.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully
◆ sl_se_erase_device()
sl_status_t sl_se_erase_device | ( | sl_se_command_context_t * | cmd_ctx | ) |
Performs a device mass erase and debug unlock.
Performs a device mass erase and resets the debug configuration to its initial unlocked state. Only available before DEVICE_ERASE_DISABLE has been executed.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Note
- This command clears and verifies the complete flash and ram of the system, excluding the user data pages and one-time programmable commissioning information in the secure element.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_COMMAND
if device erase is disabled.
◆ sl_se_disable_device_erase()
sl_status_t sl_se_disable_device_erase | ( | sl_se_command_context_t * | cmd_ctx | ) |
Disabled device erase functionality.
This command disables the device erase command. It does not lock the debug interface to the part, but it is a permanent action for the part. If device erase is disabled and the device is debug locked, there is no way to permanently unlock the part. If secure debug unlock is enabled, secure debug unlock can still be used to temporarily open the debug port.
- Warning
- This command permanently disables the device erase functionality!
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully
◆ sl_se_get_challenge()
sl_status_t sl_se_get_challenge | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_challenge_t | challenge |
||
) |
Request challenge from SE which can be used to open debug access.
This command requests a challenge (16 bytes) which can be used to generate a certificate in order to open debug access, sl_se_open_debug.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] challenge
SE challenge storage.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_roll_challenge()
sl_status_t sl_se_roll_challenge | ( | sl_se_command_context_t * | cmd_ctx | ) |
Invalidate current challenge and make a new challenge.
This command requests the SE to invalidate it's current challenge (16bytes) and generate a new challenge.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully
◆ sl_se_open_debug()
sl_status_t sl_se_open_debug | ( | sl_se_command_context_t * | cmd_ctx, |
void * | cert, |
||
uint32_t | len, |
||
const sl_se_debug_options_t * | debug_options |
||
) |
Unlock debug access using certificate and signed challenge.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] cert
Certificate for debug unlock and signed challenge. [in] len
Length of certificate in number of bytes. [in] debug_options
Debug options to open/unlock.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_disable_tamper()
sl_status_t sl_se_disable_tamper | ( | sl_se_command_context_t * | cmd_ctx, |
void * | cert, |
||
uint32_t | len, |
||
sl_se_tamper_signals_t | tamper_signals |
||
) |
Temporarily disable tamper configuration using certificate and signed challenge.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] cert
Certificate for disabling tamper and signed challenge. [in] len
Length of certificate in number of bytes. [in] tamper_signals
Tamper signals to disable. Each signal represented by a bit.
- Returns
- One of the following sl_status_t codes:
- Return values
-
SL_STATUS_OK
when the command was executed successfully SL_STATUS_INVALID_OPERATION
when the SE command ID is not recognized SL_STATUS_INVALID_CREDENTIALS
when the command is not authorized SL_STATUS_INVALID_PARAMETER
when an invalid parameter was passed
◆ sl_se_read_cert_size()
sl_status_t sl_se_read_cert_size | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_cert_size_type_t * | cert_size |
||
) |
Read size of stored certificates in SE.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in,out] cert_size
Size of the certificates stored in SE.
- Returns
- Status code, sl_status.h.
◆ sl_se_read_cert()
sl_status_t sl_se_read_cert | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_cert_type_t | cert_type, |
||
void * | cert, |
||
uint32_t | num_bytes |
||
) |
Read stored certificates in SE.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] cert_type
Type of the certificate stored in SE. [in,out] cert
Buffer to read certificate. [in] num_bytes
Length of certificate in number of bytes.
- Returns
- Status code, sl_status.h.
Macro Definition Documentation
◆ SL_SE_OTP_INIT_DEFAULT
#define SL_SE_OTP_INIT_DEFAULT |
Default configuration for OTP initialisation structure.
◆ SL_SE_CHALLENGE_SIZE
#define SL_SE_CHALLENGE_SIZE 16 |
SE Challenge size.
◆ SL_SE_CERT_KEY_SIZE
#define SL_SE_CERT_KEY_SIZE 64 |
Certificate key size.
◆ SL_SE_CERT_SIGN_SIZE
#define SL_SE_CERT_SIGN_SIZE 64 |
Certificate signature size.
◆ SL_SE_CERT_BATCH
#define SL_SE_CERT_BATCH 0x01 |
Batch ID certificate.
◆ SL_SE_CERT_DEVICE_SE
#define SL_SE_CERT_DEVICE_SE 0x02 |
SE ID certificate.
◆ SL_SE_CERT_DEVICE_HOST
#define SL_SE_CERT_DEVICE_HOST 0x03 |
Host ID certificate.
Typedef Documentation
◆ sl_se_tamper_level_t
typedef uint8_t sl_se_tamper_level_t |
SE tamper signal levels.
◆ sl_se_tamper_signals_t
typedef uint32_t sl_se_tamper_signals_t |
SE tamper signals.
◆ sl_se_tamper_filter_period_t
typedef uint8_t sl_se_tamper_filter_period_t |
SE tamper filter timeout period.
◆ sl_se_tamper_filter_threshold_t
typedef uint8_t sl_se_tamper_filter_threshold_t |
Number of tamper counts to trigger the filter signal.
◆ sl_se_cert_type_t
typedef uint8_t sl_se_cert_type_t |
SE certificate types.
◆ sl_se_debug_flags_t
typedef uint32_t sl_se_debug_flags_t |
SE Debug lock flags.
◆ sl_se_challenge_t
typedef uint8_t sl_se_challenge_t[SL_SE_CHALLENGE_SIZE] |
SE challenge storage.
Enumeration Type Documentation
◆ sl_se_device_key_type_t
OTP key types.