LFXO Initialization
Description
Initialize the LFXO oscillator.
Configure the low frequency crystal oscillator using settings in the configuration header sl_device_init_lfxo_config.h
.
The precision of the oscillator can be indicated using the configuration option SL_DEVICE_INIT_LFXO_PRECISION
. This is used by certain wireless stacks to optimize wakeup time for scheduled events (such as Bluetooth advertising).
Functions | |
sl_status_t | sl_device_init_lfxo (void) |
Initialize LFXO. | |
Function Documentation
◆ sl_device_init_lfxo()
sl_status_t sl_device_init_lfxo | ( | void |
| ) |
Initialize LFXO.
Configure the low frequency crystal oscillator using settings in the configuration header sl_device_init_lfxo_config.h
.
The precision of the oscillator can be indicated using the configuration option SL_DEVICE_INIT_LFXO_PRECISION
. This is used by certain wireless stacks to optimize wakeup time for scheduled events (such as Bluetooth advertising).
- Returns
- Status code
- Return values
-
SL_STATUS_OK
LFXO initialized successfully