EMU Initialization
Description
Initialize the Energy Management Unit.
Initializes the Energy Management Unit by configuring Energy Mode 4 (EM4) according to settings in the configuration header sl_device_init_emu_config.h
.
On Series 2 devices, debugging in EM2 is enabled by default by ensuring that power to the debug power domain is sustained on EM2 entry.
- Note
- Voltage scaling for Energy Modes 0 to 3 are configured by the Power Manager.
Functions | |
sl_status_t | sl_device_init_emu (void) |
Initialize EMU. | |
Function Documentation
◆ sl_device_init_emu()
sl_status_t sl_device_init_emu | ( | void |
| ) |
Initialize EMU.
Initializes the Energy Management Unit by configuring Energy Mode 4 (EM4) according to settings in the configuration header sl_device_init_emu_config.h
.
On Series 2 devices, debugging in EM2 is enabled by default by ensuring that power to the debug power domain is sustained on EM2 entry.
- Note
- Voltage scaling for Energy Modes 0 to 3 are configured by the Power Manager.
- Returns
- Status code
- Return values
-
SL_STATUS_OK
EMU initialized successfully