__BMP_DataType Struct Reference
BMP Data type structure to hold information about the bmp data returned.
#include <bmp.h>
Data Fields | |
uint16_t | bitsPerPixel |
Color depth of the data returned from function. | |
uint32_t | compressionType |
Compression type. | |
uint32_t | size |
Byte length of returned data. | |
uint32_t | endOfRow |
Marks whether this data is at the end of the current row. | |
BMP Data type structure to hold information about the bmp data returned.
Field Documentation
◆ bitsPerPixel
uint16_t __BMP_DataType::bitsPerPixel |
Color depth of the data returned from function.
◆ compressionType
uint32_t __BMP_DataType::compressionType |
Compression type.
◆ size
uint32_t __BMP_DataType::size |
Byte length of returned data.
◆ endOfRow
uint32_t __BMP_DataType::endOfRow |
Marks whether this data is at the end of the current row.
endOfRow == 1, if end of row is reached. endOfRow == 0, if there is still unread data left in the row