ACMP_CapsenseInit_TypeDef Struct Reference
Capsense initialization structure.
#include <em_acmp.h>
Data Fields |
|
| uint32_t | biasProg |
|
Bias current.
|
|
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
|
Hysteresis level.
|
|
| ACMP_CapsenseResistor_TypeDef | resistor |
|
A resistor used in the capacative sensing circuit.
|
|
| uint32_t | vrefDiv |
|
VDD division factor.
|
|
| bool | enable |
|
If true, ACMP is enabled after configuration.
|
|
Capsense initialization structure.
Field Documentation
◆ biasProg
| uint32_t ACMP_CapsenseInit_TypeDef::biasProg |
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ hysteresisLevel
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel |
Hysteresis level.
◆ resistor
| ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor |
A resistor used in the capacative sensing circuit.
For values see the device data sheet.
◆ vrefDiv
| uint32_t ACMP_CapsenseInit_TypeDef::vrefDiv |
VDD division factor.
VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
◆ enable
| bool ACMP_CapsenseInit_TypeDef::enable |
If true, ACMP is enabled after configuration.