LESENSE_ConfAltEx_TypeDef Struct Reference
Configuration structure for the alternate excitation.
#include <em_lesense.h>
Data Fields | |
LESENSE_AltExMap_TypeDef | altExMap |
Select alternate excitation mapping. | |
LESENSE_AltExDesc_TypeDef | AltEx [16] |
Alternate excitation channel descriptors. | |
Configuration structure for the alternate excitation.
Field Documentation
◆ altExMap
LESENSE_AltExMap_TypeDef LESENSE_ConfAltEx_TypeDef::altExMap |
Select alternate excitation mapping.
◆ AltEx
LESENSE_AltExDesc_TypeDef LESENSE_ConfAltEx_TypeDef::AltEx[16] |
Alternate excitation channel descriptors.
When altExMap==lesenseAltExMapALTEX, only the 8 first descriptors are used. In this mode they describe the configuration of LES_ALTEX0-7 pins. When altExMap==lesenseAltExMapACMP, all 16 descriptors are used. In this mode they describe the configuration of the 16 possible ACMP0-1 excitation channels. Please refer to the user manual for a complete mapping of routing. NOTE: Some parameters in the descriptors are not valid when altExMap==lesenseAltExMapACMP. Refer to the definition of the LESENSE_AltExDesc_TypeDef structure for details regarding which parameters are valid.