RMU - Reset Management Unit
Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
Functions |
|
| void | RMU_ResetControl ( RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) |
|
Disable/enable reset for various peripherals and signal sources.
|
|
| void | RMU_ResetCauseClear (void) |
|
Clear the reset cause register.
|
|
| uint32_t | RMU_ResetCauseGet (void) |
|
Get the cause of the last reset.
|
|
Macros |
|
| #define | RMU_LockupResetDisable (A) RMU_ResetControl (rmuResetLockUp, A) |
|
RMU_LockupResetDisable kept for backwards compatibility.
|
|
Enumerations |
|
| enum |
RMU_ResetMode_TypeDef
{
rmuResetModeDisabled = 0, rmuResetModeEnabled = 1 } |
|
RMU reset modes.
|
|
| enum |
RMU_Reset_TypeDef
{
rmuResetWdog0 = _EMU_RSTCTRL_WDOG0RMODE_MASK, rmuResetWdog1 = _EMU_RSTCTRL_WDOG1RMODE_MASK, rmuResetSys = _EMU_RSTCTRL_SYSRMODE_MASK, rmuResetCoreLockup = _EMU_RSTCTRL_LOCKUPRMODE_MASK, rmuResetAVDD = _EMU_RSTCTRL_AVDDBODRMODE_MASK, rmuResetIOVDD0 = _EMU_RSTCTRL_IOVDD0BODRMODE_MASK, rmuResetDecouple = _EMU_RSTCTRL_DECBODRMODE_MASK, rmuResetSESys = _EMU_RSTCTRL_SESYSRMODE_MASK, rmuResetSELockup = _EMU_RSTCTRL_SELOCKUPRMODE_MASK } |
|
RMU controlled peripheral reset control and reset source control.
|
|
Function Documentation
◆ RMU_ResetControl()
| void RMU_ResetControl | ( | RMU_Reset_TypeDef |
reset,
|
| RMU_ResetMode_TypeDef |
mode
|
||
| ) |
Disable/enable reset for various peripherals and signal sources.
- Parameters
-
[in] resetReset types to enable/disable.s [in] modeReset mode.
◆ RMU_ResetCauseClear()
| void RMU_ResetCauseClear | ( | void |
|
) |
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet() .
◆ RMU_ResetCauseGet()
| uint32_t RMU_ResetCauseGet | ( | void |
|
) |
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear() . This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
Macro Definition Documentation
◆ RMU_LockupResetDisable
| #define RMU_LockupResetDisable | ( |
A
|
) | RMU_ResetControl (rmuResetLockUp, A) |
RMU_LockupResetDisable kept for backwards compatibility.
Enumeration Type Documentation
◆ RMU_ResetMode_TypeDef
◆ RMU_Reset_TypeDef
| enum RMU_Reset_TypeDef |
RMU controlled peripheral reset control and reset source control.