SE_Command_t Struct Reference
SE Command structure to which all commands to the SE must adhere.
#include <em_se.h>
Data Fields |
|
| uint32_t | command |
|
SE Command.
|
|
| SE_DataTransfer_t * | data_in |
|
Input data.
|
|
| SE_DataTransfer_t * | data_out |
|
Output data.
|
|
| uint32_t | parameters [ SE_MAX_PARAMETERS ] |
|
Parameters.
|
|
| size_t | num_parameters |
|
Number of parameters.
|
|
SE Command structure to which all commands to the SE must adhere.
Field Documentation
◆ command
| uint32_t SE_Command_t::command |
SE Command.
◆ data_in
| SE_DataTransfer_t * SE_Command_t::data_in |
Input data.
◆ data_out
| SE_DataTransfer_t * SE_Command_t::data_out |
Output data.
◆ parameters
| uint32_t SE_Command_t::parameters[ SE_MAX_PARAMETERS ] |
Parameters.
◆ num_parameters
| size_t SE_Command_t::num_parameters |
Number of parameters.