CSEN - Capacitive Sense
Description
Capacitive Sense (CSEN) Peripheral API.
Provides functions to control the capacitive sense peripheral of Silicon Labs' 32-bit MCUs and SoCs. The CSEN includes a capacitance-to-digital circuit that measures capacitance on selected inputs. Measurements are performed using either a Successive Approximation Register (SAR) or a Delta Modulator (DM) analog to digital converter.
The CSEN can be configured to measure capacitance on a single port pin or to automatically measure multiple port pins in succession using scan mode. Also, several port pins can be shorted together to measure the combined capacitance.
The CSEN includes an accumulator, which can be configured to average multiple conversions on the selected input. Additionally, an Exponential Moving Average (EMA) calculator is included to provide data smoothing. A comparator is also included and can be used to terminate a continuous conversion when the configured threshold condition is met.
The following example shows how to initialize and start a single conversion on one input:
| Data Structures | |
| struct | CSEN_Init_TypeDef | 
| CSEN initialization structure, common for all measurement modes. | |
| struct | CSEN_InitMode_TypeDef | 
| Measurement mode initialization structure. | |
| Functions | |
| void | CSEN_DMBaselineSet (CSEN_TypeDef *csen, uint32_t up, uint32_t down) | 
| Set the DM integrator initial value. | |
| void | CSEN_Init (CSEN_TypeDef *csen, const CSEN_Init_TypeDef *init) | 
| Initialize CSEN. | |
| void | CSEN_InitMode (CSEN_TypeDef *csen, const CSEN_InitMode_TypeDef *init) | 
| Initialize a CSEN measurement mode. | |
| void | CSEN_Reset (CSEN_TypeDef *csen) | 
| Reset CSEN to same state that it was in after a hardware reset. | |
| uint32_t | CSEN_DataGet (CSEN_TypeDef *csen) | 
| Get the last conversion result. | |
| uint32_t | CSEN_EMAGet (CSEN_TypeDef *csen) | 
| Get the last exponential moving average. | |
| void | CSEN_EMASet (CSEN_TypeDef *csen, uint32_t ema) | 
| Set the exponential moving average initial value. | |
| void | CSEN_Disable (CSEN_TypeDef *csen) | 
| Disable CSEN. | |
| void | CSEN_Enable (CSEN_TypeDef *csen) | 
| Enable CSEN. | |
| void | CSEN_IntClear (CSEN_TypeDef *csen, uint32_t flags) | 
| Clear one or more pending CSEN interrupts. | |
| void | CSEN_IntDisable (CSEN_TypeDef *csen, uint32_t flags) | 
| Disable one or more CSEN interrupts. | |
| void | CSEN_IntEnable (CSEN_TypeDef *csen, uint32_t flags) | 
| Enable one or more CSEN interrupts. | |
| uint32_t | CSEN_IntGet (CSEN_TypeDef *csen) | 
| Get pending CSEN interrupt flags. | |
| uint32_t | CSEN_IntGetEnabled (CSEN_TypeDef *csen) | 
| Get enabled and pending CSEN interrupt flags. | |
| void | CSEN_IntSet (CSEN_TypeDef *csen, uint32_t flags) | 
| Set one or more pending CSEN interrupts from SW. | |
| bool | CSEN_IsBusy (CSEN_TypeDef *csen) | 
| Return CSEN conversion busy status. | |
| void | CSEN_Start (CSEN_TypeDef *csen) | 
| Start a scan sequence and/or a single conversion. | |
| Macros | |
| #define | CSEN_INIT_DEFAULT | 
| CSEN default initialization. | |
| #define | CSEN_INITMODE_DEFAULT | 
| CSEN default mode initialization. | |
| Enumerations | |
| enum | CSEN_CmpMode_TypeDef
         
         { csenCmpModeDisabled = 0, csenCmpModeGreater = CSEN_CTRL_CMPEN | CSEN_CTRL_CMPPOL_GT, csenCmpModeLessOrEqual = CSEN_CTRL_CMPEN | CSEN_CTRL_CMPPOL_LTE, csenCmpModeEMAWindow = CSEN_CTRL_EMACMPEN } | 
| Comparator Mode. | |
| enum | CSEN_ConvSel_TypeDef
         
         { csenConvSelSAR = CSEN_CTRL_CONVSEL_SAR, csenConvSelSARChop = CSEN_CTRL_CONVSEL_SAR | CSEN_CTRL_CHOPEN_ENABLE, csenConvSelDM = CSEN_CTRL_CONVSEL_DM, csenConvSelDMChop = CSEN_CTRL_CONVSEL_DM | CSEN_CTRL_CHOPEN_ENABLE } | 
| Converter Select. | |
| enum | CSEN_SampleMode_TypeDef
         
         { csenSampleModeBonded = CSEN_CTRL_CM_SGL | CSEN_CTRL_MCEN_ENABLE, csenSampleModeSingle = CSEN_CTRL_CM_SGL, csenSampleModeScan = CSEN_CTRL_CM_SCAN, csenSampleModeContBonded = CSEN_CTRL_CM_CONTSGL | CSEN_CTRL_MCEN_ENABLE, csenSampleModeContSingle = CSEN_CTRL_CM_CONTSGL, csenSampleModeContScan = CSEN_CTRL_CM_CONTSCAN } | 
| Sample Mode. | |
| enum | CSEN_TrigSel_TypeDef
         
         { csenTrigSelPRS = _CSEN_CTRL_STM_PRS, csenTrigSelTimer = _CSEN_CTRL_STM_TIMER, csenTrigSelStart = _CSEN_CTRL_STM_START } | 
| Starts Trigger Select. | |
| enum | CSEN_AccMode_TypeDef
         
         { csenAccMode1 = _CSEN_CTRL_ACU_ACC1, csenAccMode2 = _CSEN_CTRL_ACU_ACC2, csenAccMode4 = _CSEN_CTRL_ACU_ACC4, csenAccMode8 = _CSEN_CTRL_ACU_ACC8, csenAccMode16 = _CSEN_CTRL_ACU_ACC16, csenAccMode32 = _CSEN_CTRL_ACU_ACC32, csenAccMode64 = _CSEN_CTRL_ACU_ACC64 } | 
| Accumulator Mode Select. | |
| enum | CSEN_SARRes_TypeDef
         
         { csenSARRes10 = _CSEN_CTRL_SARCR_CLK10, csenSARRes12 = _CSEN_CTRL_SARCR_CLK12, csenSARRes14 = _CSEN_CTRL_SARCR_CLK14, csenSARRes16 = _CSEN_CTRL_SARCR_CLK16 } | 
| Successive Approximation (SAR) Conversion Resolution. | |
| enum | CSEN_DMRes_TypeDef
         
         { csenDMRes10 = _CSEN_DMCFG_CRMODE_DM10, csenDMRes12 = _CSEN_DMCFG_CRMODE_DM12, csenDMRes14 = _CSEN_DMCFG_CRMODE_DM14, csenDMRes16 = _CSEN_DMCFG_CRMODE_DM16 } | 
| Delta Modulator (DM) Conversion Resolution. | |
| enum | CSEN_PCPrescale_TypeDef
         
         { csenPCPrescaleDiv1 = _CSEN_TIMCTRL_PCPRESC_DIV1, csenPCPrescaleDiv2 = _CSEN_TIMCTRL_PCPRESC_DIV2, csenPCPrescaleDiv4 = _CSEN_TIMCTRL_PCPRESC_DIV4, csenPCPrescaleDiv8 = _CSEN_TIMCTRL_PCPRESC_DIV8, csenPCPrescaleDiv16 = _CSEN_TIMCTRL_PCPRESC_DIV16, csenPCPrescaleDiv32 = _CSEN_TIMCTRL_PCPRESC_DIV32, csenPCPrescaleDiv64 = _CSEN_TIMCTRL_PCPRESC_DIV64, csenPCPrescaleDiv128 = _CSEN_TIMCTRL_PCPRESC_DIV128 } | 
| Period counter clock pre-scaler. | |
| enum | CSEN_EMASample_TypeDef
         
         { csenEMASampleW1 = _CSEN_EMACTRL_EMASAMPLE_W1, csenEMASampleW2 = _CSEN_EMACTRL_EMASAMPLE_W2, csenEMASampleW4 = _CSEN_EMACTRL_EMASAMPLE_W4, csenEMASampleW8 = _CSEN_EMACTRL_EMASAMPLE_W8, csenEMASampleW16 = _CSEN_EMACTRL_EMASAMPLE_W16, csenEMASampleW32 = _CSEN_EMACTRL_EMASAMPLE_W32, csenEMASampleW64 = _CSEN_EMACTRL_EMASAMPLE_W64 } | 
| Exponential Moving Average sample weight. | |
| enum | CSEN_ResetPhaseSel_TypeDef
         
         { csenResetPhaseSel0 = 0, csenResetPhaseSel1 = 1, csenResetPhaseSel2 = 2, csenResetPhaseSel3 = 3, csenResetPhaseSel4 = 4, csenResetPhaseSel5 = 5, csenResetPhaseSel6 = 6, csenResetPhaseSel7 = 7 } | 
| Reset Phase Timing Select (units are microseconds). | |
| enum | CSEN_DriveSel_TypeDef
         
         { csenDriveSelFull = 0, csenDriveSel1 = 1, csenDriveSel2 = 2, csenDriveSel3 = 3, csenDriveSel4 = 4, csenDriveSel5 = 5, csenDriveSel6 = 6, csenDriveSel7 = 7 } | 
| Drive Strength Select. | |
| enum | CSEN_GainSel_TypeDef
         
         { csenGainSel1X = 0, csenGainSel2X = 1, csenGainSel3X = 2, csenGainSel4X = 3, csenGainSel5X = 4, csenGainSel6X = 5, csenGainSel7X = 6, csenGainSel8X = 7 } | 
| Gain Select. | |
| enum | CSEN_PRSSel_TypeDef
         
         { csenPRSSELCh0 = _CSEN_PRSSEL_PRSSEL_PRSCH0, csenPRSSELCh1 = _CSEN_PRSSEL_PRSSEL_PRSCH1, csenPRSSELCh2 = _CSEN_PRSSEL_PRSSEL_PRSCH2, csenPRSSELCh3 = _CSEN_PRSSEL_PRSSEL_PRSCH3, csenPRSSELCh4 = _CSEN_PRSSEL_PRSSEL_PRSCH4, csenPRSSELCh5 = _CSEN_PRSSEL_PRSSEL_PRSCH5, csenPRSSELCh6 = _CSEN_PRSSEL_PRSSEL_PRSCH6, csenPRSSELCh7 = _CSEN_PRSSEL_PRSSEL_PRSCH7, csenPRSSELCh8 = _CSEN_PRSSEL_PRSSEL_PRSCH8, csenPRSSELCh9 = _CSEN_PRSSEL_PRSSEL_PRSCH9, csenPRSSELCh10 = _CSEN_PRSSEL_PRSSEL_PRSCH10, csenPRSSELCh11 = _CSEN_PRSSEL_PRSSEL_PRSCH11 } | 
| Peripheral Reflex System signal used to trigger conversion. | |
| enum | CSEN_InputSel_TypeDef
         
         { csenInputSelDefault = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_DEFAULT, csenInputSelAPORT1CH0TO7 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT1CH0TO7, csenInputSelAPORT1CH8TO15 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT1CH8TO15, csenInputSelAPORT1CH16TO23 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT1CH16TO23, csenInputSelAPORT1CH24TO31 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT1CH24TO31, csenInputSelAPORT3CH0TO7 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT3CH0TO7, csenInputSelAPORT3CH8TO15 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT3CH8TO15, csenInputSelAPORT3CH16TO23 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT3CH16TO23, csenInputSelAPORT3CH24TO31 = _CSEN_SCANINPUTSEL0_INPUT0TO7SEL_APORT3CH24TO31 } | 
| APORT channel to CSEN input selection. | |
| enum | CSEN_SingleSel_TypeDef
         
         { csenSingleSelDefault = _CSEN_SINGLECTRL_SINGLESEL_DEFAULT, csenSingleSelAPORT1XCH0 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH0, csenSingleSelAPORT1YCH1 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH1, csenSingleSelAPORT1XCH2 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH2, csenSingleSelAPORT1YCH3 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH3, csenSingleSelAPORT1XCH4 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH4, csenSingleSelAPORT1YCH5 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH5, csenSingleSelAPORT1XCH6 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH6, csenSingleSelAPORT1YCH7 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH7, csenSingleSelAPORT1XCH8 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH8, csenSingleSelAPORT1YCH9 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH9, csenSingleSelAPORT1XCH10 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH10, csenSingleSelAPORT1YCH11 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH11, csenSingleSelAPORT1XCH12 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH12, csenSingleSelAPORT1YCH13 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH13, csenSingleSelAPORT1XCH14 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH14, csenSingleSelAPORT1YCH15 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH15, csenSingleSelAPORT1XCH16 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH16, csenSingleSelAPORT1YCH17 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH17, csenSingleSelAPORT1XCH18 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH18, csenSingleSelAPORT1YCH19 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH19, csenSingleSelAPORT1XCH20 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH20, csenSingleSelAPORT1YCH21 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH21, csenSingleSelAPORT1XCH22 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH22, csenSingleSelAPORT1YCH23 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH23, csenSingleSelAPORT1XCH24 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH24, csenSingleSelAPORT1YCH25 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH25, csenSingleSelAPORT1XCH26 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH26, csenSingleSelAPORT1YCH27 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH27, csenSingleSelAPORT1XCH28 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH28, csenSingleSelAPORT1YCH29 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH29, csenSingleSelAPORT1XCH30 = _CSEN_SINGLECTRL_SINGLESEL_APORT1XCH30, csenSingleSelAPORT1YCH31 = _CSEN_SINGLECTRL_SINGLESEL_APORT1YCH31, csenSingleSelAPORT3XCH0 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH0, csenSingleSelAPORT3YCH1 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH1, csenSingleSelAPORT3XCH2 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH2, csenSingleSelAPORT3YCH3 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH3, csenSingleSelAPORT3XCH4 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH4, csenSingleSelAPORT3YCH5 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH5, csenSingleSelAPORT3XCH6 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH6, csenSingleSelAPORT3YCH7 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH7, csenSingleSelAPORT3XCH8 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH8, csenSingleSelAPORT3YCH9 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH9, csenSingleSelAPORT3XCH10 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH10, csenSingleSelAPORT3YCH11 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH11, csenSingleSelAPORT3XCH12 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH12, csenSingleSelAPORT3YCH13 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH13, csenSingleSelAPORT3XCH14 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH14, csenSingleSelAPORT3YCH15 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH15, csenSingleSelAPORT3XCH16 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH16, csenSingleSelAPORT3YCH17 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH17, csenSingleSelAPORT3XCH18 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH18, csenSingleSelAPORT3YCH19 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH19, csenSingleSelAPORT3XCH20 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH20, csenSingleSelAPORT3YCH21 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH21, csenSingleSelAPORT3XCH22 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH22, csenSingleSelAPORT3YCH23 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH23, csenSingleSelAPORT3XCH24 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH24, csenSingleSelAPORT3YCH25 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH25, csenSingleSelAPORT3XCH26 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH26, csenSingleSelAPORT3YCH27 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH27, csenSingleSelAPORT3XCH28 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH28, csenSingleSelAPORT3YCH29 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH29, csenSingleSelAPORT3XCH30 = _CSEN_SINGLECTRL_SINGLESEL_APORT3XCH30, csenSingleSelAPORT3YCH31 = _CSEN_SINGLECTRL_SINGLESEL_APORT3YCH31 } | 
| APORT channel to CSEN single input selection. | |
Function Documentation
◆ CSEN_DMBaselineSet()
| void CSEN_DMBaselineSet | ( | CSEN_TypeDef * | 
            csen,
            | 
| uint32_t | 
            up,
            | ||
| uint32_t | 
            down
            | ||
| ) | 
Set the DM integrator initial value.
Sets the initial value of the integrator(s) for the Delta Modulation (DM) converter. The initial value for the ramp-down integrator has no effect if the low-frequency attenuation was not selected by the mode initialization function CSEN_InitMode() .
- Note
- Confirm CSEN is idle before calling this function.
- Parameters
- 
         [in] csenA pointer to the CSEN peripheral register block. [in] upAn initial value for the ramp-up integrator. [in] downAn initial value for the ramp-down integrator. Has no effect if low-frequency attenuation is not configured. 
◆ CSEN_Init()
| void CSEN_Init | ( | CSEN_TypeDef * | 
            csen,
            | 
| const CSEN_Init_TypeDef * | 
            init
            | ||
| ) | 
Initialize CSEN.
Initializes common functionality for all measurement types. In addition, measurement mode must be configured. See CSEN_InitMode() .
- Note
- This function will stop any ongoing conversion and disable CSEN.
- Parameters
- 
         [in] csenA pointer to the CSEN peripheral register block. [in] initA pointer to the CSEN initialization structure. 
◆ CSEN_InitMode()
| void CSEN_InitMode | ( | CSEN_TypeDef * | 
            csen,
            | 
| const CSEN_InitMode_TypeDef * | 
            init
            | ||
| ) | 
Initialize a CSEN measurement mode.
Used to configure any type of measurement mode. After the measurement has been configured, calling CSEN_Enable() will enable CSEN and allow it to start a conversion from the selected trigger source. To manually start a conversion, use CSEN_Start() . To check if a conversion is in progress, use CSEN_IsBusy() , or alternatively use the interrupt flags returned by CSEN_IntGet() to detect when a conversion is completed.
- Note
- This function will stop any ongoing conversion and disable CSEN.
- Parameters
- 
         [in] csenA pointer to the CSEN peripheral register block. [in] initA pointer to the CSEN measurement mode initialization structure. 
◆ CSEN_Reset()
| void CSEN_Reset | ( | CSEN_TypeDef * | 
            csen
            | ) | 
Reset CSEN to same state that it was in after a hardware reset.
- Parameters
- 
         [in] csenA pointer to the CSEN peripheral register block. 
◆ CSEN_DataGet()
| 
 | inline | 
Get the last conversion result.
- Note
- Check the conversion busy flag before calling this function. In addition, the result width and format depend on the parameters passed to the CSEN_InitMode() function.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
- Returns
- Result data from last conversion.
◆ CSEN_EMAGet()
| 
 | inline | 
Get the last exponential moving average.
- Note
- Confirm that CSEN is idle before calling this function.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
- Returns
- Exponential moving average from last conversion.
◆ CSEN_EMASet()
| 
 | inline | 
Set the exponential moving average initial value.
- Note
- Call this function before starting a conversion.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. [in] emaInitial value for the exponential moving average. 
◆ CSEN_Disable()
| 
 | inline | 
Disable CSEN.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
◆ CSEN_Enable()
| 
 | inline | 
Enable CSEN.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
◆ CSEN_IntClear()
| 
 | inline | 
Clear one or more pending CSEN interrupts.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. [in] flagsPending CSEN interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the CSEN module (CSEN_IF_nnn). 
◆ CSEN_IntDisable()
| 
 | inline | 
Disable one or more CSEN interrupts.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. [in] flagsCSEN interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the CSEN module (CSEN_IF_nnn). 
◆ CSEN_IntEnable()
| 
 | inline | 
Enable one or more CSEN interrupts.
- Note
- Depending on the use case, a pending interrupt may already be set prior to enabling the interrupt. Consider using CSEN_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. [in] flagsCSEN interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the CSEN module (CSEN_IF_nnn). 
◆ CSEN_IntGet()
| 
 | inline | 
Get pending CSEN interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
- Returns
- CSEN interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the CSEN module (CSEN_IF_nnn).
◆ CSEN_IntGetEnabled()
| 
 | inline | 
Get enabled and pending CSEN interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- 
         Pending and enabled CSEN interrupt sources. The return value is the bitwise AND combination of
         - the OR combination of enabled interrupt sources in CSENx_IEN_nnn register (CSENx_IEN_nnn) and
- the OR combination of valid interrupt flags of the CSEN module (CSENx_IF_nnn).
 
◆ CSEN_IntSet()
| 
 | inline | 
Set one or more pending CSEN interrupts from SW.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. [in] flagsCSEN interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the CSEN module (CSEN_IF_nnn). 
◆ CSEN_IsBusy()
| 
 | inline | 
Return CSEN conversion busy status.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
- Returns
- True if CSEN conversion is in progress.
◆ CSEN_Start()
| 
 | inline | 
Start a scan sequence and/or a single conversion.
- Parameters
- 
         [in] csenPointer to a CSEN peripheral register block. 
Macro Definition Documentation
◆ CSEN_INIT_DEFAULT
| #define CSEN_INIT_DEFAULT | 
CSEN default initialization.
◆ CSEN_INITMODE_DEFAULT
| #define CSEN_INITMODE_DEFAULT | 
CSEN default mode initialization.
Enumeration Type Documentation
◆ CSEN_CmpMode_TypeDef
| enum CSEN_CmpMode_TypeDef | 
Comparator Mode.
Selects the operation of the digital comparator.
◆ CSEN_ConvSel_TypeDef
| enum CSEN_ConvSel_TypeDef | 
Converter Select.
Determines the converter operational mode.
◆ CSEN_SampleMode_TypeDef
Sample Mode.
Determines how inputs are sampled for a conversion.
◆ CSEN_TrigSel_TypeDef
| enum CSEN_TrigSel_TypeDef | 
◆ CSEN_AccMode_TypeDef
| enum CSEN_AccMode_TypeDef | 
◆ CSEN_SARRes_TypeDef
| enum CSEN_SARRes_TypeDef | 
◆ CSEN_DMRes_TypeDef
| enum CSEN_DMRes_TypeDef | 
◆ CSEN_PCPrescale_TypeDef
Period counter clock pre-scaler.
See the reference manual for source clock information.
◆ CSEN_EMASample_TypeDef
◆ CSEN_ResetPhaseSel_TypeDef
Reset Phase Timing Select (units are microseconds).
◆ CSEN_DriveSel_TypeDef
Drive Strength Select.
Scales the output current.
◆ CSEN_GainSel_TypeDef
| enum CSEN_GainSel_TypeDef | 
◆ CSEN_PRSSel_TypeDef
| enum CSEN_PRSSel_TypeDef | 
Peripheral Reflex System signal used to trigger conversion.
◆ CSEN_InputSel_TypeDef
APORT channel to CSEN input selection.
◆ CSEN_SingleSel_TypeDef
APORT channel to CSEN single input selection.