WDOG_Init_TypeDef Struct Reference
Watchdog initialization structure.
#include <em_wdog.h>
Data Fields |
|
bool | enable |
Enable Watchdog when initialization completed.
|
|
bool | debugRun |
Counter keeps running during debug halt.
|
|
bool | clrSrc |
Select WDOG clear source: False: Write to the clear bit will clear the WDOG counter True: Rising edge on the PRS Source 0 will clear the WDOG counter.
|
|
bool | em2Run |
Counter keeps running when in EM2.
|
|
bool | em3Run |
Counter keeps running when in EM3.
|
|
bool | em4Block |
Block EMU from entering EM4.
|
|
bool | swoscBlock |
Block SW from disabling LFRCO/LFXO oscillators.
|
|
bool | lock |
Block SW from modifying the configuration (a reset is needed to reconfigure).
|
|
WDOG_ClkSel_TypeDef | clkSel |
Clock source to use for Watchdog.
|
|
WDOG_PeriodSel_TypeDef | perSel |
Watchdog timeout period.
|
|
WDOG_WarnSel_TypeDef | warnSel |
Select warning time as % of the Watchdog timeout.
|
|
WDOG_WinSel_TypeDef | winSel |
Select illegal window time as % of the Watchdog timeout.
|
|
bool | resetDisable |
Disable Watchdog reset output if true.
|
|
Watchdog initialization structure.
Field Documentation
◆ enable
bool WDOG_Init_TypeDef::enable |
Enable Watchdog when initialization completed.
◆ debugRun
bool WDOG_Init_TypeDef::debugRun |
Counter keeps running during debug halt.
◆ clrSrc
bool WDOG_Init_TypeDef::clrSrc |
Select WDOG clear source: False: Write to the clear bit will clear the WDOG counter True: Rising edge on the PRS Source 0 will clear the WDOG counter.
◆ em2Run
bool WDOG_Init_TypeDef::em2Run |
Counter keeps running when in EM2.
◆ em3Run
bool WDOG_Init_TypeDef::em3Run |
Counter keeps running when in EM3.
◆ em4Block
bool WDOG_Init_TypeDef::em4Block |
Block EMU from entering EM4.
◆ swoscBlock
bool WDOG_Init_TypeDef::swoscBlock |
Block SW from disabling LFRCO/LFXO oscillators.
◆ lock
bool WDOG_Init_TypeDef::lock |
Block SW from modifying the configuration (a reset is needed to reconfigure).
◆ clkSel
WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel |
Clock source to use for Watchdog.
◆ perSel
WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel |
Watchdog timeout period.
◆ warnSel
WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel |
Select warning time as % of the Watchdog timeout.
◆ winSel
WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel |
Select illegal window time as % of the Watchdog timeout.
◆ resetDisable
bool WDOG_Init_TypeDef::resetDisable |
Disable Watchdog reset output if true.