ADC_InitScan_TypeDef Struct Reference
Scan sequence initialization structure.
      
       #include <em_adc.h>
      
     
| Data Fields | |
| ADC_PRSSEL_TypeDef | prsSel | 
| Peripheral reflex system trigger selection. | |
| ADC_AcqTime_TypeDef | acqTime | 
| Acquisition time (in ADC clock cycles). | |
| ADC_Ref_TypeDef | reference | 
| Sample reference selection. | |
| ADC_Res_TypeDef | resolution | 
| Sample resolution. | |
| ADC_InitScanInput_TypeDef | scanInputConfig | 
| Scan input configuration. | |
| bool | diff | 
| Select if single-ended or differential input. | |
| bool | prsEnable | 
| Peripheral reflex system trigger enable. | |
| bool | leftAdjust | 
| Select if left adjustment should be done. | |
| bool | rep | 
| Select if continuous conversion until explicit stop. | |
| bool | scanDmaEm2Wu | 
| When true, DMA is available in EM2 for scan conversion. | |
| bool | fifoOverwrite | 
| When true, FIFO overwrites old data when full. | |
Scan sequence initialization structure.
Field Documentation
◆ prsSel
| ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel | 
Peripheral reflex system trigger selection.
        Only applicable if
        
         prsEnable
        
        is enabled.
       
◆ acqTime
| ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime | 
Acquisition time (in ADC clock cycles).
◆ reference
| ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference | 
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
◆ resolution
| ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution | 
Sample resolution.
◆ scanInputConfig
| ADC_InitScanInput_TypeDef ADC_InitScan_TypeDef::scanInputConfig | 
Scan input configuration.
Use ADC_ScanInputClear() , ADC_ScanSingleEndedInputAdd() or ADC_ScanDifferentialInputAdd() to update this structure.
◆ diff
| bool ADC_InitScan_TypeDef::diff | 
Select if single-ended or differential input.
◆ prsEnable
| bool ADC_InitScan_TypeDef::prsEnable | 
Peripheral reflex system trigger enable.
◆ leftAdjust
| bool ADC_InitScan_TypeDef::leftAdjust | 
Select if left adjustment should be done.
◆ rep
| bool ADC_InitScan_TypeDef::rep | 
Select if continuous conversion until explicit stop.
◆ scanDmaEm2Wu
| bool ADC_InitScan_TypeDef::scanDmaEm2Wu | 
When true, DMA is available in EM2 for scan conversion.
◆ fifoOverwrite
| bool ADC_InitScan_TypeDef::fifoOverwrite | 
When true, FIFO overwrites old data when full.
If false, FIFO discards new data. The SINGLEOF IRQ is triggered in both cases.