SegmentLcdKit Drivers
Enumerations | |
enum | SegmentLCD_BlockMode_TypeDef { segmentLCDBlockModeBlank = SEGMENT_LCD_BLOCK_MODE_BLANK, segmentLCDBlockModeFill = SEGMENT_LCD_BLOCK_MODE_FILL, segmentLCDBlockModeOutline = SEGMENT_LCD_BLOCK_MODE_OUTLINE, segmentLCDBlockModeOutlineFill = SEGMENT_LCD_BLOCK_MODE_OUTLINE_FILL } |
Functions | |
void | SegmentLCD_AllOff (void) |
Disable all segments. | |
void | SegmentLCD_AllOn (void) |
Enable all segments. | |
void | SegmentLCD_AlphaNumberOff (void) |
Turn all segments on alpha characters in display off. | |
void | SegmentLCD_ARing (int anum, int on) |
Light up or shut off Ring of Indicators. | |
void | SegmentLCD_Battery (int batteryLevel) |
Light up or shut off Battery Indicator. | |
void | SegmentLCD_Block (SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS]) |
void | SegmentLCD_Disable (void) |
Disables LCD controller. | |
void | SegmentLCD_EnergyMode (int em, int on) |
Light up or shut off Energy Mode indicator. | |
void | SegmentLCD_Init (bool useBoost) |
Segment LCD Initialization routine for EFM32 STK display. | |
void | SegmentLCD_LowerHex (uint32_t num) |
Write a hexadecimal number on lower alphanumeric part of Segment LCD display. | |
void | SegmentLCD_LowerNumber (int num) |
Write number on lower alphanumeric part of Segment LCD display. | |
void | SegmentLCD_Number (int value) |
Write number on numeric part on Segment LCD display. | |
void | SegmentLCD_NumberOff (void) |
Turn all segments on numeric digits in display off. | |
void | SegmentLCD_Symbol (lcdSymbol s, int on) |
Light up or shut off various symbols on Segment LCD. | |
void | SegmentLCD_UnsignedHex (uint32_t value) |
Write hexadecimal number on numeric part on Segment LCD display. | |
void | SegmentLCD_Write (const char *string) |
Write text on LCD display. | |
Enumeration Type Documentation
Function Documentation
void SegmentLCD_ARing | ( | int | anum, |
int | on |
||
) |
Light up or shut off Ring of Indicators.
- Parameters
-
anum
"Segment number" on "Ring", range 0 - 7 on
Zero is off, non-zero is on
Definition at line 1361
of file segmentlcd.c
.
References MCU_DISPLAY::ARing, ARING_TypeDef::bit, and ARING_TypeDef::com.
void SegmentLCD_Battery | ( | int | batteryLevel | ) |
Light up or shut off Battery Indicator.
- Parameters
-
batteryLevel
Battery Level, 0 to 4 (0 turns all off)
Definition at line 1379
of file segmentlcd.c
.
References MCU_DISPLAY::Battery, BATTERY_TypeDef::bit, and BATTERY_TypeDef::com.
void SegmentLCD_EnergyMode | ( | int | em, |
int | on |
||
) |
Light up or shut off Energy Mode indicator.
- Parameters
-
em
Energy Mode numer 0 to 4 on
Zero is off, non-zero is on
Definition at line 1406
of file segmentlcd.c
.
References EM_TypeDef::bit, EM_TypeDef::com, and MCU_DISPLAY::EMode.
void SegmentLCD_Init | ( | bool | useBoost | ) |
Segment LCD Initialization routine for EFM32 STK display.
- Parameters
-
useBoost
Set to use voltage boost
Definition at line 448
of file segmentlcd.c
.
References CMU, CMU_ClockDivSet(), CMU_ClockEnable(), CMU_ClockSelectSet(), CMU_LCDClkFDIVSet(), cmuClock_LFA, cmuSelect_LFRCO, and SegmentLCD_AllOff().
void SegmentLCD_LowerHex | ( | uint32_t | num | ) |
Write a hexadecimal number on lower alphanumeric part of Segment LCD display.
- Parameters
-
num
Hexadecimal number value to put on display, in range 0 to 0x0FFFFFFF
Definition at line 502
of file segmentlcd.c
.
References SegmentLCD_Symbol(), and SegmentLCD_Write().
void SegmentLCD_LowerNumber | ( | int | num | ) |
Write number on lower alphanumeric part of Segment LCD display.
- Parameters
-
num
Numeric value to put on display, in range -9999999 to +9999999
Definition at line 535
of file segmentlcd.c
.
References SegmentLCD_Symbol(), and SegmentLCD_Write().
void SegmentLCD_Number | ( | int | value | ) |
Write number on numeric part on Segment LCD display.
- Parameters
-
value
Numeric value to put on display, in range -999 to +9999
Definition at line 580
of file segmentlcd.c
.
References NUMBER_TypeDef::bit, NUMBER_TypeDef::com, MCU_DISPLAY::Number, Segment_Numbers, and SegmentLCD_NumberOff().
void SegmentLCD_Symbol | ( | lcdSymbol | s, |
int | on |
||
) |
Light up or shut off various symbols on Segment LCD.
- Parameters
-
s
Which symbol to turn on or off on
Zero is off, non-zero is on
Definition at line 661
of file segmentlcd.c
.
Referenced by SegmentLCD_LowerHex(), and SegmentLCD_LowerNumber().
void SegmentLCD_UnsignedHex | ( | uint32_t | value | ) |
Write hexadecimal number on numeric part on Segment LCD display.
- Parameters
-
value
Numeric value to put on display
Definition at line 1015
of file segmentlcd.c
.
References NUMBER_TypeDef::bit, NUMBER_TypeDef::com, MCU_DISPLAY::Number, Segment_Numbers, and SegmentLCD_NumberOff().
void SegmentLCD_Write | ( | const char * | string | ) |
Write text on LCD display.
- Parameters
-
string
Text string to show on display
Definition at line 1062
of file segmentlcd.c
.
References CHAR_TypeDef::bit, CHAR_TypeDef::com, Segment_Alphabet, SegmentLCD_AlphaNumberOff(), and MCU_DISPLAY::Text.
Referenced by SegmentLCD_LowerHex(), and SegmentLCD_LowerNumber().