AES_TypeDef Struct ReferenceDevices > EFM32HG_AES

Definition at line 48 of file efm32hg_aes.h.

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t DATA
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t KEYLA
 
__IOM uint32_t KEYLB
 
__IOM uint32_t KEYLC
 
__IOM uint32_t KEYLD
 
uint32_t RESERVED0 [3]
 
__IM uint32_t STATUS
 
__IOM uint32_t XORDATA
 

Field Documentation

__IOM uint32_t AES_TypeDef::CMD

Command Register

Definition at line 50 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::DATA

DATA Register

Definition at line 56 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::IEN

Interrupt Enable Register

Definition at line 52 of file efm32hg_aes.h.

__IM uint32_t AES_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::KEYLA

KEY Low Register

Definition at line 59 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::KEYLB

KEY Low Register

Definition at line 60 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::KEYLC

KEY Low Register

Definition at line 61 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::KEYLD

KEY Low Register

Definition at line 62 of file efm32hg_aes.h.

uint32_t AES_TypeDef::RESERVED0[3]

Reserved for future use

Definition at line 58 of file efm32hg_aes.h.

__IM uint32_t AES_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32hg_aes.h.

__IOM uint32_t AES_TypeDef::XORDATA

XORDATA Register

Definition at line 57 of file efm32hg_aes.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/efm32hg_aes.h