GPIO_P_TypeDef Struct ReferenceDevices
GPIO_P EFM32HG GPIO P.
       Definition at line
       
        46
       
       of file
       
        efm32hg_gpio_p.h
       
       .
      
      
       #include <
       
     
        efm32hg_gpio_p.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CTRL | 
| __IM uint32_t | DIN | 
| __IOM uint32_t | DOUT | 
| __OM uint32_t | DOUTCLR | 
| __OM uint32_t | DOUTSET | 
| __OM uint32_t | DOUTTGL | 
| __IOM uint32_t | MODEH | 
| __IOM uint32_t | MODEL | 
| __IOM uint32_t | PINLOCKN | 
Field Documentation
| __IOM uint32_t GPIO_P_TypeDef::CTRL | 
Port Control Register
        Definition at line
        
         47
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __IM uint32_t GPIO_P_TypeDef::DIN | 
Port Data In Register
        Definition at line
        
         54
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __IOM uint32_t GPIO_P_TypeDef::DOUT | 
Port Data Out Register
        Definition at line
        
         50
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __OM uint32_t GPIO_P_TypeDef::DOUTCLR | 
Port Data Out Clear Register
        Definition at line
        
         52
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __OM uint32_t GPIO_P_TypeDef::DOUTSET | 
Port Data Out Set Register
        Definition at line
        
         51
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __OM uint32_t GPIO_P_TypeDef::DOUTTGL | 
Port Data Out Toggle Register
        Definition at line
        
         53
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __IOM uint32_t GPIO_P_TypeDef::MODEH | 
Port Pin Mode High Register
        Definition at line
        
         49
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __IOM uint32_t GPIO_P_TypeDef::MODEL | 
Port Pin Mode Low Register
        Definition at line
        
         48
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
| __IOM uint32_t GPIO_P_TypeDef::PINLOCKN | 
Port Unlocked Pins Register
        Definition at line
        
         55
        
        of file
        
         efm32hg_gpio_p.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/
       efm32hg_gpio_p.h