DMA_TypeDef Struct ReferenceDevices > EFM32HG_DMA
Definition at line 48
of file efm32hg_dma.h
.
Data Fields | |
__IM uint32_t | ALTCTRLBASE |
DMA_CH_TypeDef | CH [6] |
__OM uint32_t | CHALTC |
__IOM uint32_t | CHALTS |
__OM uint32_t | CHENC |
__IOM uint32_t | CHENS |
__OM uint32_t | CHPRIC |
__IOM uint32_t | CHPRIS |
__OM uint32_t | CHREQMASKC |
__IOM uint32_t | CHREQMASKS |
__IM uint32_t | CHREQSTATUS |
__IM uint32_t | CHSREQSTATUS |
__OM uint32_t | CHSWREQ |
__OM uint32_t | CHUSEBURSTC |
__IOM uint32_t | CHUSEBURSTS |
__IM uint32_t | CHWAITSTATUS |
__OM uint32_t | CONFIG |
__IOM uint32_t | CTRLBASE |
__IOM uint32_t | ERRORC |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
uint32_t | RESERVED0 [3] |
uint32_t | RESERVED1 [880] |
uint32_t | RESERVED2 [1] |
uint32_t | RESERVED3 [121] |
uint32_t | RESERVED4 [60] |
__IM uint32_t | STATUS |
Field Documentation
__IM uint32_t DMA_TypeDef::ALTCTRLBASE |
Channel Alternate Control Data Base Pointer Register
Definition at line 52
of file efm32hg_dma.h
.
DMA_CH_TypeDef DMA_TypeDef::CH[6] |
Channel registers
Definition at line 80
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CHALTC |
Channel Alternate Clear Register
Definition at line 62
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::CHALTS |
Channel Alternate Set Register
Definition at line 61
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CHENC |
Channel Enable Clear Register
Definition at line 60
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::CHENS |
Channel Enable Set Register
Definition at line 59
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CHPRIC |
Channel Priority Clear Register
Definition at line 64
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::CHPRIS |
Channel Priority Set Register
Definition at line 63
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CHREQMASKC |
Channel Request Mask Clear Register
Definition at line 58
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::CHREQMASKS |
Channel Request Mask Set Register
Definition at line 57
of file efm32hg_dma.h
.
__IM uint32_t DMA_TypeDef::CHREQSTATUS |
Channel Request Status
Definition at line 69
of file efm32hg_dma.h
.
__IM uint32_t DMA_TypeDef::CHSREQSTATUS |
Channel Single Request Status
Definition at line 71
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CHSWREQ |
Channel Software Request Register
Definition at line 54
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CHUSEBURSTC |
Channel Useburst Clear Register
Definition at line 56
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::CHUSEBURSTS |
Channel Useburst Set Register
Definition at line 55
of file efm32hg_dma.h
.
__IM uint32_t DMA_TypeDef::CHWAITSTATUS |
Channel Wait on Request Status Register
Definition at line 53
of file efm32hg_dma.h
.
__OM uint32_t DMA_TypeDef::CONFIG |
DMA Configuration Register
Definition at line 50
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::CTRLBASE |
Channel Control Data Base Pointer Register
Definition at line 51
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::ERRORC |
Bus Error Clear Register
Definition at line 66
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::IEN |
Interrupt Enable register
Definition at line 77
of file efm32hg_dma.h
.
__IM uint32_t DMA_TypeDef::IF |
Interrupt Flag Register
Definition at line 74
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 76
of file efm32hg_dma.h
.
__IOM uint32_t DMA_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 75
of file efm32hg_dma.h
.
uint32_t DMA_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 65
of file efm32hg_dma.h
.
uint32_t DMA_TypeDef::RESERVED1[880] |
Reserved for future use
Definition at line 68
of file efm32hg_dma.h
.
uint32_t DMA_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 70
of file efm32hg_dma.h
.
uint32_t DMA_TypeDef::RESERVED3[121] |
Reserved for future use
Definition at line 73
of file efm32hg_dma.h
.
uint32_t DMA_TypeDef::RESERVED4[60] |
Reserved registers
Definition at line 79
of file efm32hg_dma.h
.
__IM uint32_t DMA_TypeDef::STATUS |
DMA Status Registers
Definition at line 49
of file efm32hg_dma.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/
efm32hg_dma.h