PCNT_TypeDef Struct ReferenceDevices > EFM32HG_PCNT

Definition at line 48 of file efm32hg_pcnt.h .

Data Fields

__IOM uint32_t AUXCNT
__IOM uint32_t CMD
__IM uint32_t CNT
__IOM uint32_t CTRL
__IOM uint32_t FREEZE
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t INPUT
uint32_t RESERVED0 [1]
__IOM uint32_t ROUTE
__IM uint32_t STATUS
__IM uint32_t SYNCBUSY
__IM uint32_t TOP
__IOM uint32_t TOPB

Field Documentation

__IOM uint32_t PCNT_TypeDef::AUXCNT

Auxiliary Counter Value Register

Definition at line 65 of file efm32hg_pcnt.h .

Referenced by PCNT_AuxCounterGet() .

__IOM uint32_t PCNT_TypeDef::CMD

Command Register

Definition at line 50 of file efm32hg_pcnt.h .

Referenced by PCNT_CounterTopSet() , PCNT_Init() , and PCNT_TopSet() .

__IM uint32_t PCNT_TypeDef::CNT

Counter Value Register

Definition at line 52 of file efm32hg_pcnt.h .

Referenced by PCNT_CounterGet() .

__IOM uint32_t PCNT_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32hg_pcnt.h .

Referenced by PCNT_CounterReset() , PCNT_CounterTopSet() , PCNT_Enable() , PCNT_Init() , PCNT_Reset() , and PCNT_TCCConfiguration() .

__IOM uint32_t PCNT_TypeDef::FREEZE

Freeze Register

Definition at line 61 of file efm32hg_pcnt.h .

Referenced by PCNT_FreezeEnable() .

__IOM uint32_t PCNT_TypeDef::IEN

Interrupt Enable Register

Definition at line 58 of file efm32hg_pcnt.h .

Referenced by PCNT_IntDisable() , PCNT_IntEnable() , PCNT_IntGetEnabled() , and PCNT_Reset() .

__IM uint32_t PCNT_TypeDef::IF

Interrupt Flag Register

Definition at line 55 of file efm32hg_pcnt.h .

Referenced by PCNT_IntGet() , and PCNT_IntGetEnabled() .

__IOM uint32_t PCNT_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 57 of file efm32hg_pcnt.h .

Referenced by PCNT_IntClear() , and PCNT_Reset() .

__IOM uint32_t PCNT_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 56 of file efm32hg_pcnt.h .

Referenced by PCNT_IntSet() .

__IOM uint32_t PCNT_TypeDef::INPUT

PCNT Input Register

Definition at line 66 of file efm32hg_pcnt.h .

Referenced by PCNT_Init() , and PCNT_PRSInputEnable() .

uint32_t PCNT_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 64 of file efm32hg_pcnt.h .

__IOM uint32_t PCNT_TypeDef::ROUTE

I/O Routing Register

Definition at line 59 of file efm32hg_pcnt.h .

__IM uint32_t PCNT_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32hg_pcnt.h .

__IM uint32_t PCNT_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 62 of file efm32hg_pcnt.h .

Referenced by PCNT_FreezeEnable() .

__IM uint32_t PCNT_TypeDef::TOP

Top Value Register

Definition at line 53 of file efm32hg_pcnt.h .

Referenced by PCNT_CounterSet() , and PCNT_TopGet() .

__IOM uint32_t PCNT_TypeDef::TOPB

Top Value Buffer Register

Definition at line 54 of file efm32hg_pcnt.h .

Referenced by PCNT_CounterTopSet() , PCNT_Init() , PCNT_TopBufferGet() , PCNT_TopBufferSet() , and PCNT_TopSet() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/ efm32hg_pcnt.h