IDAC_TypeDef Struct ReferenceDevices > EFM32HG_IDAC

Definition at line 48 of file efm32hg_idac.h .

Data Fields

__IOM uint32_t CAL
__IOM uint32_t CTRL
__IOM uint32_t CURPROG
__IOM uint32_t DUTYCONFIG

Field Documentation

__IOM uint32_t IDAC_TypeDef::CAL

Calibration Register

Definition at line 51 of file efm32hg_idac.h .

Referenced by IDAC_RangeSet() , and IDAC_Reset() .

__IOM uint32_t IDAC_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32hg_idac.h .

Referenced by IDAC_Enable() , IDAC_Init() , IDAC_MinimalOutputTransitionMode() , IDAC_OutEnable() , IDAC_RangeSet() , and IDAC_Reset() .

__IOM uint32_t IDAC_TypeDef::CURPROG

Current Programming Register

Definition at line 50 of file efm32hg_idac.h .

Referenced by IDAC_RangeSet() , IDAC_Reset() , and IDAC_StepSet() .

__IOM uint32_t IDAC_TypeDef::DUTYCONFIG

Duty Cycle Configauration Register

Definition at line 52 of file efm32hg_idac.h .

Referenced by IDAC_Reset() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/ efm32hg_idac.h