USB_StringDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB String Descriptor.
Definition at line
496
of file
em_usb.h
.
#include <
em_usb.h
>
Data Fields |
|
| uint8_t | len |
| char16_t | name [] |
| uint8_t | type |
Field Documentation
| uint8_t USB_StringDescriptor_TypeDef::len |
Size of this descriptor in bytes.
Definition at line
497
of file
em_usb.h
.
| char16_t USB_StringDescriptor_TypeDef::name[] |
The string encoded with UTF-16LE UNICODE charset.
Definition at line
499
of file
em_usb.h
.
| uint8_t USB_StringDescriptor_TypeDef::type |
Constant STRING Descriptor Type.
Definition at line
498
of file
em_usb.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
em_usb.h