CMUEMLIB
Detailed Description
Clock management unit (CMU) Peripheral API.
This module contains functions to control the CMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The CMU controls oscillators and clocks.
Data Structures | |
struct | CMU_HFXOInit_TypeDef |
struct | CMU_LFXOInit_TypeDef |
Macros | |
#define | CMU_AUXHFRCO_MAX cmuAUXHFRCOFreq_38M0Hz |
#define | CMU_AUXHFRCO_MIN cmuAUXHFRCOFreq_1M0Hz |
#define | CMU_HFRCO_MAX cmuHFRCOFreq_38M0Hz |
#define | CMU_HFRCO_MIN cmuHFRCOFreq_1M0Hz |
#define | CMU_HFXOINIT_DEFAULT |
#define | CMU_HFXOINIT_EXTERNAL_CLOCK |
#define | CMU_LFXOINIT_DEFAULT |
#define | CMU_LFXOINIT_EXTERNAL_CLOCK |
#define | cmuClkDiv_1 1 |
#define | cmuClkDiv_1024 1024 |
#define | cmuClkDiv_128 128 |
#define | cmuClkDiv_16 16 |
#define | cmuClkDiv_16384 16384 |
#define | cmuClkDiv_2 2 |
#define | cmuClkDiv_2048 2048 |
#define | cmuClkDiv_256 256 |
#define | cmuClkDiv_32 32 |
#define | cmuClkDiv_32768 32768 |
#define | cmuClkDiv_4 4 |
#define | cmuClkDiv_4096 4096 |
#define | cmuClkDiv_512 512 |
#define | cmuClkDiv_64 64 |
#define | cmuClkDiv_8 8 |
#define | cmuClkDiv_8192 8192 |
Typedefs | |
typedef uint32_t | CMU_ClkDiv_TypeDef |
typedef uint32_t | CMU_ClkPresc_TypeDef |
Functions | |
CMU_AUXHFRCOFreq_TypeDef | CMU_AUXHFRCOBandGet (void) |
Get current AUXHFRCO frequency. | |
void | CMU_AUXHFRCOBandSet (CMU_AUXHFRCOFreq_TypeDef setFreq) |
Set AUXHFRCO calibration for the selected target frequency. | |
static uint32_t | CMU_AUXHFRCODevinfoGet (CMU_AUXHFRCOFreq_TypeDef freq) |
Get the AUXHFRCO frequency calibration word in DEVINFO. | |
__STATIC_INLINE CMU_AUXHFRCOFreq_TypeDef | CMU_AUXHFRCOFreqGet (void) |
Get current AUXHFRCO frequency. | |
__STATIC_INLINE void | CMU_AUXHFRCOFreqSet (CMU_AUXHFRCOFreq_TypeDef setFreq) |
Set AUXHFRCO calibration for the selected target frequency. | |
uint32_t | CMU_Calibrate (uint32_t HFCycles, CMU_Osc_TypeDef reference) |
Calibrate clock. | |
void | CMU_CalibrateConfig (uint32_t downCycles, CMU_Osc_TypeDef downSel, CMU_Osc_TypeDef upSel) |
Configure clock calibration. | |
__STATIC_INLINE void | CMU_CalibrateCont (bool enable) |
Configures continuous calibration mode. | |
uint32_t | CMU_CalibrateCountGet (void) |
Get calibration count register. | |
__STATIC_INLINE void | CMU_CalibrateStart (void) |
Starts calibration. | |
__STATIC_INLINE void | CMU_CalibrateStop (void) |
Stop the calibration counters. | |
CMU_ClkDiv_TypeDef | CMU_ClockDivGet (CMU_Clock_TypeDef clock) |
Get clock divisor/prescaler. | |
void | CMU_ClockDivSet (CMU_Clock_TypeDef clock, CMU_ClkDiv_TypeDef div) |
Set clock divisor/prescaler. | |
void | CMU_ClockEnable (CMU_Clock_TypeDef clock, bool enable) |
Enable/disable a clock. | |
uint32_t | CMU_ClockFreqGet (CMU_Clock_TypeDef clock) |
Get clock frequency for a clock point. | |
uint32_t | CMU_ClockPrescGet (CMU_Clock_TypeDef clock) |
Get clock prescaler. | |
void | CMU_ClockPrescSet (CMU_Clock_TypeDef clock, CMU_ClkPresc_TypeDef presc) |
Set clock prescaler. | |
CMU_Select_TypeDef | CMU_ClockSelectGet (CMU_Clock_TypeDef clock) |
Get currently selected reference clock used for a clock branch. | |
void | CMU_ClockSelectSet (CMU_Clock_TypeDef clock, CMU_Select_TypeDef ref) |
Select reference clock/oscillator used for a clock branch. | |
__STATIC_INLINE uint32_t | CMU_DivToLog2 (CMU_ClkDiv_TypeDef div) |
Convert dividend to logarithmic value. Only works for even numbers equal to 2^n. | |
void | CMU_FreezeEnable (bool enable) |
CMU low frequency register synchronization freeze control. | |
CMU_HFRCOFreq_TypeDef | CMU_HFRCOBandGet (void) |
Get current HFRCO frequency. | |
void | CMU_HFRCOBandSet (CMU_HFRCOFreq_TypeDef setFreq) |
Set HFRCO calibration for the selected target frequency. | |
static uint32_t | CMU_HFRCODevinfoGet (CMU_HFRCOFreq_TypeDef freq) |
Get the HFRCO frequency calibration word in DEVINFO. | |
__STATIC_INLINE CMU_HFRCOFreq_TypeDef | CMU_HFRCOFreqGet (void) |
Get current HFRCO frequency. | |
__STATIC_INLINE void | CMU_HFRCOFreqSet (CMU_HFRCOFreq_TypeDef setFreq) |
Set HFRCO calibration for the selected target frequency. | |
void | CMU_HFXOAutostartEnable (uint32_t userSel, bool enEM0EM1Start, bool enEM0EM1StartSel) |
Enable or disable HFXO autostart. | |
void | CMU_HFXOInit (const CMU_HFXOInit_TypeDef *hfxoInit) |
Set HFXO control registers. | |
__STATIC_INLINE void | CMU_IntClear (uint32_t flags) |
Clear one or more pending CMU interrupts. | |
__STATIC_INLINE void | CMU_IntDisable (uint32_t flags) |
Disable one or more CMU interrupts. | |
__STATIC_INLINE void | CMU_IntEnable (uint32_t flags) |
Enable one or more CMU interrupts. | |
__STATIC_INLINE uint32_t | CMU_IntGet (void) |
Get pending CMU interrupts. | |
__STATIC_INLINE uint32_t | CMU_IntGetEnabled (void) |
Get enabled and pending CMU interrupt flags. | |
__STATIC_INLINE void | CMU_IntSet (uint32_t flags) |
Set one or more pending CMU interrupts. | |
uint32_t | CMU_LCDClkFDIVGet (void) |
Get the LCD framerate divisor (FDIV) setting. | |
void | CMU_LCDClkFDIVSet (uint32_t div) |
Set the LCD framerate divisor (FDIV) setting. | |
void | CMU_LFXOInit (const CMU_LFXOInit_TypeDef *lfxoInit) |
Set LFXO control registers. | |
__STATIC_INLINE void | CMU_Lock (void) |
Lock the CMU in order to protect some of its registers against unintended modification. | |
__STATIC_INLINE uint32_t | CMU_Log2ToDiv (uint32_t log2) |
Convert logarithm of 2 prescaler to division factor. | |
void | CMU_OscillatorEnable (CMU_Osc_TypeDef osc, bool enable, bool wait) |
Enable/disable oscillator. | |
uint32_t | CMU_OscillatorTuningGet (CMU_Osc_TypeDef osc) |
Get oscillator frequency tuning setting. | |
bool | CMU_OscillatorTuningOptimize (CMU_Osc_TypeDef osc, CMU_HFXOTuningMode_TypeDef mode, bool wait) |
Start and optionally wait for oscillator tuning optimization. | |
void | CMU_OscillatorTuningSet (CMU_Osc_TypeDef osc, uint32_t val) |
Set the oscillator frequency tuning control. | |
bool | CMU_OscillatorTuningWait (CMU_Osc_TypeDef osc, CMU_HFXOTuningMode_TypeDef mode) |
Wait for oscillator tuning optimization. | |
bool | CMU_PCNTClockExternalGet (unsigned int instance) |
Determine if currently selected PCNTn clock used is external or LFBCLK. | |
void | CMU_PCNTClockExternalSet (unsigned int instance, bool external) |
Select PCNTn clock. | |
__STATIC_INLINE uint32_t | CMU_PrescToLog2 (CMU_ClkPresc_TypeDef presc) |
Convert prescaler dividend to logarithmic value. Only works for even numbers equal to 2^n. | |
__STATIC_INLINE void | CMU_Unlock (void) |
Unlock the CMU so that writing to locked registers again is possible. | |
void | CMU_UpdateWaitStates (uint32_t freq, int vscale) |
Macro Definition Documentation
#define CMU_HFXOINIT_DEFAULT |
Default HFXO initialization values for Platform 2 devices which contain a separate HFXOCTRL register.
Definition at line 1456
of file em_cmu.h
.
#define CMU_HFXOINIT_EXTERNAL_CLOCK |
Definition at line 1494
of file em_cmu.h
.
#define CMU_LFXOINIT_DEFAULT |
Default LFXO initialization values for platform 2 devices which contain a separate LFXOCTRL register.
Definition at line 1363
of file em_cmu.h
.
#define CMU_LFXOINIT_EXTERNAL_CLOCK |
Definition at line 1370
of file em_cmu.h
.
#define cmuClkDiv_1 1 |
Clock divisors. These values are valid for prescalers. Divide clock by 1.
Definition at line 177
of file em_cmu.h
.
Referenced by CAPLESENSE_setupCMU(), CMU_ClockDivGet(), CMU_ClockDivSet(), and RETARGET_SerialInit().
#define cmuClkDiv_1024 1024 |
Divide clock by 1024.
Definition at line 187
of file em_cmu.h
.
#define cmuClkDiv_128 128 |
Divide clock by 128.
Definition at line 184
of file em_cmu.h
.
Referenced by CMU_ClockDivSet(), and CMU_LCDClkFDIVSet().
#define cmuClkDiv_16 16 |
Divide clock by 16.
Definition at line 181
of file em_cmu.h
.
Referenced by CMU_ClockDivGet(), CMU_ClockDivSet(), and CMU_ClockFreqGet().
#define cmuClkDiv_16384 16384 |
Divide clock by 16384.
Definition at line 191
of file em_cmu.h
.
#define cmuClkDiv_2 2 |
Divide clock by 2.
Definition at line 178
of file em_cmu.h
.
#define cmuClkDiv_2048 2048 |
Divide clock by 2048.
Definition at line 188
of file em_cmu.h
.
#define cmuClkDiv_256 256 |
#define cmuClkDiv_32 32 |
Divide clock by 32.
Definition at line 182
of file em_cmu.h
.
#define cmuClkDiv_32768 32768 |
#define cmuClkDiv_4 4 |
Divide clock by 4.
Definition at line 179
of file em_cmu.h
.
#define cmuClkDiv_4096 4096 |
Divide clock by 4096.
Definition at line 189
of file em_cmu.h
.
#define cmuClkDiv_512 512 |
#define cmuClkDiv_64 64 |
Divide clock by 64.
Definition at line 183
of file em_cmu.h
.
#define cmuClkDiv_8 8 |
#define cmuClkDiv_8192 8192 |
Divide clock by 8192.
Definition at line 190
of file em_cmu.h
.
Typedef Documentation
typedef uint32_t CMU_ClkDiv_TypeDef |
Clock divider configuration
Definition at line 195
of file em_cmu.h
.
typedef uint32_t CMU_ClkPresc_TypeDef |
Clockprescaler configuration
Definition at line 199
of file em_cmu.h
.
Enumeration Type Documentation
AUX High frequency RCO bands
Definition at line 296
of file em_cmu.h
.
enum CMU_Clock_TypeDef |
Clock points in CMU. Please refer to CMU overview in reference manual.
Definition at line 326
of file em_cmu.h
.
High frequency system RCO bands
Definition at line 255
of file em_cmu.h
.
enum CMU_Osc_TypeDef |
Oscillator types.
Definition at line 1236
of file em_cmu.h
.
enum CMU_OscMode_TypeDef |
enum CMU_Select_TypeDef |
Selectable clock sources.
Definition at line 1261
of file em_cmu.h
.
Function Documentation
CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOBandGet | ( | void |
| ) |
Get current AUXHFRCO frequency.
- Returns
- AUXHFRCO frequency
Definition at line 1376
of file em_cmu.c
.
Referenced by CMU_AUXHFRCOFreqGet().
void CMU_AUXHFRCOBandSet | ( | CMU_AUXHFRCOFreq_TypeDef | setFreq | ) |
Set AUXHFRCO calibration for the selected target frequency.
- Parameters
-
[in] setFreq
AUXHFRCO frequency to set
Definition at line 1390
of file em_cmu.c
.
References _CMU_AUXHFRCOCTRL_CLKDIV_MASK, _CMU_SYNCBUSY_AUXHFRCOBSY_SHIFT, BUS_RegBitRead(), CMU, CMU_AUXHFRCOCTRL_CLKDIV_DIV1, CMU_AUXHFRCOCTRL_CLKDIV_DIV2, CMU_AUXHFRCOCTRL_CLKDIV_DIV4, CMU_AUXHFRCODevinfoGet(), cmuAUXHFRCOFreq_1M0Hz, cmuAUXHFRCOFreq_2M0Hz, and cmuAUXHFRCOFreq_4M0Hz.
Referenced by CMU_AUXHFRCOFreqSet().
|
static |
Get the AUXHFRCO frequency calibration word in DEVINFO.
- Parameters
-
[in] freq
Frequency in Hz
- Returns
- AUXHFRCO calibration word for a given frequency
Definition at line 1323
of file em_cmu.c
.
References cmuAUXHFRCOFreq_13M0Hz, cmuAUXHFRCOFreq_16M0Hz, cmuAUXHFRCOFreq_19M0Hz, cmuAUXHFRCOFreq_1M0Hz, cmuAUXHFRCOFreq_26M0Hz, cmuAUXHFRCOFreq_2M0Hz, cmuAUXHFRCOFreq_32M0Hz, cmuAUXHFRCOFreq_38M0Hz, cmuAUXHFRCOFreq_4M0Hz, cmuAUXHFRCOFreq_7M0Hz, and DEVINFO.
Referenced by CMU_AUXHFRCOBandSet().
__STATIC_INLINE CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOFreqGet | ( | void |
| ) |
Get current AUXHFRCO frequency.
- Deprecated:
- Deprecated function. New code should use CMU_AUXHFRCOBandGet().
- Returns
- AUXHFRCO frequency
Definition at line 1932
of file em_cmu.h
.
References CMU_AUXHFRCOBandGet().
__STATIC_INLINE void CMU_AUXHFRCOFreqSet | ( | CMU_AUXHFRCOFreq_TypeDef | setFreq | ) |
Set AUXHFRCO calibration for the selected target frequency.
- Deprecated:
- Deprecated function. New code should use CMU_AUXHFRCOBandSet().
- Parameters
-
[in] setFreq
AUXHFRCO frequency to set
Definition at line 1947
of file em_cmu.h
.
References CMU_AUXHFRCOBandSet().
uint32_t CMU_Calibrate | ( | uint32_t | HFCycles, |
CMU_Osc_TypeDef | reference |
||
) |
Calibrate clock.
Run a calibration for HFCLK against a selectable reference clock. Please refer to the reference manual, CMU chapter, for further details.
- Note
- This function will not return until calibration measurement is completed.
- Parameters
-
[in] HFCycles
The number of HFCLK cycles to run calibration. Increasing this number increases precision, but the calibration will take more time. [in] ref
The reference clock used to compare HFCLK with.
- Returns
- The number of ticks the reference clock after HFCycles ticks on the HF clock.
Definition at line 1451
of file em_cmu.c
.
References _CMU_CALCNT_CALCNT_MASK, _CMU_CALCNT_CALCNT_SHIFT, _CMU_STATUS_CALRDY_SHIFT, BUS_RegBitRead(), CMU, CMU_CALCTRL_UPSEL_AUXHFRCO, CMU_CALCTRL_UPSEL_HFRCO, CMU_CALCTRL_UPSEL_HFXO, CMU_CALCTRL_UPSEL_LFRCO, CMU_CALCTRL_UPSEL_LFXO, CMU_CMD_CALSTART, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.
void CMU_CalibrateConfig | ( | uint32_t | downCycles, |
CMU_Osc_TypeDef | downSel, |
||
CMU_Osc_TypeDef | upSel |
||
) |
Configure clock calibration.
Configure a calibration for a selectable clock source against another selectable reference clock. Refer to the reference manual, CMU chapter, for further details.
- Note
- After configuration, a call to CMU_CalibrateStart() is required, and the resulting calibration value can be read out with the CMU_CalibrateCountGet() function call.
- Parameters
-
[in] downCycles
The number of downSel clock cycles to run calibration. Increasing this number increases precision, but the calibration will take more time. [in] downSel
The clock which will be counted down downCycles [in] upSel
The reference clock, the number of cycles generated by this clock will be counted and added up, the result can be given with the CMU_CalibrateCountGet() function call.
Definition at line 1534
of file em_cmu.c
.
References _CMU_CALCNT_CALCNT_MASK, _CMU_CALCNT_CALCNT_SHIFT, _CMU_CALCTRL_DOWNSEL_MASK, _CMU_CALCTRL_UPSEL_MASK, CMU, CMU_CALCTRL_DOWNSEL_AUXHFRCO, CMU_CALCTRL_DOWNSEL_HFRCO, CMU_CALCTRL_DOWNSEL_HFXO, CMU_CALCTRL_DOWNSEL_LFRCO, CMU_CALCTRL_DOWNSEL_LFXO, CMU_CALCTRL_UPSEL_AUXHFRCO, CMU_CALCTRL_UPSEL_HFRCO, CMU_CALCTRL_UPSEL_HFXO, CMU_CALCTRL_UPSEL_LFRCO, CMU_CALCTRL_UPSEL_LFXO, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, and cmuOsc_LFXO.
__STATIC_INLINE void CMU_CalibrateCont | ( | bool | enable | ) |
Configures continuous calibration mode.
- Parameters
-
[in] enable
If true, enables continuous calibration, if false disables continuous calibrartion
Definition at line 1662
of file em_cmu.h
.
References _CMU_CALCTRL_CONT_SHIFT, BUS_RegBitWrite(), and CMU.
uint32_t CMU_CalibrateCountGet | ( | void |
| ) |
Get calibration count register.
- Note
- If continuous calibrartion mode is active, calibration busy will almost always be off, and we just need to read the value, where the normal case would be that this function call has been triggered by the CALRDY interrupt flag.
- Returns
- Calibration count, the number of UPSEL clocks (see CMU_CalibrateConfig()) in the period of DOWNSEL oscillator clock cycles configured by a previous write operation to CMU->CALCNT
Definition at line 1630
of file em_cmu.c
.
References _CMU_CALCTRL_CONT_SHIFT, _CMU_STATUS_CALRDY_SHIFT, BUS_RegBitRead(), and CMU.
__STATIC_INLINE void CMU_CalibrateStart | ( | void |
| ) |
Starts calibration.
- Note
- This call is usually invoked after CMU_CalibrateConfig() and possibly CMU_CalibrateCont()
Definition at line 1675
of file em_cmu.h
.
References CMU, and CMU_CMD_CALSTART.
CMU_ClkDiv_TypeDef CMU_ClockDivGet | ( | CMU_Clock_TypeDef | clock | ) |
Get clock divisor/prescaler.
- Parameters
-
[in] clock
Clock point to get divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. Please refer to CMU overview in reference manual.
- Returns
- The current clock point divisor/prescaler. 1 is returned if
clock
specifies a clock point without a divisor/prescaler.
Definition at line 1665
of file em_cmu.c
.
References _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, CMU, CMU_ClockPrescGet(), CMU_DivToLog2(), CMU_Log2ToDiv(), cmuClkDiv_1, cmuClkDiv_16, cmuClock_LETIMER0, and cmuClock_LEUART0.
Referenced by UDELAY_Calibrate().
void CMU_ClockDivSet | ( | CMU_Clock_TypeDef | clock, |
CMU_ClkDiv_TypeDef | div |
||
) |
Set clock divisor/prescaler.
- Note
- If setting a LF clock prescaler, synchronization into the low frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. Please refer to CMU_FreezeEnable() for a suggestion on how to reduce stalling time in some use cases.
- Parameters
-
[in] clock
Clock point to set divisor/prescaler for. Notice that not all clock points have a divisor/prescaler, please refer to CMU overview in the reference manual. [in] div
The clock divisor to use (<= cmuClkDiv_512).
Definition at line 1793
of file em_cmu.c
.
References _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, CMU, CMU_ClockPrescSet(), CMU_DivToLog2(), CMU_SYNCBUSY_LFAPRESC0, CMU_SYNCBUSY_LFBPRESC0, cmuClkDiv_1, cmuClkDiv_128, cmuClkDiv_16, cmuClkDiv_32768, cmuClkDiv_512, cmuClkDiv_8, cmuClock_LETIMER0, cmuClock_LEUART0, SystemCoreClockGet(), and SystemHFClockGet().
Referenced by CAPLESENSE_setupCMU(), RETARGET_SerialInit(), RTCDRV_Init(), SegmentLCD_Init(), UARTDRV_InitLeuart(), and UDELAY_Calibrate().
void CMU_ClockEnable | ( | CMU_Clock_TypeDef | clock, |
bool | enable |
||
) |
Enable/disable a clock.
In general, module clocking is disabled after a reset. If a module clock is disabled, the registers of that module are not accessible and reading from such registers may return undefined values. Writing to registers of clock disabled modules have no effect. One should normally avoid accessing module registers of a module with a disabled clock.
- Note
- If enabling/disabling a LF clock, synchronization into the low frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. Please refer to CMU_FreezeEnable() for a suggestion on how to reduce stalling time in some use cases.
- Parameters
-
[in] clock
The clock to enable/disable. Notice that not all defined clock points have separate enable/disable control, please refer to CMU overview in reference manual. [in] enable
- true - enable specified clock.
- false - disable specified clock.
Definition at line 1998
of file em_cmu.c
.
References BUS_RegBitWrite(), CMU, CMU_ClockFreqGet(), CMU_SYNCBUSY_LFACLKEN0, CMU_SYNCBUSY_LFBCLKEN0, CMU_SYNCBUSY_LFECLKEN0, and cmuClock_HFLE.
Referenced by adcInit(), BOARD_init(), BSP_BccDeInit(), BSP_BccInit(), BSP_BusControlModeSet(), BSP_EbiInit(), BSP_initBoard(), BSP_McuBoard_Init(), CAPLESENSE_setupCMU(), CAPSENSE_Init(), DMADRV_DeInit(), ezradio_hal_GpioInit(), I2CSPM_Init(), ICM20648_spiInit(), LDMA_DeInit(), LDMA_Init(), MIC_init(), MICROSD_Init(), MICROSD_PowerOff(), MICROSD_PowerOn(), MSDD_Init(), RETARGET_SerialInit(), RTCDRV_DeInit(), RTCDRV_Init(), SegmentLCD_Disable(), SegmentLCD_Init(), setupOscillators(), SPI_TFT_Init(), SPIDRV_DeInit(), SPIDRV_Init(), TOUCH_Init(), UARTDRV_DeInit(), UARTDRV_InitLeuart(), UARTDRV_InitUart(), UDELAY_Calibrate(), USTIMER_DeInit(), USTIMER_Init(), VDDCHECK_Disable(), and VDDCHECK_Init().
uint32_t CMU_ClockFreqGet | ( | CMU_Clock_TypeDef | clock | ) |
Get clock frequency for a clock point.
- Parameters
-
[in] clock
Clock point to fetch frequency for.
- Returns
- The current frequency in Hz.
Definition at line 2117
of file em_cmu.c
.
References _CMU_HFCOREPRESC_PRESC_MASK, _CMU_HFCOREPRESC_PRESC_SHIFT, _CMU_HFEXPPRESC_PRESC_MASK, _CMU_HFEXPPRESC_PRESC_SHIFT, _CMU_HFPERPRESC_PRESC_MASK, _CMU_HFPERPRESC_PRESC_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, CMU, CMU_DivToLog2(), CMU_Log2ToDiv(), cmuClkDiv_16, cmuClock_LFA, cmuClock_LFB, cmuClock_LFE, SystemCoreClockGet(), and SystemHFClockGet().
Referenced by ADC_PrescaleCalc(), ADC_TimebaseCalc(), BSP_TraceProfilerSetup(), CMU_ClockEnable(), CMU_ClockPrescSet(), CMU_ClockSelectSet(), CMU_HFRCOBandSet(), I2C_BusFreqGet(), I2C_BusFreqSet(), LEUART_BaudrateGet(), LEUART_BaudrateSet(), MIC_init(), MSC_Init(), UARTDRV_InitLeuart(), USART_BaudrateAsyncSet(), USART_BaudrateGet(), USART_BaudrateSyncSet(), USTIMER_Init(), and UTIL_init().
uint32_t CMU_ClockPrescGet | ( | CMU_Clock_TypeDef | clock | ) |
Get clock prescaler.
- Parameters
-
[in] clock
Clock point to get the prescaler for. Notice that not all clock points have a prescaler. Please refer to CMU overview in reference manual.
- Returns
- The prescaler value of the current clock point. 0 is returned if
clock
specifies a clock point without a prescaler.
Definition at line 2356
of file em_cmu.c
.
References _CMU_HFCOREPRESC_PRESC_MASK, _CMU_HFCOREPRESC_PRESC_SHIFT, _CMU_HFEXPPRESC_PRESC_MASK, _CMU_HFEXPPRESC_PRESC_SHIFT, _CMU_HFPERPRESC_PRESC_MASK, _CMU_HFPERPRESC_PRESC_SHIFT, _CMU_HFPRESC_HFCLKLEPRESC_MASK, _CMU_HFPRESC_HFCLKLEPRESC_SHIFT, _CMU_HFPRESC_PRESC_MASK, _CMU_HFPRESC_PRESC_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, _CMU_LFEPRESC0_RTCC_DIV1, CMU, CMU_Log2ToDiv(), cmuClock_ADC0ASYNC, cmuClock_LETIMER0, cmuClock_LEUART0, and cmuClock_RTCC.
Referenced by CMU_ClockDivGet().
void CMU_ClockPrescSet | ( | CMU_Clock_TypeDef | clock, |
CMU_ClkPresc_TypeDef | presc |
||
) |
Set clock prescaler.
- Note
- If setting a LF clock prescaler, synchronization into the low frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. Please refer to CMU_FreezeEnable() for a suggestion on how to reduce stalling time in some use cases.
- Parameters
-
[in] clock
Clock point to set prescaler for. Notice that not all clock points have a prescaler, please refer to CMU overview in the reference manual. [in] presc
The clock prescaler to use.
Definition at line 2548
of file em_cmu.c
.
References _CMU_HFCOREPRESC_PRESC_MASK, _CMU_HFCOREPRESC_PRESC_SHIFT, _CMU_HFEXPPRESC_PRESC_MASK, _CMU_HFEXPPRESC_PRESC_SHIFT, _CMU_HFPERPRESC_PRESC_MASK, _CMU_HFPERPRESC_PRESC_SHIFT, _CMU_HFPRESC_HFCLKLEPRESC_MASK, _CMU_HFPRESC_HFCLKLEPRESC_SHIFT, _CMU_HFPRESC_PRESC_MASK, _CMU_HFPRESC_PRESC_SHIFT, _CMU_LFAPRESC0_LETIMER0_MASK, _CMU_LFAPRESC0_LETIMER0_SHIFT, _CMU_LFBPRESC0_LEUART0_MASK, _CMU_LFBPRESC0_LEUART0_SHIFT, _CMU_LFEPRESC0_RTCC_MASK, _CMU_LFEPRESC0_RTCC_SHIFT, CMU, CMU_ClockFreqGet(), CMU_PrescToLog2(), CMU_SYNCBUSY_LFAPRESC0, CMU_SYNCBUSY_LFBPRESC0, CMU_SYNCBUSY_LFEPRESC0, cmuClock_ADC0ASYNC, cmuClock_HFLE, cmuClock_LETIMER0, cmuClock_LEUART0, cmuClock_RTCC, and SystemCoreClockGet().
Referenced by CMU_ClockDivSet().
CMU_Select_TypeDef CMU_ClockSelectGet | ( | CMU_Clock_TypeDef | clock | ) |
Get currently selected reference clock used for a clock branch.
- Parameters
-
[in] clock
Clock branch to fetch selected ref. clock for. One of:
- Returns
- Reference clock used for clocking selected branch, cmuSelect_Error if invalid
clock
provided.
Definition at line 2843
of file em_cmu.c
.
References _CMU_ADCCTRL_ADC0CLKSEL_MASK, _CMU_DBGCLKSEL_DBG_MASK, _CMU_HFCLKSTATUS_SELECTED_MASK, _CMU_LFACLKSEL_LFA_MASK, _CMU_LFBCLKSEL_LFB_MASK, _CMU_LFECLKSEL_LFE_MASK, CMU, CMU_ADCCTRL_ADC0CLKSEL_AUXHFRCO, CMU_ADCCTRL_ADC0CLKSEL_DISABLED, CMU_ADCCTRL_ADC0CLKSEL_HFSRCCLK, CMU_ADCCTRL_ADC0CLKSEL_HFXO, CMU_DBGCLKSEL_DBG_AUXHFRCO, CMU_DBGCLKSEL_DBG_HFCLK, CMU_HFCLKSTATUS_SELECTED_HFXO, CMU_HFCLKSTATUS_SELECTED_LFRCO, CMU_HFCLKSTATUS_SELECTED_LFXO, CMU_LFACLKSEL_LFA_LFRCO, CMU_LFACLKSEL_LFA_LFXO, CMU_LFACLKSEL_LFA_ULFRCO, CMU_LFBCLKSEL_LFB_HFCLKLE, CMU_LFBCLKSEL_LFB_LFRCO, CMU_LFBCLKSEL_LFB_LFXO, CMU_LFBCLKSEL_LFB_ULFRCO, CMU_LFECLKSEL_LFE_LFRCO, CMU_LFECLKSEL_LFE_LFXO, CMU_LFECLKSEL_LFE_ULFRCO, cmuSelect_AUXHFRCO, cmuSelect_Disabled, cmuSelect_Error, cmuSelect_HFCLK, cmuSelect_HFCLKLE, cmuSelect_HFRCO, cmuSelect_HFSRCCLK, cmuSelect_HFXO, cmuSelect_LFRCO, cmuSelect_LFXO, and cmuSelect_ULFRCO.
Referenced by CMU_HFRCOBandSet(), CMU_HFXOInit(), CMU_LFXOInit(), and UDELAY_Calibrate().
void CMU_ClockSelectSet | ( | CMU_Clock_TypeDef | clock, |
CMU_Select_TypeDef | ref |
||
) |
Select reference clock/oscillator used for a clock branch.
Notice that if a selected reference is not enabled prior to selecting its use, it will be enabled, and this function will wait for the selected oscillator to be stable. It will however NOT be disabled if another reference clock is selected later.
This feature is particularly important if selecting a new reference clock for the clock branch clocking the core, otherwise the system may halt.
- Parameters
-
[in] clock
Clock branch to select reference clock for. One of: [in] ref
Reference selected for clocking, please refer to reference manual for for details on which reference is available for a specific clock branch.
Definition at line 3341
of file em_cmu.c
.
References _CMU_ADCCTRL_ADC0CLKSEL_AUXHFRCO, _CMU_ADCCTRL_ADC0CLKSEL_DISABLED, _CMU_ADCCTRL_ADC0CLKSEL_HFSRCCLK, _CMU_ADCCTRL_ADC0CLKSEL_HFXO, _CMU_ADCCTRL_ADC0CLKSEL_MASK, _CMU_ADCCTRL_ADC0CLKSEL_SHIFT, _CMU_HFBUSCLKEN0_LE_SHIFT, _CMU_LFACLKSEL_LFA_DISABLED, _CMU_LFACLKSEL_LFA_LFRCO, _CMU_LFACLKSEL_LFA_LFXO, _CMU_LFACLKSEL_LFA_ULFRCO, _CMU_LFBCLKSEL_LFB_HFCLKLE, BUS_RegBitWrite(), CMU, CMU_ClockFreqGet(), CMU_DBGCLKSEL_DBG_AUXHFRCO, CMU_DBGCLKSEL_DBG_HFCLK, CMU_HFCLKSEL_HF_HFRCO, CMU_HFCLKSEL_HF_HFXO, CMU_HFCLKSEL_HF_LFRCO, CMU_HFCLKSEL_HF_LFXO, CMU_HFRCOBandGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuClock_HFLE, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, cmuOsc_LFXO, cmuSelect_AUXHFRCO, cmuSelect_Disabled, cmuSelect_HFCLK, cmuSelect_HFCLKLE, cmuSelect_HFRCO, cmuSelect_HFSRCCLK, cmuSelect_HFXO, cmuSelect_LFRCO, cmuSelect_LFXO, cmuSelect_ULFRCO, SL_FALLTHROUGH, SystemCoreClockGet(), and SystemHFXOClockGet().
Referenced by BSP_BccInit(), BSP_initClocks(), CAPLESENSE_setupCMU(), MIC_init(), RETARGET_SerialInit(), RTCDRV_Init(), SegmentLCD_Init(), setupOscillators(), UARTDRV_InitLeuart(), and UDELAY_Calibrate().
__STATIC_INLINE uint32_t CMU_DivToLog2 | ( | CMU_ClkDiv_TypeDef | div | ) |
Convert dividend to logarithmic value. Only works for even numbers equal to 2^n.
- Parameters
-
[in] div
Unscaled dividend.
- Returns
- Logarithm of 2, as used by fixed prescalers.
Definition at line 1702
of file em_cmu.h
.
Referenced by CMU_ClockDivGet(), CMU_ClockDivSet(), CMU_ClockFreqGet(), and RTCDRV_Init().
void CMU_FreezeEnable | ( | bool | enable | ) |
CMU low frequency register synchronization freeze control.
Some CMU registers requires synchronization into the low frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
Another usage scenario of this feature, is when using an API (such as the CMU API) for modifying several bit fields consecutively in the same register. If freeze mode is enabled during this sequence, stalling can be avoided.
- Note
- When enabling freeze mode, this function will wait for all current ongoing CMU synchronization to LF domain to complete (Normally synchronization will not be in progress.) However for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unecessary stalling.
- Parameters
-
[in] enable
- true - enable freeze, modified registers are not propagated to the LF domain
- false - disable freeze, modified registers are propagated to LF domain
Definition at line 4160
of file em_cmu.c
.
References CMU, and CMU_FREEZE_REGFREEZE.
CMU_HFRCOFreq_TypeDef CMU_HFRCOBandGet | ( | void |
| ) |
Get current HFRCO frequency.
- Returns
- HFRCO frequency
Definition at line 4348
of file em_cmu.c
.
References SystemHfrcoFreq.
Referenced by CMU_ClockSelectSet(), and CMU_HFRCOFreqGet().
void CMU_HFRCOBandSet | ( | CMU_HFRCOFreq_TypeDef | setFreq | ) |
Set HFRCO calibration for the selected target frequency.
- Parameters
-
[in] setFreq
HFRCO frequency to set
Definition at line 4360
of file em_cmu.c
.
References _CMU_HFRCOCTRL_CLKDIV_MASK, _CMU_SYNCBUSY_HFRCOBSY_SHIFT, BUS_RegBitRead(), CMU, CMU_ClockFreqGet(), CMU_ClockSelectGet(), CMU_HFRCOCTRL_CLKDIV_DIV1, CMU_HFRCOCTRL_CLKDIV_DIV2, CMU_HFRCOCTRL_CLKDIV_DIV4, CMU_HFRCODevinfoGet(), cmuClock_HF, cmuClock_HFLE, cmuHFRCOFreq_1M0Hz, cmuHFRCOFreq_2M0Hz, cmuHFRCOFreq_4M0Hz, cmuSelect_HFRCO, SystemCoreClockGet(), and SystemHfrcoFreq.
Referenced by CMU_HFRCOFreqSet().
|
static |
Get the HFRCO frequency calibration word in DEVINFO.
- Parameters
-
[in] freq
Frequency in Hz
- Returns
- HFRCO calibration word for a given frequency
Definition at line 4286
of file em_cmu.c
.
References cmuHFRCOFreq_13M0Hz, cmuHFRCOFreq_16M0Hz, cmuHFRCOFreq_19M0Hz, cmuHFRCOFreq_1M0Hz, cmuHFRCOFreq_26M0Hz, cmuHFRCOFreq_2M0Hz, cmuHFRCOFreq_32M0Hz, cmuHFRCOFreq_38M0Hz, cmuHFRCOFreq_4M0Hz, cmuHFRCOFreq_7M0Hz, and DEVINFO.
Referenced by CMU_HFRCOBandSet().
__STATIC_INLINE CMU_HFRCOFreq_TypeDef CMU_HFRCOFreqGet | ( | void |
| ) |
Get current HFRCO frequency.
- Deprecated:
- Deprecated function. New code should use CMU_HFRCOBandGet().
- Returns
- HFRCO frequency
Definition at line 1900
of file em_cmu.h
.
References CMU_HFRCOBandGet().
__STATIC_INLINE void CMU_HFRCOFreqSet | ( | CMU_HFRCOFreq_TypeDef | setFreq | ) |
Set HFRCO calibration for the selected target frequency.
- Deprecated:
- Deprecated function. New code should use CMU_HFRCOBandSet().
- Parameters
-
[in] setFreq
HFRCO frequency to set
Definition at line 1915
of file em_cmu.h
.
References CMU_HFRCOBandSet().
void CMU_HFXOAutostartEnable | ( | uint32_t | userSel, |
bool | enEM0EM1Start, |
||
bool | enEM0EM1StartSel |
||
) |
Enable or disable HFXO autostart.
- Parameters
-
[in] userSel
Additional user specified enable bit. [in] enEM0EM1Start
If true, HFXO is automatically started upon entering EM0/EM1 entry from EM2/EM3. HFXO selection has to be handled by the user. If false, HFXO is not started automatically when entering EM0/EM1. [in] enEM0EM1StartSel
If true, HFXO is automatically started and immediately selected upon entering EM0/EM1 entry from EM2/EM3. Note that this option stalls the use of HFSRCCLK until HFXO becomes ready. If false, HFXO is not started or selected automatically when entering EM0/EM1.
Definition at line 4569
of file em_cmu.c
.
References _CMU_HFXOCTRL_AUTOSTARTEM0EM1_MASK, _CMU_HFXOCTRL_AUTOSTARTSELEM0EM1_MASK, CMU, CMU_HFXOCTRL_AUTOSTARTEM0EM1, CMU_HFXOCTRL_AUTOSTARTSELEM0EM1, and SystemHFXOClockGet().
Referenced by BSP_initClocks().
void CMU_HFXOInit | ( | const CMU_HFXOInit_TypeDef * | hfxoInit | ) |
Set HFXO control registers.
- Note
- HFXO configuration should be obtained from a configuration tool, app note or xtal datasheet. This function disables the HFXO to ensure a valid state before update.
- Parameters
-
[in] hfxoInit
HFXO setup parameters
Definition at line 4616
of file em_cmu.c
.
References _CMU_HFXOCTRL1_PEAKDETTHR_MASK, _CMU_HFXOCTRL1_PEAKDETTHR_SHIFT, _CMU_HFXOCTRL_LOWPOWER_SHIFT, _CMU_HFXOCTRL_MODE_MASK, _CMU_HFXOSTARTUPCTRL_CTUNE_SHIFT, _CMU_HFXOSTARTUPCTRL_IBTRIMXOCORE_SHIFT, _CMU_HFXOSTEADYSTATECTRL_CTUNE_MASK, _CMU_HFXOSTEADYSTATECTRL_CTUNE_SHIFT, _CMU_HFXOSTEADYSTATECTRL_IBTRIMXOCORE_MASK, _CMU_HFXOSTEADYSTATECTRL_IBTRIMXOCORE_SHIFT, _CMU_HFXOSTEADYSTATECTRL_REGISH_MASK, _CMU_HFXOSTEADYSTATECTRL_REGISH_SHIFT, _CMU_HFXOSTEADYSTATECTRL_REGISHUPPER_MASK, _CMU_HFXOTIMEOUTCTRL_PEAKDETTIMEOUT_SHIFT, _CMU_HFXOTIMEOUTCTRL_SHUNTOPTTIMEOUT_SHIFT, _CMU_HFXOTIMEOUTCTRL_STARTUPTIMEOUT_SHIFT, _CMU_HFXOTIMEOUTCTRL_STEADYTIMEOUT_SHIFT, CMU_HFXOInit_TypeDef::autoSelEm01, CMU_HFXOInit_TypeDef::autoStartEm01, CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup, BUS_RegBitWrite(), CMU, CMU_ClockSelectGet(), CMU_HFXOCTRL_MODE_XTAL, CMU_OscillatorEnable(), cmuClock_HF, cmuOsc_HFXO, cmuOscMode_AcCoupled, cmuOscMode_Crystal, cmuOscMode_External, cmuSelect_HFXO, CMU_HFXOInit_TypeDef::ctuneStartup, CMU_HFXOInit_TypeDef::ctuneSteadyState, CMU_HFXOInit_TypeDef::lowPowerMode, CMU_HFXOInit_TypeDef::mode, CMU_HFXOInit_TypeDef::regIshSteadyState, SystemHFXOClockGet(), CMU_HFXOInit_TypeDef::thresholdPeakDetect, CMU_HFXOInit_TypeDef::timeoutPeakDetect, CMU_HFXOInit_TypeDef::timeoutShuntOptimization, CMU_HFXOInit_TypeDef::timeoutStartup, CMU_HFXOInit_TypeDef::timeoutSteady, CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup, and CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState.
Referenced by BSP_initClocks().
__STATIC_INLINE void CMU_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending CMU interrupts.
- Parameters
-
[in] flags
CMU interrupt sources to clear.
Definition at line 1735
of file em_cmu.h
.
References CMU.
__STATIC_INLINE void CMU_IntDisable | ( | uint32_t | flags | ) |
Disable one or more CMU interrupts.
- Parameters
-
[in] flags
CMU interrupt sources to disable.
Definition at line 1747
of file em_cmu.h
.
References CMU.
__STATIC_INLINE void CMU_IntEnable | ( | uint32_t | flags | ) |
Enable one or more CMU interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using CMU_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] flags
CMU interrupt sources to enable.
Definition at line 1764
of file em_cmu.h
.
References CMU.
__STATIC_INLINE uint32_t CMU_IntGet | ( | void |
| ) |
Get pending CMU interrupts.
- Returns
- CMU interrupt sources pending.
Definition at line 1776
of file em_cmu.h
.
References CMU.
__STATIC_INLINE uint32_t CMU_IntGetEnabled | ( | void |
| ) |
Get enabled and pending CMU interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending and enabled CMU interrupt sources The return value is the bitwise AND of
- the enabled interrupt sources in CMU_IEN and
- the pending interrupt flags CMU_IF
Definition at line 1797
of file em_cmu.h
.
References CMU.
__STATIC_INLINE void CMU_IntSet | ( | uint32_t | flags | ) |
Set one or more pending CMU interrupts.
- Parameters
-
[in] flags
CMU interrupt sources to set to pending.
Definition at line 1812
of file em_cmu.h
.
References CMU.
uint32_t CMU_LCDClkFDIVGet | ( | void |
| ) |
Get the LCD framerate divisor (FDIV) setting.
- Returns
- The LCD framerate divisor.
Definition at line 4754
of file em_cmu.c
.
References CMU.
void CMU_LCDClkFDIVSet | ( | uint32_t | div | ) |
Set the LCD framerate divisor (FDIV) setting.
- Note
- The FDIV field (CMU LCDCTRL register) should only be modified while the LCD module is clock disabled (CMU LFACLKEN0.LCD bit is 0). This function will NOT modify FDIV if the LCD module clock is enabled. Please refer to CMU_ClockEnable() for disabling/enabling LCD clock.
- Parameters
-
[in] div
The FDIV setting to use.
Definition at line 4776
of file em_cmu.c
.
References CMU, and cmuClkDiv_128.
Referenced by SegmentLCD_Init().
void CMU_LFXOInit | ( | const CMU_LFXOInit_TypeDef * | lfxoInit | ) |
Set LFXO control registers.
- Note
- LFXO configuration should be obtained from a configuration tool, app note or xtal datasheet. This function disables the LFXO to ensure a valid state before update.
- Parameters
-
[in] lfxoInit
LFXO setup parameters
Definition at line 4806
of file em_cmu.c
.
References _CMU_LFXOCTRL_GAIN_MASK, _CMU_LFXOCTRL_GAIN_SHIFT, _CMU_LFXOCTRL_MODE_MASK, _CMU_LFXOCTRL_MODE_SHIFT, _CMU_LFXOCTRL_TIMEOUT_MASK, _CMU_LFXOCTRL_TIMEOUT_SHIFT, _CMU_LFXOCTRL_TUNING_MASK, _CMU_LFXOCTRL_TUNING_SHIFT, BUS_RegBitWrite(), BUS_RegMaskedWrite(), CMU, CMU_ClockSelectGet(), CMU_OscillatorEnable(), cmuClock_HF, cmuOsc_LFXO, cmuSelect_LFXO, CMU_LFXOInit_TypeDef::ctune, EMU, CMU_LFXOInit_TypeDef::gain, CMU_LFXOInit_TypeDef::mode, and CMU_LFXOInit_TypeDef::timeout.
Referenced by BSP_initClocks().
__STATIC_INLINE void CMU_Lock | ( | void |
| ) |
Lock the CMU in order to protect some of its registers against unintended modification.
Please refer to the reference manual for CMU registers that will be locked.
- Note
- If locking the CMU registers, they must be unlocked prior to using any CMU API functions modifying CMU registers protected by the lock.
Definition at line 1830
of file em_cmu.h
.
References CMU, and CMU_LOCK_LOCKKEY_LOCK.
Referenced by EMU_EnterEM3().
__STATIC_INLINE uint32_t CMU_Log2ToDiv | ( | uint32_t | log2 | ) |
Convert logarithm of 2 prescaler to division factor.
- Parameters
-
[in] log2
Logarithm of 2, as used by fixed prescalers.
- Returns
- Dividend.
Definition at line 1845
of file em_cmu.h
.
Referenced by CMU_ClockDivGet(), CMU_ClockFreqGet(), CMU_ClockPrescGet(), and CMU_PrescToLog2().
void CMU_OscillatorEnable | ( | CMU_Osc_TypeDef | osc, |
bool | enable, |
||
bool | wait |
||
) |
Enable/disable oscillator.
- Note
- WARNING: When this function is called to disable either cmuOsc_LFXO or cmuOsc_HFXO the LFXOMODE or HFXOMODE fields of the CMU_CTRL register are reset to the reset value. I.e. if external clock sources are selected in either LFXOMODE or HFXOMODE fields, the configuration will be cleared and needs to be reconfigured if needed later.
- Parameters
-
[in] osc
The oscillator to enable/disable. [in] enable
- true - enable specified oscillator.
- false - disable specified oscillator.
[in] wait
Only used if enable
is true.- true - wait for oscillator start-up time to timeout before returning.
- false - do not wait for oscillator start-up time to timeout before returning.
Definition at line 4867
of file em_cmu.c
.
References _CMU_HFXOCTRL_MODE_MASK, _CMU_STATUS_AUXHFRCOENS_SHIFT, _CMU_STATUS_AUXHFRCORDY_SHIFT, _CMU_STATUS_HFRCOENS_SHIFT, _CMU_STATUS_HFRCORDY_SHIFT, _CMU_STATUS_HFXOENS_SHIFT, _CMU_STATUS_HFXORDY_SHIFT, _CMU_STATUS_LFRCOENS_SHIFT, _CMU_STATUS_LFRCORDY_SHIFT, _CMU_STATUS_LFXOENS_SHIFT, _CMU_STATUS_LFXORDY_SHIFT, BUS_RegBitRead(), CMU, CMU_OSCENCMD_AUXHFRCODIS, CMU_OSCENCMD_AUXHFRCOEN, CMU_OSCENCMD_HFRCODIS, CMU_OSCENCMD_HFRCOEN, CMU_OSCENCMD_HFXODIS, CMU_OSCENCMD_HFXOEN, CMU_OSCENCMD_LFRCODIS, CMU_OSCENCMD_LFRCOEN, CMU_OSCENCMD_LFXODIS, CMU_OSCENCMD_LFXOEN, CMU_OscillatorTuningGet(), CMU_OscillatorTuningOptimize(), CMU_OscillatorTuningSet(), CMU_OscillatorTuningWait(), cmuHFXOTuningMode_ShuntCommand, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, cmuOsc_LFRCO, cmuOsc_LFXO, and EMU.
Referenced by BSP_initClocks(), CMU_ClockSelectSet(), CMU_HFXOInit(), CMU_LFXOInit(), DBG_SWOEnable(), setupOscillators(), and UDELAY_Calibrate().
uint32_t CMU_OscillatorTuningGet | ( | CMU_Osc_TypeDef | osc | ) |
Get oscillator frequency tuning setting.
- Parameters
-
[in] osc
Oscillator to get tuning value for, one of: - cmuOsc_LFRCO
- cmuOsc_HFRCO
- cmuOsc_AUXHFRCO
- cmuOsc_HFXO if CMU_HFXOCTRL_PEAKDETSHUNTOPTMODE is defined
- Returns
- The oscillator frequency tuning setting in use.
Definition at line 5045
of file em_cmu.c
.
References _CMU_AUXHFRCOCTRL_TUNING_MASK, _CMU_AUXHFRCOCTRL_TUNING_SHIFT, _CMU_HFRCOCTRL_TUNING_MASK, _CMU_HFRCOCTRL_TUNING_SHIFT, _CMU_HFXOTRIMSTATUS_IBTRIMXOCORE_MASK, _CMU_HFXOTRIMSTATUS_REGISH_MASK, _CMU_LFRCOCTRL_TUNING_MASK, _CMU_LFRCOCTRL_TUNING_SHIFT, CMU, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, and cmuOsc_LFRCO.
Referenced by CMU_OscillatorEnable().
bool CMU_OscillatorTuningOptimize | ( | CMU_Osc_TypeDef | osc, |
CMU_HFXOTuningMode_TypeDef | mode, |
||
bool | wait |
||
) |
Start and optionally wait for oscillator tuning optimization.
- Parameters
-
[in] osc
Oscillator to set tuning value for, one of: [in] mode
Tuning optimization mode. [in] wait
Wait for tuning optimization to complete. true - wait for tuning optimization to complete. false - return without waiting.
- Returns
- Returns false on invalid parameters or oscillator error status.
Definition at line 5289
of file em_cmu.c
.
References CMU, CMU_IFC_HFXOPEAKDETERR, CMU_OscillatorTuningWait(), and cmuOsc_HFXO.
Referenced by CMU_OscillatorEnable().
void CMU_OscillatorTuningSet | ( | CMU_Osc_TypeDef | osc, |
uint32_t | val |
||
) |
Set the oscillator frequency tuning control.
- Note
- Oscillator tuning is done during production, and the tuning value is automatically loaded after a reset. Changing the tuning value from the calibrated value is for more advanced use. Certain oscillators also have build-in tuning optimization.
- Parameters
-
[in] osc
Oscillator to set tuning value for, one of: - cmuOsc_LFRCO
- cmuOsc_HFRCO
- cmuOsc_AUXHFRCO
- cmuOsc_HFXO if PEAKDETSHUNTOPTMODE is available. Note that CMD mode is set.
[in] val
The oscillator frequency tuning setting to use.
Definition at line 5113
of file em_cmu.c
.
References _CMU_AUXHFRCOCTRL_TUNING_MASK, _CMU_AUXHFRCOCTRL_TUNING_SHIFT, _CMU_HFRCOCTRL_TUNING_MASK, _CMU_HFRCOCTRL_TUNING_SHIFT, _CMU_HFXOCTRL_PEAKDETSHUNTOPTMODE_MASK, _CMU_HFXOSTEADYSTATECTRL_IBTRIMXOCORE_MASK, _CMU_HFXOSTEADYSTATECTRL_REGISH_MASK, _CMU_HFXOSTEADYSTATECTRL_REGISH_SHIFT, _CMU_HFXOSTEADYSTATECTRL_REGISHUPPER_MASK, _CMU_LFRCOCTRL_TUNING_MASK, _CMU_LFRCOCTRL_TUNING_SHIFT, _CMU_SYNCBUSY_AUXHFRCOBSY_SHIFT, _CMU_SYNCBUSY_HFRCOBSY_SHIFT, _CMU_SYNCBUSY_LFRCOBSY_SHIFT, BUS_RegBitRead(), CMU, CMU_HFXOCTRL_PEAKDETSHUNTOPTMODE_CMD, CMU_STATUS_HFXOENS, cmuOsc_AUXHFRCO, cmuOsc_HFRCO, cmuOsc_HFXO, and cmuOsc_LFRCO.
Referenced by CMU_OscillatorEnable().
bool CMU_OscillatorTuningWait | ( | CMU_Osc_TypeDef | osc, |
CMU_HFXOTuningMode_TypeDef | mode |
||
) |
Wait for oscillator tuning optimization.
- Parameters
-
[in] osc
Oscillator to set tuning value for, one of: [in] mode
Tuning optimization mode.
- Returns
- Returns false on invalid parameters or oscillator error status.
Definition at line 5223
of file em_cmu.c
.
References _CMU_STATUS_MASK, CMU, CMU_IF_HFXOPEAKDETERR, CMU_STATUS_HFXOPEAKDETRDY, CMU_STATUS_HFXOSHUNTOPTRDY, cmuHFXOTuningMode_PeakShuntCommand, cmuHFXOTuningMode_ShuntCommand, and cmuOsc_HFXO.
Referenced by CMU_OscillatorEnable(), and CMU_OscillatorTuningOptimize().
bool CMU_PCNTClockExternalGet | ( | unsigned int | instance | ) |
Determine if currently selected PCNTn clock used is external or LFBCLK.
- Parameters
-
[in] instance
PCNT instance number to get currently selected clock source for.
- Returns
- true - selected clock is external clock.
- false - selected clock is LFBCLK.
Definition at line 5326
of file em_cmu.c
.
References CMU, and CMU_PCNTCTRL_PCNT0CLKSEL_PCNT0S0.
void CMU_PCNTClockExternalSet | ( | unsigned int | instance, |
bool | external |
||
) |
Select PCNTn clock.
- Parameters
-
[in] instance
PCNT instance number to set selected clock source for. [in] external
Set to true to select external clock, false to select LFBCLK.
Definition at line 5366
of file em_cmu.c
.
References BUS_RegBitWrite(), CMU, and PCNT_COUNT.
Referenced by PCNT_Init(), and PCNT_Reset().
__STATIC_INLINE uint32_t CMU_PrescToLog2 | ( | CMU_ClkPresc_TypeDef | presc | ) |
Convert prescaler dividend to logarithmic value. Only works for even numbers equal to 2^n.
- Parameters
-
[in] presc
Unscaled dividend (dividend = presc + 1).
- Returns
- Logarithm of 2, as used by fixed 2^n prescalers.
Definition at line 1863
of file em_cmu.h
.
References CMU_Log2ToDiv().
Referenced by CMU_ClockPrescSet().