IDAC_Init_TypeDef Struct ReferenceEMLIB > IDAC
IDAC init structure, common for both channels.
       Definition at line
       
        167
       
       of file
       
        em_idac.h
       
       .
      
      
       #include <
       
     
        em_idac.h
       
       >
      
| Data Fields | |
| bool | enable | 
| IDAC_OutMode_TypeDef | outMode | 
| bool | prsEnable | 
| IDAC_PRSSEL_TypeDef | prsSel | 
| bool | sinkEnable | 
Field Documentation
| bool IDAC_Init_TypeDef::enable | 
| IDAC_OutMode_TypeDef IDAC_Init_TypeDef::outMode | 
| bool IDAC_Init_TypeDef::prsEnable | 
Enable Peripheral reflex system (PRS) to control IDAC output. If false, the IDAC output is controlled by writing to IDAC_OUTEN in IDAC_CTRL or by calling IDAC_OutEnable() .
        Definition at line
        
         179
        
        of file
        
         em_idac.h
        
        .
       
Referenced by IDAC_Init() .
| IDAC_PRSSEL_TypeDef IDAC_Init_TypeDef::prsSel | 
        Peripheral reflex system channel selection. Only applicable if
        
         prsEnable
        
        is enabled.
       
        Definition at line
        
         185
        
        of file
        
         em_idac.h
        
        .
       
Referenced by IDAC_Init() .
| bool IDAC_Init_TypeDef::sinkEnable | 
Enable/disable current sink mode.
        Definition at line
        
         188
        
        of file
        
         em_idac.h
        
        .
       
Referenced by IDAC_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_idac.h