GPIO_TypeDef Struct ReferenceDevices > GPIO
GPIO Register Declaration
       Definition at line
       
        49
       
       of file
       
        efr32bg1p_gpio.h
       
       .
      
      
       #include <
       
     
        efr32bg1p_gpio.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | EM4WUEN | 
| __IOM uint32_t | EXTIFALL | 
| __IOM uint32_t | EXTILEVEL | 
| __IOM uint32_t | EXTIPINSELH | 
| __IOM uint32_t | EXTIPINSELL | 
| __IOM uint32_t | EXTIPSELH | 
| __IOM uint32_t | EXTIPSELL | 
| __IOM uint32_t | EXTIRISE | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | INSENSE | 
| __IOM uint32_t | LOCK | 
| GPIO_P_TypeDef | P [6] | 
| uint32_t | RESERVED0 [184] | 
| uint32_t | RESERVED1 [4] | 
| uint32_t | RESERVED2 [2] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IOM uint32_t | ROUTEPEN | 
Field Documentation
| __IOM uint32_t GPIO_TypeDef::EM4WUEN | 
EM4 Wake Up Enable Register
        Definition at line
        
         64
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIFALL | 
External Interrupt Falling Edge Trigger Register
        Definition at line
        
         58
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTILEVEL | 
External Interrupt Level Register
        Definition at line
        
         59
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIPINSELH | 
External Interrupt Pin Select High Register
        Definition at line
        
         56
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIPINSELL | 
External Interrupt Pin Select Low Register
        Definition at line
        
         55
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIPSELH | 
External Interrupt Port Select High Register
        Definition at line
        
         54
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIPSELL | 
External Interrupt Port Select Low Register
        Definition at line
        
         53
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::EXTIRISE | 
External Interrupt Rising Edge Trigger Register
        Definition at line
        
         57
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         63
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IM uint32_t GPIO_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         60
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         62
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         61
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::INSENSE | 
Input Sense Register
        Definition at line
        
         71
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         72
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| GPIO_P_TypeDef GPIO_TypeDef::P[6] | 
Port configuration bits
        Definition at line
        
         50
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| uint32_t GPIO_TypeDef::RESERVED0[184] | 
Reserved for future use
        Definition at line
        
         52
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| uint32_t GPIO_TypeDef::RESERVED1[4] | 
Reserved for future use
        Definition at line
        
         66
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| uint32_t GPIO_TypeDef::RESERVED2[2] | 
Reserved for future use
        Definition at line
        
         70
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         68
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
| __IOM uint32_t GPIO_TypeDef::ROUTEPEN | 
I/O Routing Pin Enable Register
        Definition at line
        
         67
        
        of file
        
         efr32bg1p_gpio.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG1P/Include/
       efr32bg1p_gpio.h