LDMAEMLIB
Detailed Description
Linked Direct Memory Access (LDMA) Peripheral API.
The LDMA API functions provide full support for the LDMA peripheral.
The LDMA supports these DMA transfer types:
- Memory to memory.
- Memory to peripheral.
- Peripheral to memory.
- Peripheral to peripheral.
- Constant value to memory.
The LDMA supports linked lists of DMA descriptors allowing:
- Circular and ping-pong buffer transfers.
- Scatter-gather transfers.
- Looped transfers.
The LDMA has some advanced features:
- Intra-channel synchronization (SYNC), allowing hardware events to pause and restart a DMA sequence.
- Immediate-write (WRI), allowing the DMA to write a constant anywhere in the memory map.
- Complex flow control allowing if-else constructs.
A basic understanding of the LDMA controller is assumed. Please refer to the reference manual for further details. The LDMA examples described in the reference manual are particularly helpful in understanding LDMA operations.
In order to use the DMA controller, the initialization function LDMA_Init() must have been executed once (normally during system init).
DMA transfers are initiated by a call to LDMA_StartTransfer() , the transfer properties are controlled by the contents of LDMA_TransferCfg_t and LDMA_Descriptor_t structure parameters. The LDMA_Descriptor_t structure parameter may be a pointer to an array of descriptors, the descriptors in the array should be linked together as needed.
Transfer and descriptor initialization macros are provided for the most common transfer types. Due to the flexibility of the LDMA peripheral only a small subset of all possible initializer macros are provided, the user should create new one's when needed.
Examples of LDMA usage:
A simple memory to memory transfer:
      
      A linked list of three memory to memory transfers:
     
      
      DMA from serial port peripheral to memory:
     
      
      Ping pong DMA from serial port peripheral to memory:
     
- Note
- The LDMA module does not implement the LDMA interrupt handler. A template for an LDMA IRQ handler is include here as an example.
| Data Structures | |
| union | LDMA_Descriptor_t | 
| DMA descriptor. | |
| struct | LDMA_Init_t | 
| LDMA initialization configuration structure. | |
| struct | LDMA_TransferCfg_t | 
| DMA transfer configuration structure. | |
| Macros | |
| #define | LDMA_DESCRIPTOR_LINKABS_M2M_BYTE (src, dest, count) | 
| DMA descriptor initializer for linked memory to memory byte transfer. | |
| #define | LDMA_DESCRIPTOR_LINKABS_M2M_HALF (src, dest, count) | 
| DMA descriptor initializer for linked memory to memory half-word transfer. | |
| #define | LDMA_DESCRIPTOR_LINKABS_M2M_WORD (src, dest, count) | 
| DMA descriptor initializer for linked memory to memory word transfer. | |
| #define | LDMA_DESCRIPTOR_LINKABS_SYNC (set, clr, matchValue, matchEnable) | 
| DMA descriptor initializer for SYNC transfer. | |
| #define | LDMA_DESCRIPTOR_LINKABS_WRITE (value, address) | 
| DMA descriptor initializer for Immediate WRITE transfer. | |
| #define | LDMA_DESCRIPTOR_LINKREL_M2M_BYTE (src, dest, count, linkjmp) | 
| DMA descriptor initializer for linked memory to memory byte transfer. | |
| #define | LDMA_DESCRIPTOR_LINKREL_M2M_HALF (src, dest, count, linkjmp) | 
| DMA descriptor initializer for linked memory to memory half-word transfer. | |
| #define | LDMA_DESCRIPTOR_LINKREL_M2M_WORD (src, dest, count, linkjmp) | 
| DMA descriptor initializer for linked memory to memory word transfer. | |
| #define | LDMA_DESCRIPTOR_LINKREL_M2P_BYTE (src, dest, count, linkjmp) | 
| DMA descriptor initializer for byte transfers from memory to a peripheral. | |
| #define | LDMA_DESCRIPTOR_LINKREL_P2M_BYTE (src, dest, count, linkjmp) | 
| DMA descriptor initializer for byte transfers from a peripheral to memory. | |
| #define | LDMA_DESCRIPTOR_LINKREL_SYNC (set, clr, matchValue, matchEnable, linkjmp) | 
| DMA descriptor initializer for SYNC transfer. | |
| #define | LDMA_DESCRIPTOR_LINKREL_WRITE (value, address, linkjmp) | 
| DMA descriptor initializer for Immediate WRITE transfer. | |
| #define | LDMA_DESCRIPTOR_SINGLE_M2M_BYTE (src, dest, count) | 
| DMA descriptor initializer for single memory to memory byte transfer. | |
| #define | LDMA_DESCRIPTOR_SINGLE_M2M_HALF (src, dest, count) | 
| DMA descriptor initializer for single memory to memory half-word transfer. | |
| #define | LDMA_DESCRIPTOR_SINGLE_M2M_WORD (src, dest, count) | 
| DMA descriptor initializer for single memory to memory word transfer. | |
| #define | LDMA_DESCRIPTOR_SINGLE_M2P_BYTE (src, dest, count) | 
| DMA descriptor initializer for byte transfers from memory to a peripheral. | |
| #define | LDMA_DESCRIPTOR_SINGLE_P2M_BYTE (src, dest, count) | 
| DMA descriptor initializer for byte transfers from a peripheral to memory. | |
| #define | LDMA_DESCRIPTOR_SINGLE_P2P_BYTE (src, dest, count) | 
| DMA descriptor initializer for byte transfers from a peripheral to a peripheral. | |
| #define | LDMA_DESCRIPTOR_SINGLE_SYNC (set, clr, matchValue, matchEnable) | 
| DMA descriptor initializer for SYNC transfer. | |
| #define | LDMA_DESCRIPTOR_SINGLE_WRITE (value, address) | 
| DMA descriptor initializer for Immediate WRITE transfer. | |
| #define | LDMA_INIT_DEFAULT | 
| Default DMA initialization structure. | |
| #define | LDMA_TRANSFER_CFG_MEMORY () | 
| Generic DMA transfer configuration for memory to memory transfers. | |
| #define | LDMA_TRANSFER_CFG_MEMORY_LOOP (loopCnt) | 
| Generic DMA transfer configuration for looped memory to memory transfers. | |
| #define | LDMA_TRANSFER_CFG_PERIPHERAL (signal) | 
| Generic DMA transfer configuration for memory to/from peripheral transfers. | |
| #define | LDMA_TRANSFER_CFG_PERIPHERAL_LOOP (signal, loopCnt) | 
| Generic DMA transfer configuration for looped memory to/from peripheral transfers. | |
| Enumerations | |
| enum | LDMA_CfgArbSlots_t
         
         { ldmaCfgArbSlotsAs1 = _LDMA_CH_CFG_ARBSLOTS_ONE, ldmaCfgArbSlotsAs2 = _LDMA_CH_CFG_ARBSLOTS_TWO, ldmaCfgArbSlotsAs4 = _LDMA_CH_CFG_ARBSLOTS_FOUR, ldmaCfgArbSlotsAs8 = _LDMA_CH_CFG_ARBSLOTS_EIGHT } | 
| enum | LDMA_CfgDstIncSign_t
         
         { ldmaCfgDstIncSignPos = _LDMA_CH_CFG_DSTINCSIGN_POSITIVE, ldmaCfgDstIncSignNeg = _LDMA_CH_CFG_DSTINCSIGN_NEGATIVE } | 
| enum | LDMA_CfgSrcIncSign_t
         
         { ldmaCfgSrcIncSignPos = _LDMA_CH_CFG_SRCINCSIGN_POSITIVE, ldmaCfgSrcIncSignNeg = _LDMA_CH_CFG_SRCINCSIGN_NEGATIVE } | 
| enum | LDMA_CtrlBlockSize_t
         
         { ldmaCtrlBlockSizeUnit1 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT1, ldmaCtrlBlockSizeUnit2 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT2, ldmaCtrlBlockSizeUnit3 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT3, ldmaCtrlBlockSizeUnit4 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT4, ldmaCtrlBlockSizeUnit6 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT6, ldmaCtrlBlockSizeUnit8 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT8, ldmaCtrlBlockSizeUnit16 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT16, ldmaCtrlBlockSizeUnit32 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT32, ldmaCtrlBlockSizeUnit64 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT64, ldmaCtrlBlockSizeUnit128 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT128, ldmaCtrlBlockSizeUnit256 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT256, ldmaCtrlBlockSizeUnit512 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT512, ldmaCtrlBlockSizeUnit1024 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT1024, ldmaCtrlBlockSizeAll = _LDMA_CH_CTRL_BLOCKSIZE_ALL } | 
| enum | LDMA_CtrlDstAddrMode_t
         
         { ldmaCtrlDstAddrModeAbs = _LDMA_CH_CTRL_DSTMODE_ABSOLUTE, ldmaCtrlDstAddrModeRel = _LDMA_CH_CTRL_DSTMODE_RELATIVE } | 
| enum | LDMA_CtrlDstInc_t
         
         { ldmaCtrlDstIncOne = _LDMA_CH_CTRL_DSTINC_ONE, ldmaCtrlDstIncTwo = _LDMA_CH_CTRL_DSTINC_TWO, ldmaCtrlDstIncFour = _LDMA_CH_CTRL_DSTINC_FOUR, ldmaCtrlDstIncNone = _LDMA_CH_CTRL_DSTINC_NONE } | 
| enum | LDMA_CtrlReqMode_t
         
         { ldmaCtrlReqModeBlock = _LDMA_CH_CTRL_REQMODE_BLOCK, ldmaCtrlReqModeAll = _LDMA_CH_CTRL_REQMODE_ALL } | 
| enum | LDMA_CtrlSize_t
         
         { ldmaCtrlSizeByte = _LDMA_CH_CTRL_SIZE_BYTE, ldmaCtrlSizeHalf = _LDMA_CH_CTRL_SIZE_HALFWORD, ldmaCtrlSizeWord = _LDMA_CH_CTRL_SIZE_WORD } | 
| enum | LDMA_CtrlSrcAddrMode_t
         
         { ldmaCtrlSrcAddrModeAbs = _LDMA_CH_CTRL_SRCMODE_ABSOLUTE, ldmaCtrlSrcAddrModeRel = _LDMA_CH_CTRL_SRCMODE_RELATIVE } | 
| enum | LDMA_CtrlSrcInc_t
         
         { ldmaCtrlSrcIncOne = _LDMA_CH_CTRL_SRCINC_ONE, ldmaCtrlSrcIncTwo = _LDMA_CH_CTRL_SRCINC_TWO, ldmaCtrlSrcIncFour = _LDMA_CH_CTRL_SRCINC_FOUR, ldmaCtrlSrcIncNone = _LDMA_CH_CTRL_SRCINC_NONE } | 
| enum | LDMA_CtrlStructType_t
         
         { ldmaCtrlStructTypeXfer = _LDMA_CH_CTRL_STRUCTTYPE_TRANSFER, ldmaCtrlStructTypeSync = _LDMA_CH_CTRL_STRUCTTYPE_SYNCHRONIZE, ldmaCtrlStructTypeWrite = _LDMA_CH_CTRL_STRUCTTYPE_WRITE } | 
| enum | LDMA_LinkMode_t
         
         { ldmaLinkModeAbs = _LDMA_CH_LINK_LINKMODE_ABSOLUTE, ldmaLinkModeRel = _LDMA_CH_LINK_LINKMODE_RELATIVE } | 
| enum | LDMA_PeripheralSignal_t
         
         { ldmaPeripheralSignal_NONE = LDMA_CH_REQSEL_SOURCESEL_NONE, ldmaPeripheralSignal_ADC0_SCAN = LDMA_CH_REQSEL_SIGSEL_ADC0SCAN | LDMA_CH_REQSEL_SOURCESEL_ADC0, ldmaPeripheralSignal_ADC0_SINGLE = LDMA_CH_REQSEL_SIGSEL_ADC0SINGLE | LDMA_CH_REQSEL_SOURCESEL_ADC0, ldmaPeripheralSignal_CRYPTO_DATA0RD = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA0RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, ldmaPeripheralSignal_CRYPTO_DATA0WR = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA0WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, ldmaPeripheralSignal_CRYPTO_DATA0XWR = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA0XWR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, ldmaPeripheralSignal_CRYPTO_DATA1RD = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA1RD | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, ldmaPeripheralSignal_CRYPTO_DATA1WR = LDMA_CH_REQSEL_SIGSEL_CRYPTODATA1WR | LDMA_CH_REQSEL_SOURCESEL_CRYPTO, ldmaPeripheralSignal_I2C0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_I2C0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_I2C0, ldmaPeripheralSignal_I2C0_TXBL = LDMA_CH_REQSEL_SIGSEL_I2C0TXBL | LDMA_CH_REQSEL_SOURCESEL_I2C0, ldmaPeripheralSignal_LEUART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_LEUART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_LEUART0, ldmaPeripheralSignal_LEUART0_TXBL = LDMA_CH_REQSEL_SIGSEL_LEUART0TXBL | LDMA_CH_REQSEL_SOURCESEL_LEUART0, ldmaPeripheralSignal_LEUART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_LEUART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_LEUART0, ldmaPeripheralSignal_MSC_WDATA = LDMA_CH_REQSEL_SIGSEL_MSCWDATA | LDMA_CH_REQSEL_SOURCESEL_MSC, ldmaPeripheralSignal_PRS_REQ0 = LDMA_CH_REQSEL_SIGSEL_PRSREQ0 | LDMA_CH_REQSEL_SOURCESEL_PRS, ldmaPeripheralSignal_PRS_REQ1 = LDMA_CH_REQSEL_SIGSEL_PRSREQ1 | LDMA_CH_REQSEL_SOURCESEL_PRS, ldmaPeripheralSignal_TIMER0_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, ldmaPeripheralSignal_TIMER0_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, ldmaPeripheralSignal_TIMER0_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER0CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER0, ldmaPeripheralSignal_TIMER0_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER0UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER0, ldmaPeripheralSignal_TIMER1_CC0 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC0 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, ldmaPeripheralSignal_TIMER1_CC1 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC1 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, ldmaPeripheralSignal_TIMER1_CC2 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC2 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, ldmaPeripheralSignal_TIMER1_CC3 = LDMA_CH_REQSEL_SIGSEL_TIMER1CC3 | LDMA_CH_REQSEL_SOURCESEL_TIMER1, ldmaPeripheralSignal_TIMER1_UFOF = LDMA_CH_REQSEL_SIGSEL_TIMER1UFOF | LDMA_CH_REQSEL_SOURCESEL_TIMER1, ldmaPeripheralSignal_USART0_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART0RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART0, ldmaPeripheralSignal_USART0_TXBL = LDMA_CH_REQSEL_SIGSEL_USART0TXBL | LDMA_CH_REQSEL_SOURCESEL_USART0, ldmaPeripheralSignal_USART0_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART0TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART0, ldmaPeripheralSignal_USART1_RXDATAV = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAV | LDMA_CH_REQSEL_SOURCESEL_USART1, ldmaPeripheralSignal_USART1_RXDATAVRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1RXDATAVRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1, ldmaPeripheralSignal_USART1_TXBL = LDMA_CH_REQSEL_SIGSEL_USART1TXBL | LDMA_CH_REQSEL_SOURCESEL_USART1, ldmaPeripheralSignal_USART1_TXBLRIGHT = LDMA_CH_REQSEL_SIGSEL_USART1TXBLRIGHT | LDMA_CH_REQSEL_SOURCESEL_USART1, ldmaPeripheralSignal_USART1_TXEMPTY = LDMA_CH_REQSEL_SIGSEL_USART1TXEMPTY | LDMA_CH_REQSEL_SOURCESEL_USART1 } | 
| Functions | |
| void | LDMA_DeInit (void) | 
| De-initialize the LDMA controller. | |
| void | LDMA_EnableChannelRequest (int ch, bool enable) | 
| Enable or disable a LDMA channel request. | |
| void | LDMA_Init (const LDMA_Init_t *init) | 
| Initialize the LDMA controller. | |
| __STATIC_INLINE void | LDMA_IntClear (uint32_t flags) | 
| Clear one or more pending LDMA interrupts. | |
| __STATIC_INLINE void | LDMA_IntDisable (uint32_t flags) | 
| Disable one or more LDMA interrupts. | |
| __STATIC_INLINE void | LDMA_IntEnable (uint32_t flags) | 
| Enable one or more LDMA interrupts. | |
| __STATIC_INLINE uint32_t | LDMA_IntGet (void) | 
| Get pending LDMA interrupt flags. | |
| __STATIC_INLINE uint32_t | LDMA_IntGetEnabled (void) | 
| Get enabled and pending LDMA interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
| __STATIC_INLINE void | LDMA_IntSet (uint32_t flags) | 
| Set one or more pending LDMA interrupts. | |
| void | LDMA_StartTransfer (int ch, const LDMA_TransferCfg_t *transfer, const LDMA_Descriptor_t *descriptor) | 
| Start a DMA transfer. | |
| void | LDMA_StopTransfer (int ch) | 
| Stop a DMA transfer. | |
| bool | LDMA_TransferDone (int ch) | 
| Check if a DMA transfer has completed. | |
| uint32_t | LDMA_TransferRemainingCount (int ch) | 
| Get number of items remaining in a transfer. | |
Macro Definition Documentation
| #define LDMA_DESCRIPTOR_LINKABS_M2M_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:201
          
         
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for linked memory to memory byte transfer.
The link address must be an absolute address.
- Note
- The linkAddr member of the transfer descriptor is not initialized.
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of bytes to transfer. 
        Definition at line
        
         968
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKABS_M2M_HALF | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:201
          
         
           em_ldma.h:135
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:175
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for linked memory to memory half-word transfer.
The link address must be an absolute address.
- Note
- The linkAddr member of the transfer descriptor is not initialized.
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of half-words to transfer. 
        Definition at line
        
         930
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKABS_M2M_WORD | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:201
          
         
           em_ldma.h:135
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:176
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for linked memory to memory word transfer.
The link address must be an absolute address.
- Note
- The linkAddr member of the transfer descriptor is not initialized.
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of words to transfer. 
        Definition at line
        
         892
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKABS_SYNC | ( | 
            set,
            | |
| 
            clr,
            | |||
| 
            matchValue,
            | |||
| 
            matchEnable
            | |||
| ) | 
           em_ldma.h:201
          
         
           em_ldma.h:154
          
         DMA descriptor initializer for SYNC transfer.
The link address must be an absolute address.
- Note
- The linkAddr member of the transfer descriptor is not initialized.
- Parameters
- 
         [in] setSync pattern bits to set. [in] clrSync pattern bits to clear. [in] matchValueSync pattern to match. [in] matchEnableSync pattern bits to enable for match. 
        Definition at line
        
         1456
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKABS_WRITE | ( | 
            value,
            | |
| 
            address
            | |||
| ) | 
           em_ldma.h:201
          
         
           em_ldma.h:155
          
         DMA descriptor initializer for Immediate WRITE transfer.
The link address must be an absolute address.
- Note
- The linkAddr member of the transfer descriptor is not initialized.
- Parameters
- 
         [in] valueImmediate value to write. [in] addressWrite sddress. 
        Definition at line
        
         1344
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_M2M_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:202
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for linked memory to memory byte transfer.
The link address is a relative address.
- Note
- The linkAddr member of the transfer descriptor is initialized to 4, assuming that the next descriptor immediately follows this descriptor (in memory).
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of bytes to transfer. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1100
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_M2M_HALF | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:175
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:202
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for linked memory to memory half-word transfer.
The link address is a relative address.
- Note
- The linkAddr member of the transfer descriptor is initialized to 4, assuming that the next descriptor immediately follows this descriptor (in memory).
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of half-words to transfer. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1056
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_M2M_WORD | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:176
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:202
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for linked memory to memory word transfer.
The link address is a relative address.
- Note
- The linkAddr member of the transfer descriptor is initialized to 4, assuming that the next descriptor immediately follows this descriptor (in memory).
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of words to transfer. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1012
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_M2P_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:160
          
         
           em_ldma.h:153
          
         
           em_ldma.h:166
          
         
           em_ldma.h:184
          
         
           em_ldma.h:202
          
         DMA descriptor initializer for byte transfers from memory to a peripheral.
- Parameters
- 
         [in] srcSource data address. [in] destPeripheral data register destination address. [in] countNumber of bytes to transfer. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1275
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_P2M_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:160
          
         
           em_ldma.h:153
          
         
           em_ldma.h:169
          
         
           em_ldma.h:202
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for byte transfers from a peripheral to memory.
- Parameters
- 
         [in] srcPeripheral data source register address. [in] destDestination data address. [in] countNumber of bytes to transfer. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1237
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_SYNC | ( | 
            set,
            | |
| 
            clr,
            | |||
| 
            matchValue,
            | |||
| 
            matchEnable,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:154
          
         
           em_ldma.h:202
          
         DMA descriptor initializer for SYNC transfer.
- Parameters
- 
         [in] setSync pattern bits to set. [in] clrSync pattern bits to clear. [in] matchValueSync pattern to match. [in] matchEnableSync pattern bits to enable for match. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1497
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_LINKREL_WRITE | ( | 
            value,
            | |
| 
            address,
            | |||
| 
            linkjmp
            | |||
| ) | 
           em_ldma.h:155
          
         
           em_ldma.h:202
          
         DMA descriptor initializer for Immediate WRITE transfer.
- Parameters
- 
         [in] valueImmediate value to write. [in] addressWrite sddress. [in] linkjmpAddress of descriptor to link to expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=one this descriptor, -1=one descriptor back in memory. 
        Definition at line
        
         1381
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_M2M_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for single memory to memory byte transfer.
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of bytes to transfer. 
        Definition at line
        
         854
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_M2M_HALF | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:175
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for single memory to memory half-word transfer.
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of half-words to transfer. 
        Definition at line
        
         821
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_M2M_WORD | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:153
          
         
           em_ldma.h:176
          
         
           em_ldma.h:166
          
         
           em_ldma.h:161
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for single memory to memory word transfer.
- Parameters
- 
         [in] srcSource data address. [in] destDestination data address. [in] countNumber of words to transfer. 
        Definition at line
        
         788
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_M2P_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:160
          
         
           em_ldma.h:153
          
         
           em_ldma.h:166
          
         
           em_ldma.h:184
          
         DMA descriptor initializer for byte transfers from memory to a peripheral.
- Parameters
- 
         [in] srcSource data address. [in] destPeripheral data register destination address. [in] countNumber of bytes to transfer. 
        Definition at line
        
         1199
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_P2M_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:160
          
         
           em_ldma.h:153
          
         
           em_ldma.h:169
          
         
           em_ldma.h:181
          
         DMA descriptor initializer for byte transfers from a peripheral to memory.
- Parameters
- 
         [in] srcPeripheral data source register address. [in] destDestination data address. [in] countNumber of bytes to transfer. 
        Definition at line
        
         1133
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_P2P_BYTE | ( | 
            src,
            | |
| 
            dest,
            | |||
| 
            count
            | |||
| ) | 
           em_ldma.h:135
          
         
           em_ldma.h:174
          
         
           em_ldma.h:189
          
         
           em_ldma.h:195
          
         
           em_ldma.h:160
          
         
           em_ldma.h:153
          
         
           em_ldma.h:169
          
         
           em_ldma.h:184
          
         DMA descriptor initializer for byte transfers from a peripheral to a peripheral.
- Parameters
- 
         [in] srcPeripheral data source register address. [in] destPeripheral data destination register address. [in] countNumber of bytes to transfer. 
        Definition at line
        
         1166
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_SYNC | ( | 
            set,
            | |
| 
            clr,
            | |||
| 
            matchValue,
            | |||
| 
            matchEnable
            | |||
| ) | 
           em_ldma.h:154
          
         DMA descriptor initializer for SYNC transfer.
- Parameters
- 
         [in] setSync pattern bits to set. [in] clrSync pattern bits to clear. [in] matchValueSync pattern to match. [in] matchEnableSync pattern bits to enable for match. 
        Definition at line
        
         1415
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_DESCRIPTOR_SINGLE_WRITE | ( | 
            value,
            | |
| 
            address
            | |||
| ) | 
           em_ldma.h:155
          
         DMA descriptor initializer for Immediate WRITE transfer.
- Parameters
- 
         [in] valueImmediate value to write. [in] addressWrite sddress. 
        Definition at line
        
         1307
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_INIT_DEFAULT | 
Default DMA initialization structure.
        Definition at line
        
         728
        
        of file
        
         em_ldma.h
        
        .
       
Referenced by DMADRV_Init() .
| #define LDMA_TRANSFER_CFG_MEMORY | ( | 
            | ) | 
           em_ldma.h:207
          
         
           em_ldma.h:221
          
         Generic DMA transfer configuration for memory to memory transfers.
        Definition at line
        
         740
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_TRANSFER_CFG_MEMORY_LOOP | ( | 
            loopCnt
            | ) | 
           em_ldma.h:207
          
         
           em_ldma.h:221
          
         Generic DMA transfer configuration for looped memory to memory transfers.
        Definition at line
        
         751
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_TRANSFER_CFG_PERIPHERAL | ( | 
            signal
            | ) | 
           em_ldma.h:207
          
         
           em_ldma.h:221
          
         Generic DMA transfer configuration for memory to/from peripheral transfers.
        Definition at line
        
         763
        
        of file
        
         em_ldma.h
        
        .
       
| #define LDMA_TRANSFER_CFG_PERIPHERAL_LOOP | ( | 
            signal,
            | |
| 
            loopCnt
            | |||
| ) | 
           em_ldma.h:207
          
         
           em_ldma.h:221
          
         Generic DMA transfer configuration for looped memory to/from peripheral transfers.
        Definition at line
        
         774
        
        of file
        
         em_ldma.h
        
        .
       
Enumeration Type Documentation
| enum LDMA_CfgArbSlots_t | 
Insert extra arbitration slots to increase channel arbitration priority.
        Definition at line
        
         206
        
        of file
        
         em_ldma.h
        
        .
       
| enum LDMA_CfgDstIncSign_t | 
| enum LDMA_CfgSrcIncSign_t | 
| enum LDMA_CtrlBlockSize_t | 
This value controls the number of unit data transfers per arbitration cycle, providing a means to balance DMA channels' load on the controller.
        Definition at line
        
         134
        
        of file
        
         em_ldma.h
        
        .
       
| enum LDMA_CtrlDstInc_t | 
Destination address increment unit size.
        Definition at line
        
         180
        
        of file
        
         em_ldma.h
        
        .
       
| enum LDMA_CtrlReqMode_t | 
| enum LDMA_CtrlSize_t | 
| enum LDMA_CtrlSrcInc_t | 
Source address increment unit size.
        Definition at line
        
         165
        
        of file
        
         em_ldma.h
        
        .
       
| enum LDMA_LinkMode_t | 
Peripherals that can trigger LDMA transfers.
        Definition at line
        
         226
        
        of file
        
         em_ldma.h
        
        .
       
Function Documentation
| void LDMA_DeInit | ( | void | 
            | ) | 
De-initialize the LDMA controller.
LDMA interrupts are disabled and the LDMA clock is stopped.
        Definition at line
        
         87
        
        of file
        
         em_ldma.c
        
        .
       
References CMU_ClockEnable() , cmuClock_LDMA , LDMA , and LDMA_IRQn .
Referenced by DMADRV_DeInit() .
| void LDMA_EnableChannelRequest | ( | int | 
            ch,
            | 
| bool | 
            enable
            | ||
| ) | 
Enable or disable a LDMA channel request.
Use this function to enable or disable a LDMA channel request. This will prevent the LDMA from proceeding after its current transaction if disabled.
- Parameters
- 
         [in] channelLDMA channel to enable or disable requests on. [in] enableIf 'true' request will be enabled. If 'false' request will be disabled. 
        Definition at line
        
         109
        
        of file
        
         em_ldma.c
        
        .
       
References BUS_RegBitWrite() , and LDMA .
Referenced by DMADRV_PauseTransfer() , and DMADRV_ResumeTransfer() .
| void LDMA_Init | ( | const LDMA_Init_t * | 
            init
            | ) | 
Initialize the LDMA controller.
This function will disable all the LDMA channels and enable the LDMA bus clock in the CMU. This function will also enable the LDMA IRQ in the NVIC and set the LDMA IRQ priority to a user configurable priority. The LDMA interrupt priority is configured using the LDMA_Init_t structure.
- Note
- Since this function enables the LDMA IRQ you should always add a custom LDMA_IRQHandler to the application in order to handle any interrupts from LDMA.
- Parameters
- 
         [in] initPointer to initialization structure used to configure the LDMA. 
        Definition at line
        
         134
        
        of file
        
         em_ldma.c
        
        .
       
References __NVIC_PRIO_BITS , _LDMA_CTRL_NUMFIXED_MASK , _LDMA_CTRL_NUMFIXED_SHIFT , _LDMA_CTRL_SYNCPRSCLREN_MASK , _LDMA_CTRL_SYNCPRSCLREN_SHIFT , _LDMA_CTRL_SYNCPRSSETEN_MASK , _LDMA_CTRL_SYNCPRSSETEN_SHIFT , CMU_ClockEnable() , cmuClock_LDMA , LDMA , LDMA_IEN_ERROR , LDMA_IRQn , LDMA_Init_t::ldmaInitCtrlNumFixed , LDMA_Init_t::ldmaInitCtrlSyncPrsClrEn , LDMA_Init_t::ldmaInitCtrlSyncPrsSetEn , and LDMA_Init_t::ldmaInitIrqPriority .
Referenced by DMADRV_Init() .
| __STATIC_INLINE void LDMA_IntClear | ( | uint32_t | 
            flags
            | ) | 
Clear one or more pending LDMA interrupts.
- Parameters
- 
         [in] flagsPending LDMA interrupt sources to clear. Use one or more valid interrupt flags for the LDMA module. The flags are LDMA_IFC_ERROR and one done flag for each channel. 
        Definition at line
        
         1548
        
        of file
        
         em_ldma.h
        
        .
       
References LDMA .
| __STATIC_INLINE void LDMA_IntDisable | ( | uint32_t | 
            flags
            | ) | 
Disable one or more LDMA interrupts.
- Parameters
- 
         [in] flagsLDMA interrupt sources to disable. Use one or more valid interrupt flags for the LDMA module. The flags are LDMA_IEN_ERROR and one done flag for each channel. 
        Definition at line
        
         1562
        
        of file
        
         em_ldma.h
        
        .
       
References LDMA .
| __STATIC_INLINE void LDMA_IntEnable | ( | uint32_t | 
            flags
            | ) | 
Enable one or more LDMA interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using LDMA_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
- 
         [in] flagsLDMA interrupt sources to enable. Use one or more valid interrupt flags for the LDMA module. The flags are LDMA_IEN_ERROR and one done flag for each channel. 
        Definition at line
        
         1581
        
        of file
        
         em_ldma.h
        
        .
       
References LDMA .
| __STATIC_INLINE uint32_t LDMA_IntGet | ( | void | 
            | ) | 
Get pending LDMA interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- LDMA interrupt sources pending. Returns one or more valid interrupt flags for the LDMA module. The flags are LDMA_IF_ERROR and one flag for each LDMA channel.
        Definition at line
        
         1598
        
        of file
        
         em_ldma.h
        
        .
       
References LDMA .
| __STATIC_INLINE uint32_t LDMA_IntGetEnabled | ( | void | 
            | ) | 
Get enabled and pending LDMA interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- 
         Pending and enabled LDMA interrupt sources The return value is the bitwise AND of
         - the enabled interrupt sources in LDMA_IEN and
- the pending interrupt flags LDMA_IF
 
        Definition at line
        
         1617
        
        of file
        
         em_ldma.h
        
        .
       
References LDMA .
| __STATIC_INLINE void LDMA_IntSet | ( | uint32_t | 
            flags
            | ) | 
Set one or more pending LDMA interrupts.
- Parameters
- 
         [in] flagsLDMA interrupt sources to set to pending. Use one or more valid interrupt flags for the LDMA module. The flags are LDMA_IFS_ERROR and one done flag for each LDMA channel. 
        Definition at line
        
         1634
        
        of file
        
         em_ldma.h
        
        .
       
References LDMA .
| void LDMA_StartTransfer | ( | int | 
            ch,
            | 
| const LDMA_TransferCfg_t * | 
            transfer,
            | ||
| const LDMA_Descriptor_t * | 
            descriptor
            | ||
| ) | 
Start a DMA transfer.
- Parameters
- 
         [in] chDMA channel. [in] transferInitialization structure used to configure the transfer. [in] descriptorTransfer descriptor, can be an array of descriptors linked together. 
        Definition at line
        
         180
        
        of file
        
         em_ldma.c
        
        .
       
References _LDMA_CH_CFG_ARBSLOTS_MASK , _LDMA_CH_CFG_ARBSLOTS_SHIFT , _LDMA_CH_CFG_DSTINCSIGN_MASK , _LDMA_CH_CFG_DSTINCSIGN_SHIFT , _LDMA_CH_CFG_SRCINCSIGN_MASK , _LDMA_CH_CFG_SRCINCSIGN_SHIFT , _LDMA_CH_LINK_LINKADDR_MASK , _LDMA_CH_LOOP_LOOPCNT_MASK , _LDMA_CH_LOOP_LOOPCNT_SHIFT , _LDMA_CH_REQSEL_MASK , _LDMA_CTRL_SYNCPRSCLREN_MASK , _LDMA_CTRL_SYNCPRSCLREN_SHIFT , _LDMA_CTRL_SYNCPRSSETEN_MASK , _LDMA_CTRL_SYNCPRSSETEN_SHIFT , BUS_RegMaskedClear() , CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , LDMA , LDMA_TransferCfg_t::ldmaCfgArbSlots , LDMA_TransferCfg_t::ldmaCfgDstIncSign , LDMA_TransferCfg_t::ldmaCfgSrcIncSign , LDMA_TransferCfg_t::ldmaCtrlSyncPrsClrOff , LDMA_TransferCfg_t::ldmaCtrlSyncPrsClrOn , LDMA_TransferCfg_t::ldmaCtrlSyncPrsSetOff , LDMA_TransferCfg_t::ldmaCtrlSyncPrsSetOn , LDMA_TransferCfg_t::ldmaDbgHalt , LDMA_TransferCfg_t::ldmaLoopCnt , LDMA_TransferCfg_t::ldmaReqDis , and LDMA_TransferCfg_t::ldmaReqSel .
Referenced by DMADRV_LdmaStartTransfer() .
| void LDMA_StopTransfer | ( | int | 
            ch
            | ) | 
Stop a DMA transfer.
- Note
- The DMA will complete the current AHB burst transfer before stopping.
- Parameters
- 
         [in] chDMA channel to stop. 
        Definition at line
        
         275
        
        of file
        
         em_ldma.c
        
        .
       
References BUS_RegMaskedClear() , CORE_ATOMIC_SECTION , and LDMA .
Referenced by DMADRV_StopTransfer() .
| bool LDMA_TransferDone | ( | int | 
            ch
            | ) | 
Check if a DMA transfer has completed.
- Parameters
- 
         [in] chDMA channel to check. 
- Returns
- True if transfer has completed, false if not.
        Definition at line
        
         297
        
        of file
        
         em_ldma.c
        
        .
       
References CORE_ATOMIC_SECTION , and LDMA .
Referenced by DMADRV_TransferDone() .
| uint32_t LDMA_TransferRemainingCount | ( | int | 
            ch
            | ) | 
Get number of items remaining in a transfer.
- Note
- This function is does not take into account that a DMA transfers with a chain of linked transfers might be ongoing. It will only check the count for the current transfer.
- Parameters
- 
         [in] chThe channel number of the transfer to check. 
- Returns
- Number of items remaining in the transfer.
        Definition at line
        
         328
        
        of file
        
         em_ldma.c
        
        .
       
References _LDMA_CH_CTRL_XFERCNT_MASK , _LDMA_CH_CTRL_XFERCNT_SHIFT , CORE_ATOMIC_SECTION , and LDMA .
Referenced by DMADRV_TransferRemainingCount() .