RTCC_CC_TypeDef Struct ReferenceDevicesDevices > | RTCC
RTCC_CC RTCC CC Register
.
       Definition at line
       
        47
       
       of file
       
        efr32bg1p_rtcc_cc.h
       
       .
      
      
       #include <
       
     
        efr32bg1p_rtcc_cc.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CCV | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DATE | 
| __IOM uint32_t | TIME | 
Field Documentation
| __IOM uint32_t RTCC_CC_TypeDef::CCV | 
Capture/Compare Value Register
        Definition at line
        
         49
        
        of file
        
         efr32bg1p_rtcc_cc.h
        
        .
       
| __IOM uint32_t RTCC_CC_TypeDef::CTRL | 
CC Channel Control Register
        Definition at line
        
         48
        
        of file
        
         efr32bg1p_rtcc_cc.h
        
        .
       
| __IOM uint32_t RTCC_CC_TypeDef::DATE | 
Capture/Compare Date Register
        Definition at line
        
         51
        
        of file
        
         efr32bg1p_rtcc_cc.h
        
        .
       
| __IOM uint32_t RTCC_CC_TypeDef::TIME | 
Capture/Compare Time Register
        Definition at line
        
         50
        
        of file
        
         efr32bg1p_rtcc_cc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG1P/Include/
       efr32bg1p_rtcc_cc.h