LDMA_Descriptor_t Union ReferenceEMLIB > LDMA
DMA descriptor.
The LDMA DMA controller supports three different DMA descriptors. Each consist of four WORD's which map directly onto hw control registers for a given DMA channel. The three descriptor types are XFER, SYNC and WRI. Refer to the reference manual for further information.
       Definition at line
       
        606
       
       of file
       
        em_ldma.h
       
       .
      
      
       #include <
       
     
        em_ldma.h
       
       >
      
| Data Fields | |
| struct { | |
| uint32_t blockSize : 4 | |
| uint32_t byteSwap : 1 | |
| uint32_t decLoopCnt : 1 | |
| uint32_t doneIfs : 1 | |
| uint32_t dstAddrMode : 1 | |
| uint32_t dstInc : 2 | |
| uint32_t ignoreSrec : 1 | |
| uint32_t link : 1 | |
| int32_t linkAddr : 30 | |
| uint32_t linkMode : 1 | |
| uint32_t matchEn : 8 | |
| uint32_t matchVal : 8 | |
| uint32_t reqMode : 1 | |
| uint32_t reserved0 : 1 | |
| uint32_t reserved3 : 16 | |
| uint32_t reserved4 : 16 | |
| uint32_t size : 2 | |
| uint32_t srcAddrMode : 1 | |
| uint32_t srcInc : 2 | |
| uint32_t structReq : 1 | |
| uint32_t structType : 2 | |
| uint32_t syncClr : 8 | |
| uint32_t syncSet : 8 | |
| uint32_t xferCnt : 11 | |
| } | sync | 
| struct { | |
| uint32_t blockSize : 4 | |
| uint32_t byteSwap : 1 | |
| uint32_t decLoopCnt : 1 | |
| uint32_t doneIfs : 1 | |
| uint32_t dstAddr | |
| uint32_t dstAddrMode : 1 | |
| uint32_t dstInc : 2 | |
| uint32_t ignoreSrec : 1 | |
| uint32_t immVal | |
| uint32_t link : 1 | |
| int32_t linkAddr : 30 | |
| uint32_t linkMode : 1 | |
| uint32_t reqMode : 1 | |
| uint32_t reserved0 : 1 | |
| uint32_t size : 2 | |
| uint32_t srcAddrMode : 1 | |
| uint32_t srcInc : 2 | |
| uint32_t structReq : 1 | |
| uint32_t structType : 2 | |
| uint32_t xferCnt : 11 | |
| } | wri | 
| struct { | |
| uint32_t blockSize : 4 | |
| uint32_t byteSwap : 1 | |
| uint32_t decLoopCnt : 1 | |
| uint32_t doneIfs : 1 | |
| uint32_t dstAddr | |
| uint32_t dstAddrMode : 1 | |
| uint32_t dstInc : 2 | |
| uint32_t ignoreSrec : 1 | |
| uint32_t link : 1 | |
| int32_t linkAddr : 30 | |
| uint32_t linkMode : 1 | |
| uint32_t reqMode : 1 | |
| uint32_t reserved0 : 1 | |
| uint32_t size : 2 | |
| uint32_t srcAddr | |
| uint32_t srcAddrMode : 1 | |
| uint32_t srcInc : 2 | |
| uint32_t structReq : 1 | |
| uint32_t structType : 2 | |
| uint32_t xferCnt : 11 | |
| } | xfer | 
Field Documentation
| uint32_t LDMA_Descriptor_t::blockSize | 
Number of unit transfers per arb. cycle.
        Definition at line
        
         617
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::byteSwap | 
Enable byte swapping transfers.
        Definition at line
        
         616
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::decLoopCnt | 
Enable looped transfers.
        Definition at line
        
         620
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::doneIfs | 
Generate interrupt when done.
        Definition at line
        
         618
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::dstAddr | 
DMA destination address.
DMA write destination address.
        Definition at line
        
         629
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::dstAddrMode | 
Destination addressing mode.
        Definition at line
        
         626
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::dstInc | 
Destination address increment unit size.
        Definition at line
        
         624
        
        of file
        
         em_ldma.h
        
        .
       
Referenced by MIC_init() .
| uint32_t LDMA_Descriptor_t::ignoreSrec | 
Ignore single requests.
        Definition at line
        
         621
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::immVal | 
Data to be written at dstAddr.
        Definition at line
        
         686
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::link | 
Enable LINKLOAD when transfer is done.
        Definition at line
        
         632
        
        of file
        
         em_ldma.h
        
        .
       
| int32_t LDMA_Descriptor_t::linkAddr | 
Address of next (linked) descriptor.
        Definition at line
        
         633
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::linkMode | 
Select absolute or relative link address.
        Definition at line
        
         631
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::matchEn | 
Sync trig match enable.
        Definition at line
        
         660
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::matchVal | 
Sync trig match value.
        Definition at line
        
         659
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::reqMode | 
Block or cycle transfer selector.
        Definition at line
        
         619
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::size | 
| uint32_t LDMA_Descriptor_t::srcAddr | 
DMA source address.
        Definition at line
        
         628
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::srcAddrMode | 
Source addressing mode.
        Definition at line
        
         625
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::srcInc | 
Source address increment unit size.
        Definition at line
        
         622
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::structReq | 
DMA transfer trigger during LINKLOAD.
        Definition at line
        
         614
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::structType | 
Set to 0 to select XFER descriptor type.
Set to 1 to select SYNC descriptor type.
Set to 2 to select WRITE descriptor type.
        Definition at line
        
         612
        
        of file
        
         em_ldma.h
        
        .
       
| struct { ... } LDMA_Descriptor_t::sync | 
SYNCHRONIZE DMA descriptor, used for intra channel transfer syncronization.
| uint32_t LDMA_Descriptor_t::syncClr | 
Clear bits in LDMA_CTRL.SYNCTRIG register
        Definition at line
        
         657
        
        of file
        
         em_ldma.h
        
        .
       
| uint32_t LDMA_Descriptor_t::syncSet | 
Set bits in LDMA_CTRL.SYNCTRIG register.
        Definition at line
        
         656
        
        of file
        
         em_ldma.h
        
        .
       
| struct { ... } LDMA_Descriptor_t::wri | 
WRITE DMA descriptor, used for write immediate operations.
| struct { ... } LDMA_Descriptor_t::xfer | 
TRANSFER DMA descriptor, this is the only descriptor type which can be used to start a DMA transfer.
Referenced by MIC_init() .
| uint32_t LDMA_Descriptor_t::xferCnt | 
Transfer count minus one.
        Definition at line
        
         615
        
        of file
        
         em_ldma.h
        
        .
       
The documentation for this union was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_ldma.h