Transmit_PluginEMDRV > EZRADIODRV > Plugin_System

Detailed Description

Transmit plugin, see Plugin System Layer for detailed documentation.


     

.

Data Structures

struct EZRADIODRV_FieldLength
struct EZRADIODRV_PacketLengthConfig
EzRadio transmit packet length configuration structure.
struct EZRADIODRV_PacketTxHandle
EzRadio transmit plug-in instance initialization and handler structure.

Macros

#define ECODE_EMDRV_EZRADIODRV_TRANSMIT_FAILED ( ECODE_EMDRV_EZRADIODRV_TRANSMIT_PLUGIN_BASE | 0x00000001)
Unable to start transmission.
#define EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT
Configuration data for EzRadio transmit plug-in.

Typedefs

typedef struct EZRADIODRV_FieldLength EZRADIODRV_FieldLength_t
typedef struct EZRADIODRV_PacketLengthConfig EZRADIODRV_PacketLengthConfig_t
EzRadio transmit packet length configuration structure.
typedef struct EZRADIODRV_PacketTxHandle EZRADIODRV_PacketTxHandle_t
EzRadio transmit plug-in instance initialization and handler structure.
typedef enum EZRADIODRV_TransmitLengthMode EZRADIODRV_TransmitLengthMode_t
EzRadio transmit packet length mode.
typedef enum EZRADIODRV_TransmitPacketType EZRADIODRV_TransmitPacketType_t
EzRadio transmit packet type.

Enumerations

enum EZRADIODRV_TransmitLengthMode {
ezradiodrvTransmitLenghtDefault = 0,
ezradiodrvTransmitLenghtCustomPacketLen = 1,
ezradiodrvTransmitLenghtCustomFieldLen = 2
}
EzRadio transmit packet length mode.
enum EZRADIODRV_TransmitPacketType {
ezradiodrvPacketTypeNormal = 0,
ezradiodrvPacketTypeAutoAck = 1
}
EzRadio transmit packet type.

Functions

Ecode_t ezradioStartTransmitBasic ( EZRADIODRV_Handle_t radioHandle, uint16_t packetLength, uint8_t *pioRadioPacket)
Start basic transmission. Radio transmits with data only in the first field in this case.
Ecode_t ezradioStartTransmitConfigured ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket)
Start transmission using the packet parameters from the generated configuration header file.
Ecode_t ezradioStartTransmitCustom ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket)
Start transmission using the packet parameters from pktLengthConf.
Ecode_t ezradioStartTransmitDefault ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket)
Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.
Ecode_t ezradioStartTransmitSmart ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket)
Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.

Macro Definition Documentation

#define EZRADIODRV_TRANSMIT_PLUGIN_INIT_DEFAULT
Value:
{ /* Packet TX */ \
NULL, /* CallBack */ \
{ /* Packet length config */ \
ezradiodrvTransmitLenghtDefault, /* Default length mode */ \
0, /* Packet length */ \
{ 0, 0, 0, 0, 0 } /* Field lengths */ \
}, \
RADIO_CONFIGURATION_DATA_CHANNEL_NUMBER, /* Channel */ \
ezradiodrvPacketTypeNormal, /* Packet type */ \
0, /* Packet ID */ \
},

Configuration data for EzRadio transmit plug-in.

Definition at line 116 of file ezradio_transmit_plugin.h .

Typedef Documentation

EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.

Enumeration Type Documentation

EzRadio transmit packet length mode.

Enumerator
ezradiodrvTransmitLenghtDefault

Transmit packet length is defined in the generated configuration.

ezradiodrvTransmitLenghtCustomPacketLen

Transmit packet length is defined by the application for field1 only.

ezradiodrvTransmitLenghtCustomFieldLen

Transmit packet length is defined by the application for multiple fields.

Definition at line 68 of file ezradio_transmit_plugin.h .

EzRadio transmit packet type.

Enumerator
ezradiodrvPacketTypeNormal

Normal packet type.

ezradiodrvPacketTypeAutoAck

Auto acknowledge packet type.

Definition at line 75 of file ezradio_transmit_plugin.h .

Function Documentation

Ecode_t ezradioStartTransmitBasic ( EZRADIODRV_Handle_t radioHandle,
uint16_t packetLength,
uint8_t * pioRadioPacket
)

Start basic transmission. Radio transmits with data only in the first field in this case.

Parameters
radioHandle Handler of the EzRadio driver instance where packet length and channel configurations are set.
packetLength Length of the basic packet.
pioRadioPacket Pointer to the packet buffer.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 70 of file ezradio_transmit_plugin.c .

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomPacketLen , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .

Referenced by ezradioStartTransmitSmart() .

Ecode_t ezradioStartTransmitConfigured ( EZRADIODRV_Handle_t radioHandle,
uint8_t * pioRadioPacket
)

Start transmission using the packet parameters from the generated configuration header file.

Parameters
radioHandle Handler of the EzRadio driver instance where packet length and channel configurations are set.
pioRadioPacket Pointer to the packet buffer.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 111 of file ezradio_transmit_plugin.c .

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtDefault , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .

Referenced by ezradioStartTransmitSmart() .

Ecode_t ezradioStartTransmitCustom ( EZRADIODRV_Handle_t radioHandle,
EZRADIODRV_PacketLengthConfig_t pktLengthConf,
uint8_t * pioRadioPacket
)

Start transmission using the packet parameters from pktLengthConf.

Parameters
radioHandle Handler of the EzRadio driver instance where packet length and channel configurations are set.
pktLengthConf Packet length configuration structure configuration of the custom packet.
pioRadioPacket Pointer to the packet buffer.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 152 of file ezradio_transmit_plugin.c .

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomPacketLen , EZRADIODRV_FieldLength::f1 , EZRADIODRV_FieldLength::f2 , EZRADIODRV_FieldLength::f3 , EZRADIODRV_FieldLength::f4 , EZRADIODRV_FieldLength::f5 , EZRADIODRV_PacketLengthConfig::fieldLen , EZRADIODRV_PacketTxHandle::lenConfig , EZRADIODRV_PacketLengthConfig::lenMode , EZRADIODRV_HandleData::packetTx , and EZRADIODRV_PacketLengthConfig::pktLen .

Referenced by ezradioStartTransmitSmart() .

Ecode_t ezradioStartTransmitDefault ( EZRADIODRV_Handle_t radioHandle,
uint8_t * pioRadioPacket
)

Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called.

Parameters
radioHandle Handler of the EzRadio driver instance where packet length and channel configurations are set.
pioRadioPacket Pointer to the packet buffer.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 221 of file ezradio_transmit_plugin.c .

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradioStartTransmitSmart() , EZRADIODRV_PacketTxHandle::lenConfig , and EZRADIODRV_HandleData::packetTx .

Ecode_t ezradioStartTransmitSmart ( EZRADIODRV_Handle_t radioHandle,
EZRADIODRV_PacketLengthConfig_t pktLengthConf,
uint8_t * pioRadioPacket
)

Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called.

Parameters
radioHandle Handler of the EzRadio driver instance where packet length and channel configurations are set.
pktLengthConf Packet length configuration structure configuration of the custom packet.
pioRadioPacket Pointer to the packet buffer.
Returns
ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.

Definition at line 191 of file ezradio_transmit_plugin.c .

References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , ezradiodrvTransmitLenghtCustomFieldLen , ezradiodrvTransmitLenghtCustomPacketLen , ezradiodrvTransmitLenghtDefault , ezradioStartTransmitBasic() , ezradioStartTransmitConfigured() , ezradioStartTransmitCustom() , EZRADIODRV_PacketLengthConfig::lenMode , and EZRADIODRV_PacketLengthConfig::pktLen .

Referenced by ezradioStartTransmitDefault() .