BCP_Packet_ Struct ReferenceBSP > API for STKs and WSTKs

BCP Packet Structure - Board controller communication protocol version 1.

Definition at line 73 of file bsp_bcp.h.

#include <bsp_bcp.h>

Data Fields

uint8_t data [BSP_BCP_PACKET_SIZE]
 
uint8_t magic
 
uint8_t payloadLength
 
uint8_t type
 

Field Documentation

uint8_t BCP_Packet_::data[BSP_BCP_PACKET_SIZE]

BCP Packet Data payload

Definition at line 77 of file bsp_bcp.h.

uint8_t BCP_Packet_::magic

Magic - start of packet - must be BSP_BCP_MAGIC

Definition at line 74 of file bsp_bcp.h.

uint8_t BCP_Packet_::payloadLength

Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE

Definition at line 76 of file bsp_bcp.h.

uint8_t BCP_Packet_::type

Type of packet

Definition at line 75 of file bsp_bcp.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/bsp/bsp_bcp.h