MPU_RegionInit_TypeDef Struct ReferenceEMLIB > MPU
MPU Region init structure.
Definition at line 122
of file em_mpu.h
.
#include <
em_mpu.h
>
Data Fields | |
MPU_RegionAp_TypeDef | accessPermission |
uint32_t | baseAddress |
bool | bufferable |
bool | cacheable |
bool | disableExec |
bool | regionEnable |
uint8_t | regionNo |
bool | shareable |
MPU_RegionSize_TypeDef | size |
uint8_t | srd |
uint8_t | tex |
Field Documentation
MPU_RegionAp_TypeDef MPU_RegionInit_TypeDef::accessPermission |
Memory access permissions.
Definition at line 127
of file em_mpu.h
.
Referenced by MPU_ConfigureRegion().
uint32_t MPU_RegionInit_TypeDef::baseAddress |
bool MPU_RegionInit_TypeDef::bufferable |
Memory bufferable attribute.
Definition at line 131
of file em_mpu.h
.
Referenced by MPU_ConfigureRegion().
bool MPU_RegionInit_TypeDef::cacheable |
Memory cacheable attribute.
Definition at line 130
of file em_mpu.h
.
Referenced by MPU_ConfigureRegion().
bool MPU_RegionInit_TypeDef::disableExec |
bool MPU_RegionInit_TypeDef::regionEnable |
uint8_t MPU_RegionInit_TypeDef::regionNo |
bool MPU_RegionInit_TypeDef::shareable |
Memory shareable attribute.
Definition at line 129
of file em_mpu.h
.
Referenced by MPU_ConfigureRegion().
MPU_RegionSize_TypeDef MPU_RegionInit_TypeDef::size |
uint8_t MPU_RegionInit_TypeDef::srd |
Memory subregion disable bits.
Definition at line 132
of file em_mpu.h
.
Referenced by MPU_ConfigureRegion().
uint8_t MPU_RegionInit_TypeDef::tex |
Memory type extension attributes.
Definition at line 133
of file em_mpu.h
.
Referenced by MPU_ConfigureRegion().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_mpu.h