SMU_TypeDef Struct ReferenceDevices > EFR32MG13P932F512GM48 > Peripheral TypeDefsDevices > EFR32MG13P932F512GM48 > | Bit Fields > SMUDevices > | SMU
SMU Register Declaration
Definition at line
516
of file
efr32mg13p932f512gm48.h
.
#include <
efr32mg13p932f512gm48.h
>
Data Fields |
|
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | PPUCTRL |
| __IM uint32_t | PPUFS |
| __IOM uint32_t | PPUPATD0 |
| __IOM uint32_t | PPUPATD1 |
| uint32_t | RESERVED0 [3] |
| uint32_t | RESERVED1 [9] |
| uint32_t | RESERVED2 [3] |
| uint32_t | RESERVED3 [14] |
Field Documentation
| __IOM uint32_t SMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line
521
of file
efr32mg13p932f512gm48.h
.
| __IM uint32_t SMU_TypeDef::IF |
Interrupt Flag Register
Definition at line
518
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t SMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
520
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t SMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
519
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t SMU_TypeDef::PPUCTRL |
PPU Control Register
Definition at line
524
of file
efr32mg13p932f512gm48.h
.
| __IM uint32_t SMU_TypeDef::PPUFS |
PPU Fault Status
Definition at line
530
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t SMU_TypeDef::PPUPATD0 |
PPU Privilege Access Type Descriptor 0
Definition at line
526
of file
efr32mg13p932f512gm48.h
.
| __IOM uint32_t SMU_TypeDef::PPUPATD1 |
PPU Privilege Access Type Descriptor 1
Definition at line
527
of file
efr32mg13p932f512gm48.h
.
| uint32_t SMU_TypeDef::RESERVED0 |
Reserved for future use
Definition at line
517
of file
efr32mg13p932f512gm48.h
.
| uint32_t SMU_TypeDef::RESERVED1 |
Reserved for future use
Definition at line
523
of file
efr32mg13p932f512gm48.h
.
| uint32_t SMU_TypeDef::RESERVED2 |
Reserved for future use
Definition at line
525
of file
efr32mg13p932f512gm48.h
.
| uint32_t SMU_TypeDef::RESERVED3 |
Reserved for future use
Definition at line
529
of file
efr32mg13p932f512gm48.h
.
The documentation for this struct was generated from the following files:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG13P/Include/
efr32mg13p932f512gm48.h -
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG13P/Include/
efr32mg13p_smu.h