tftdirect.c File Reference
EFM32GG_DK3750, TFT Initialization and setup for Direct Drive mode.
- Version
 - 5.5.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        tftdirect.c
       
       .
      
       #include <stdbool.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_ebi.h
       
       "
      
      
       #include "
       
        bsp.h
       
       "
      
      
       #include "
       
        tftdirect.h
       
       "
      
      
       #include "
       
        glib/glib.h
       
       "
      
      
         Functions | 
       |
| void | TFT_DirectGPIOConfig (void) | 
| 
         GPIO configuration for TFT direct drive.
          | 
       |
| bool | TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit) | 
| 
         TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)
          | 
       |
         Variables | 
       |
| static bool | runOnce = true | 
Variable Documentation
           
  | 
          static | 
Flag to indicate that we need to initialize once if starting up in
        Definition at line
        
         26
        
        of file
        
         tftdirect.c
        
        .
       
Referenced by TFT_DirectInit() .