msdd.h File Reference

Mass Storage class Device (MSD) driver.

Version
5.5.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file msdd.h.

Data Structures

struct  MSDD_CmdStatus_TypeDef
 Status info for one BOT CBW -> Data I/O -> CSW cycle.
 

Macros

#define MEDIA_BUFSIZ   4096
 

Functions

bool MSDD_Handler (void)
 Serve the MSD state machine. This function should be called on a regular basis from your main loop. It cannot be called from within an interrupt handler.
 
void MSDD_Init (int activityLedPort, uint32_t activityLedPin)
 Initialize MSD device.
 
int MSDD_SetupCmd (const USB_Setup_TypeDef *setup)
 Called whenever a USB setup command is received. This function overrides standard CLEAR_FEATURE commands, and implements MSD class commands "Bulk-Only Mass Storage Reset" and "Get Max LUN".
 
void MSDD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState)
 Called whenever the USB device has changed its device state.