LESENSE_ST_TypeDef Struct ReferenceDevicesDevices > | LESENSE

LESENSE_ST LESENSE ST Register


      

.

Definition at line 47 of file efr32bg12p_lesense_st.h .

#include < efr32bg12p_lesense_st.h >

Data Fields

__IOM uint32_t TCONFA
__IOM uint32_t TCONFB

Field Documentation

__IOM uint32_t LESENSE_ST_TypeDef::TCONFA

State Transition Configuration a

Definition at line 48 of file efr32bg12p_lesense_st.h .

__IOM uint32_t LESENSE_ST_TypeDef::TCONFB

State Transition Configuration B

Definition at line 49 of file efr32bg12p_lesense_st.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG12P/Include/ efr32bg12p_lesense_st.h