MSDSCSI_StartStopUnit_TypeDef Struct ReferenceKit Drivers > Msd
SCSI Start Stop Unit Command Descriptor Block (CDB) typedef.
Definition at line 277
of file msdscsi.h
.
#include <
msdscsi.h
>
Data Fields | |
struct { | |
uint8_t Immed: 1 | |
uint8_t Reserved1: 7 | |
}; | |
struct { | |
uint8_t PowerConditionModifier: 4 | |
uint8_t Reserved3: 4 | |
}; | |
struct { | |
uint8_t LoEj: 1 | |
uint8_t No_Flush: 1 | |
uint8_t PowerCondition: 4 | |
uint8_t Reserved4: 1 | |
uint8_t Start: 1 | |
}; | |
uint8_t | Control |
uint8_t | OpCode |
uint8_t | Reserved2 |
Field Documentation
uint8_t MSDSCSI_StartStopUnit_TypeDef::Control |
Control byte.
Definition at line 295
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::Immed |
Immediate bit.
Definition at line 280
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::LoEj |
Load Eject.
Definition at line 290
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::No_Flush |
Dont flush cached data to the medium.
Definition at line 291
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::OpCode |
Command opcode.
Definition at line 278
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::PowerCondition |
Power Condition field.
Definition at line 293
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::PowerConditionModifier |
Additional power condition info.
Definition at line 285
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved1 |
Reserved, expect 0.
Definition at line 281
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved2 |
Reserved, expect 0.
Definition at line 283
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved3 |
Reserved, expect 0.
Definition at line 286
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved4 |
Reserved, expect 0.
Definition at line 292
of file msdscsi.h
.
uint8_t MSDSCSI_StartStopUnit_TypeDef::Start |
Start bit.
Definition at line 289
of file msdscsi.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/hardware/kit/common/drivers/
msdscsi.h