VDAC_InitChannel_TypeDef Struct ReferenceEMLIB > VDAC
VDAC channel initialization structure.
Definition at line
209
of file
em_vdac.h
.
#include <
em_vdac.h
>
Data Fields |
|
bool | enable |
bool | prsAsync |
VDAC_PrsSel_TypeDef | prsSel |
bool | sampleOffMode |
VDAC_TrigMode_TypeDef | trigMode |
Field Documentation
bool VDAC_InitChannel_TypeDef::enable |
bool VDAC_InitChannel_TypeDef::prsAsync |
Treat the PRS signal asynchronously.
Definition at line
219
of file
em_vdac.h
.
Referenced by VDAC_InitChannel() .
VDAC_PrsSel_TypeDef VDAC_InitChannel_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
trigMode
is set to
vdacTrigModePrs
or
vdacTrigModeSwPrs
.
Definition at line
216
of file
em_vdac.h
.
Referenced by VDAC_InitChannel() .
bool VDAC_InitChannel_TypeDef::sampleOffMode |
Set channel conversion mode to sample/shut-off mode. Default is continuous.
Definition at line
226
of file
em_vdac.h
.
Referenced by VDAC_InitChannel() .
VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode |
Channel conversion trigger mode.
Definition at line
222
of file
em_vdac.h
.
Referenced by VDAC_InitChannel() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_vdac.h