spidrv.h File Reference
SPIDRV API definition.
- Version
- 5.5.0
License
(C) Copyright 2014 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
spidrv.h
.
#include "
em_device.h
"
#include "
em_cmu.h
"
#include "
ecode.h
"
#include "spidrv_config.h"
#include "
rtcdriver.h
"
#include "
dmadrv.h
"
Data Structures |
|
struct | SPIDRV_HandleData |
struct | SPIDRV_Init |
Macros |
|
#define | ECODE_EMDRV_SPIDRV_ABORTED ( ECODE_EMDRV_SPIDRV_BASE | 0x00000007) |
An SPI transfer has been aborted.
|
|
#define | ECODE_EMDRV_SPIDRV_BUSY ( ECODE_EMDRV_SPIDRV_BASE | 0x00000003) |
The SPI port is busy.
|
|
#define | ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000009) |
Unable to allocate DMA channels.
|
|
#define | ECODE_EMDRV_SPIDRV_IDLE ( ECODE_EMDRV_SPIDRV_BASE | 0x00000006) |
No SPI transfer in progress.
|
|
#define | ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE ( ECODE_EMDRV_SPIDRV_BASE | 0x00000001) |
An illegal SPI handle.
|
|
#define | ECODE_EMDRV_SPIDRV_MODE_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000008) |
SPI master used slave API or vica versa.
|
|
#define | ECODE_EMDRV_SPIDRV_OK ( ECODE_OK ) |
A successful return value.
|
|
#define | ECODE_EMDRV_SPIDRV_PARAM_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000002) |
An illegal input parameter.
|
|
#define | ECODE_EMDRV_SPIDRV_TIMEOUT ( ECODE_EMDRV_SPIDRV_BASE | 0x00000005) |
An SPI transfer timeout.
|
|
#define | ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR ( ECODE_EMDRV_SPIDRV_BASE | 0x00000004) |
Unable to allocate timeout timer.
|
|
#define | SPIDRV_MASTER_USART0 |
Configuration data for SPI master using USART0.
|
|
#define | SPIDRV_MASTER_USART1 |
Configuration data for SPI master using USART1.
|
|
#define | SPIDRV_MASTER_USART2 |
Configuration data for SPI master using USART2.
|
|
#define | SPIDRV_MASTER_USART3 |
Configuration data for SPI master using USART3.
|
|
#define | SPIDRV_SLAVE_USART0 |
Configuration data for SPI slave using USART0.
|
|
#define | SPIDRV_SLAVE_USART1 |
Configuration data for SPI slave using USART1.
|
|
#define | SPIDRV_SLAVE_USART2 |
Configuration data for SPI slave using USART2.
|
|
#define | SPIDRV_SLAVE_USART3 |
Configuration data for SPI slave using USART3.
|
|
Typedefs |
|
typedef enum SPIDRV_BitOrder | SPIDRV_BitOrder_t |
SPI bus bit order.
|
|
typedef void(* | SPIDRV_Callback_t ) (struct SPIDRV_HandleData *handle, Ecode_t transferStatus, int itemsTransferred) |
SPIDRV transfer completion callback function.
|
|
typedef enum SPIDRV_ClockMode | SPIDRV_ClockMode_t |
SPI clock mode (clock polarity and phase).
|
|
typedef enum SPIDRV_CsControl | SPIDRV_CsControl_t |
SPI master chip select (CS) control scheme.
|
|
typedef SPIDRV_HandleData_t * | SPIDRV_Handle_t |
An SPI driver instance handle.
|
|
typedef struct SPIDRV_HandleData | SPIDRV_HandleData_t |
typedef struct SPIDRV_Init | SPIDRV_Init_t |
typedef enum SPIDRV_SlaveStart | SPIDRV_SlaveStart_t |
SPI slave transfer start scheme.
|
|
typedef enum SPIDRV_Type | SPIDRV_Type_t |
SPI driver instance type.
|
|
Enumerations |
|
enum |
SPIDRV_BitOrder
{
spidrvBitOrderLsbFirst = 0, spidrvBitOrderMsbFirst = 1 } |
SPI bus bit order.
|
|
enum |
SPIDRV_ClockMode
{
spidrvClockMode0 = 0, spidrvClockMode1 = 1, spidrvClockMode2 = 2, spidrvClockMode3 = 3 } |
SPI clock mode (clock polarity and phase).
|
|
enum |
SPIDRV_CsControl
{
spidrvCsControlAuto = 0, spidrvCsControlApplication = 1 } |
SPI master chip select (CS) control scheme.
|
|
enum |
SPIDRV_SlaveStart
{
spidrvSlaveStartImmediate = 0, spidrvSlaveStartDelayed = 1 } |
SPI slave transfer start scheme.
|
|
enum |
SPIDRV_Type
{
spidrvMaster = 0, spidrvSlave = 1 } |
SPI driver instance type.
|
|
Functions |
|
Ecode_t | SPIDRV_AbortTransfer ( SPIDRV_Handle_t handle) |
Abort an ongoing SPI transfer.
|
|
Ecode_t | SPIDRV_DeInit ( SPIDRV_Handle_t handle) |
Deinitialize an SPI driver instance.
|
|
Ecode_t | SPIDRV_GetBitrate ( SPIDRV_Handle_t handle, uint32_t *bitRate) |
Get current SPI bus bitrate.
|
|
Ecode_t | SPIDRV_GetFramelength ( SPIDRV_Handle_t handle, uint32_t *frameLength) |
Get current SPI framelength.
|
|
Ecode_t | SPIDRV_GetTransferStatus ( SPIDRV_Handle_t handle, int *itemsTransferred, int *itemsRemaining) |
Get the status of an SPI transfer.
|
|
Ecode_t | SPIDRV_Init ( SPIDRV_Handle_t handle, SPIDRV_Init_t *initData) |
Initialize an SPI driver instance.
|
|
Ecode_t | SPIDRV_MReceive ( SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback) |
Start an SPI master receive transfer.
|
|
Ecode_t | SPIDRV_MReceiveB ( SPIDRV_Handle_t handle, void *buffer, int count) |
Start an SPI master blocking receive transfer.
|
|
Ecode_t | SPIDRV_MTransfer ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, SPIDRV_Callback_t callback) |
Start an SPI master transfer.
|
|
Ecode_t | SPIDRV_MTransferB ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count) |
Start an SPI master blocking transfer.
|
|
Ecode_t | SPIDRV_MTransferSingleItemB ( SPIDRV_Handle_t handle, uint32_t txValue, void *rxValue) |
Start an SPI master blocking single item (frame) transfer.
|
|
Ecode_t | SPIDRV_MTransmit ( SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback) |
Start an SPI master transmit transfer.
|
|
Ecode_t | SPIDRV_MTransmitB ( SPIDRV_Handle_t handle, const void *buffer, int count) |
Start an SPI master blocking transmit transfer.
|
|
Ecode_t | SPIDRV_SetBitrate ( SPIDRV_Handle_t handle, uint32_t bitRate) |
Set SPI bus bitrate.
|
|
Ecode_t | SPIDRV_SetFramelength ( SPIDRV_Handle_t handle, uint32_t frameLength) |
Set SPI framelength.
|
|
Ecode_t | SPIDRV_SReceive ( SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) |
Start an SPI slave receive transfer.
|
|
Ecode_t | SPIDRV_SReceiveB ( SPIDRV_Handle_t handle, void *buffer, int count, int timeoutMs) |
Start an SPI slave blocking receive transfer.
|
|
Ecode_t | SPIDRV_STransfer ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, SPIDRV_Callback_t callback, int timeoutMs) |
Start an SPI slave transfer.
|
|
Ecode_t | SPIDRV_STransferB ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, int timeoutMs) |
Start an SPI slave blocking transfer.
|
|
Ecode_t | SPIDRV_STransmit ( SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) |
Start an SPI slave transmit transfer.
|
|
Ecode_t | SPIDRV_STransmitB ( SPIDRV_Handle_t handle, const void *buffer, int count, int timeoutMs) |
Start an SPI slave blocking transmit transfer.
|
|