VDAC_OPA_TypeDef Struct ReferenceDevicesDevices > | VDAC

VDAC_OPA VDAC OPA Register

.

Definition at line 47 of file efr32mg12p_vdac_opa.h.

#include <efr32mg12p_vdac_opa.h>

Data Fields

__IM uint32_t APORTCONFLICT
 
__IM uint32_t APORTREQ
 
__IOM uint32_t CAL
 
__IOM uint32_t CTRL
 
__IOM uint32_t MUX
 
__IOM uint32_t OUT
 
uint32_t RESERVED0 [1]
 
__IOM uint32_t TIMER
 

Field Documentation

__IM uint32_t VDAC_OPA_TypeDef::APORTCONFLICT

Operational Amplifier APORT Conflict Status Register

Definition at line 49 of file efr32mg12p_vdac_opa.h.

__IM uint32_t VDAC_OPA_TypeDef::APORTREQ

Operational Amplifier APORT Request Status Register

Definition at line 48 of file efr32mg12p_vdac_opa.h.

__IOM uint32_t VDAC_OPA_TypeDef::CAL

Operational Amplifier Calibration Register

Definition at line 54 of file efr32mg12p_vdac_opa.h.

__IOM uint32_t VDAC_OPA_TypeDef::CTRL

Operational Amplifier Control Register

Definition at line 50 of file efr32mg12p_vdac_opa.h.

__IOM uint32_t VDAC_OPA_TypeDef::MUX

Operational Amplifier Mux Configuration Register

Definition at line 52 of file efr32mg12p_vdac_opa.h.

__IOM uint32_t VDAC_OPA_TypeDef::OUT

Operational Amplifier Output Configuration Register

Definition at line 53 of file efr32mg12p_vdac_opa.h.

uint32_t VDAC_OPA_TypeDef::RESERVED0[1]

Reserved future

Definition at line 55 of file efr32mg12p_vdac_opa.h.

__IOM uint32_t VDAC_OPA_TypeDef::TIMER

Operational Amplifier Timer Control Register

Definition at line 51 of file efr32mg12p_vdac_opa.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/efr32mg12p_vdac_opa.h