LESENSE_CH_TypeDef Struct ReferenceDevicesDevices > | LESENSE

LESENSE_CH LESENSE CH Register


      

.

Definition at line 47 of file efr32mg12p_lesense_ch.h .

#include < efr32mg12p_lesense_ch.h >

Data Fields

__IOM uint32_t EVAL
__IOM uint32_t INTERACT
uint32_t RESERVED0 [1]
__IOM uint32_t TIMING

Field Documentation

__IOM uint32_t LESENSE_CH_TypeDef::EVAL

Scan Configuration

Definition at line 50 of file efr32mg12p_lesense_ch.h .

Referenced by LESENSE_ChannelSlidingWindow() , and LESENSE_ChannelStepDetection() .

__IOM uint32_t LESENSE_CH_TypeDef::INTERACT

Scan Configuration

Definition at line 49 of file efr32mg12p_lesense_ch.h .

uint32_t LESENSE_CH_TypeDef::RESERVED0[1]

Reserved future

Definition at line 51 of file efr32mg12p_lesense_ch.h .

__IOM uint32_t LESENSE_CH_TypeDef::TIMING

Scan Configuration

Definition at line 48 of file efr32mg12p_lesense_ch.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/ efr32mg12p_lesense_ch.h