TIMER_CC_TypeDef Struct ReferenceDevicesDevices > | TIMER
TIMER_CC TIMER CC Register
.
Definition at line 47
of file efr32mg12p_timer_cc.h
.
#include <
efr32mg12p_timer_cc.h
>
Data Fields | |
__IOM uint32_t | CCV |
__IOM uint32_t | CCVB |
__IM uint32_t | CCVP |
__IOM uint32_t | CTRL |
Field Documentation
__IOM uint32_t TIMER_CC_TypeDef::CCV |
CC Channel Value Register
Definition at line 49
of file efr32mg12p_timer_cc.h
.
Referenced by TIMER_CaptureGet(), TIMER_CompareSet(), and TIMER_Reset().
__IOM uint32_t TIMER_CC_TypeDef::CCVB |
CC Channel Buffer Register
Definition at line 51
of file efr32mg12p_timer_cc.h
.
Referenced by TIMER_CompareBufSet(), and TIMER_Reset().
__IM uint32_t TIMER_CC_TypeDef::CCVP |
CC Channel Value Peek Register
Definition at line 50
of file efr32mg12p_timer_cc.h
.
__IOM uint32_t TIMER_CC_TypeDef::CTRL |
CC Channel Control Register
Definition at line 48
of file efr32mg12p_timer_cc.h
.
Referenced by TIMER_InitCC(), and TIMER_Reset().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/
efr32mg12p_timer_cc.h