PRS_TypeDef Struct ReferenceDevices > PRS
PRS Register Declaration
Definition at line 49
of file efr32mg12p_prs.h
.
#include <
efr32mg12p_prs.h
>
Data Fields | |
PRS_CH_TypeDef | CH [12] |
__IOM uint32_t | CTRL |
__IOM uint32_t | DMAREQ0 |
__IOM uint32_t | DMAREQ1 |
__IM uint32_t | PEEK |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [5] |
uint32_t | RESERVED2 [1] |
uint32_t | RESERVED3 [3] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTELOC1 |
__IOM uint32_t | ROUTELOC2 |
__IOM uint32_t | ROUTEPEN |
__IOM uint32_t | SWLEVEL |
__IOM uint32_t | SWPULSE |
Field Documentation
PRS_CH_TypeDef PRS_TypeDef::CH[12] |
Channel registers
Definition at line 66
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::CTRL |
Control Register
Definition at line 59
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::DMAREQ0 |
DMA Request 0 Register
Definition at line 60
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::DMAREQ1 |
DMA Request 1 Register
Definition at line 61
of file efr32mg12p_prs.h
.
__IM uint32_t PRS_TypeDef::PEEK |
PRS Channel Values
Definition at line 63
of file efr32mg12p_prs.h
.
uint32_t PRS_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 53
of file efr32mg12p_prs.h
.
uint32_t PRS_TypeDef::RESERVED1[5] |
Reserved for future use
Definition at line 58
of file efr32mg12p_prs.h
.
uint32_t PRS_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 62
of file efr32mg12p_prs.h
.
uint32_t PRS_TypeDef::RESERVED3[3] |
Reserved registers
Definition at line 65
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 54
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTELOC1 |
I/O Routing Location Register
Definition at line 55
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTELOC2 |
I/O Routing Location Register
Definition at line 56
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line 52
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::SWLEVEL |
Software Level Register
Definition at line 51
of file efr32mg12p_prs.h
.
__IOM uint32_t PRS_TypeDef::SWPULSE |
Software Pulse Register
Definition at line 50
of file efr32mg12p_prs.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/
efr32mg12p_prs.h