CRYOTIMER_TypeDef Struct ReferenceDevices > CRYOTIMER

CRYOTIMER Register Declaration

Definition at line 49 of file efr32mg12p_cryotimer.h .

#include < efr32mg12p_cryotimer.h >

Data Fields

__IM uint32_t CNT
__IOM uint32_t CTRL
__IOM uint32_t EM4WUEN
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t PERIODSEL

Field Documentation

__IM uint32_t CRYOTIMER_TypeDef::CNT

Counter Value

Definition at line 52 of file efr32mg12p_cryotimer.h .

__IOM uint32_t CRYOTIMER_TypeDef::CTRL

Control Register

Definition at line 50 of file efr32mg12p_cryotimer.h .

__IOM uint32_t CRYOTIMER_TypeDef::EM4WUEN

Wake Up Enable

Definition at line 53 of file efr32mg12p_cryotimer.h .

__IOM uint32_t CRYOTIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 57 of file efr32mg12p_cryotimer.h .

__IM uint32_t CRYOTIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 54 of file efr32mg12p_cryotimer.h .

__IOM uint32_t CRYOTIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 56 of file efr32mg12p_cryotimer.h .

__IOM uint32_t CRYOTIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 55 of file efr32mg12p_cryotimer.h .

__IOM uint32_t CRYOTIMER_TypeDef::PERIODSEL

Interrupt Duration

Definition at line 51 of file efr32mg12p_cryotimer.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/ efr32mg12p_cryotimer.h