__GLIB_Font_t Struct ReferencePlatform Middleware > GLIB
Font definition structure.
Definition at line
219
of file
glib.h
.
#include <
glib.h
>
Data Fields |
|
uint8_t | charSpacing |
GLIB_Font_Class | class |
uint16_t | cntOfMapElements |
uint8_t | fontHeight |
uint8_t | fontRowOffset |
uint8_t | fontWidth |
uint8_t | lineSpacing |
void * | pFontPixMap |
uint8_t | sizeOfMapElement |
Field Documentation
uint8_t __GLIB_Font_t::charSpacing |
Number of pixels between each character in this font.
Definition at line
242
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
GLIB_Font_Class __GLIB_Font_t::class |
The font class is used to tell glib if the font contains numbers only or characters and numbers
Definition at line
246
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
uint16_t __GLIB_Font_t::cntOfMapElements |
Number of elements in the font pixel map.
Definition at line
224
of file
glib.h
.
Referenced by GLIB_drawChar() .
uint8_t __GLIB_Font_t::fontHeight |
Height in pixels of each character.
Definition at line
236
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
uint8_t __GLIB_Font_t::fontRowOffset |
uint8_t __GLIB_Font_t::fontWidth |
Width in pixels of each character.
Definition at line
233
of file
glib.h
.
Referenced by GLIB_drawChar() , and GLIB_drawString() .
uint8_t __GLIB_Font_t::lineSpacing |
Number of pixels between each line in this font.
Definition at line
239
of file
glib.h
.
Referenced by GLIB_drawString() .
void* __GLIB_Font_t::pFontPixMap |
Pointer to the pixel map for the font.
Definition at line
221
of file
glib.h
.
Referenced by GLIB_drawChar() .
uint8_t __GLIB_Font_t::sizeOfMapElement |
Size of each element in the font pixel map.
Definition at line
227
of file
glib.h
.
Referenced by GLIB_drawChar() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/middleware/glib/glib/
glib.h