ACMP_TypeDef Struct ReferenceDevices > ACMP
ACMP Register Declaration
Definition at line 49
of file efr32mg12p_acmp.h
.
#include <
efr32mg12p_acmp.h
>
Data Fields | |
__IM uint32_t | APORTCONFLICT |
__IM uint32_t | APORTREQ |
__IOM uint32_t | CTRL |
__IOM uint32_t | EXTIFCTRL |
__IOM uint32_t | HYSTERESIS0 |
__IOM uint32_t | HYSTERESIS1 |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INPUTSEL |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [4] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTEPEN |
__IM uint32_t | STATUS |
Field Documentation
__IM uint32_t ACMP_TypeDef::APORTCONFLICT |
APORT Conflict Status Register
Definition at line 59
of file efr32mg12p_acmp.h
.
__IM uint32_t ACMP_TypeDef::APORTREQ |
APORT Request Status Register
Definition at line 58
of file efr32mg12p_acmp.h
.
__IOM uint32_t ACMP_TypeDef::CTRL |
Control Register
Definition at line 50
of file efr32mg12p_acmp.h
.
Referenced by ACMP_CapsenseInit(), ACMP_Disable(), ACMP_Enable(), ACMP_GPIOSetup(), ACMP_Init(), and ACMP_Reset().
__IOM uint32_t ACMP_TypeDef::EXTIFCTRL |
External Override Interface Control
Definition at line 66
of file efr32mg12p_acmp.h
.
Referenced by ACMP_ExternalInputSelect().
__IOM uint32_t ACMP_TypeDef::HYSTERESIS0 |
Hysteresis 0 Register
Definition at line 60
of file efr32mg12p_acmp.h
.
Referenced by ACMP_CapsenseInit(), ACMP_Reset(), ACMP_VASetup(), and ACMP_VBSetup().
__IOM uint32_t ACMP_TypeDef::HYSTERESIS1 |
Hysteresis 1 Register
Definition at line 61
of file efr32mg12p_acmp.h
.
Referenced by ACMP_CapsenseInit(), ACMP_Reset(), ACMP_VASetup(), and ACMP_VBSetup().
__IOM uint32_t ACMP_TypeDef::IEN |
Interrupt Enable Register
Definition at line 56
of file efr32mg12p_acmp.h
.
Referenced by ACMP_IntDisable(), ACMP_IntEnable(), ACMP_IntGetEnabled(), and ACMP_Reset().
__IM uint32_t ACMP_TypeDef::IF |
Interrupt Flag Register
Definition at line 53
of file efr32mg12p_acmp.h
.
Referenced by ACMP_IntGet(), and ACMP_IntGetEnabled().
__IOM uint32_t ACMP_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 55
of file efr32mg12p_acmp.h
.
Referenced by ACMP_IntClear(), and ACMP_Reset().
__IOM uint32_t ACMP_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 54
of file efr32mg12p_acmp.h
.
Referenced by ACMP_IntSet().
__IOM uint32_t ACMP_TypeDef::INPUTSEL |
Input Selection Register
Definition at line 51
of file efr32mg12p_acmp.h
.
Referenced by ACMP_CapsenseChannelSet(), ACMP_CapsenseInit(), ACMP_ChannelSet(), ACMP_Init(), ACMP_Reset(), ACMP_VASetup(), and ACMP_VBSetup().
uint32_t ACMP_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 57
of file efr32mg12p_acmp.h
.
uint32_t ACMP_TypeDef::RESERVED1[4] |
Reserved for future use
Definition at line 63
of file efr32mg12p_acmp.h
.
__IOM uint32_t ACMP_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 65
of file efr32mg12p_acmp.h
.
Referenced by ACMP_GPIOSetup().
__IOM uint32_t ACMP_TypeDef::ROUTEPEN |
I/O Routing Pine Enable Register
Definition at line 64
of file efr32mg12p_acmp.h
.
Referenced by ACMP_GPIOSetup().
__IM uint32_t ACMP_TypeDef::STATUS |
Status Register
Definition at line 52
of file efr32mg12p_acmp.h
.
Referenced by ACMP_ExternalInputSelect().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG12P/Include/
efr32mg12p_acmp.h