retargetserial.c File Reference

Provide stdio retargeting to USART/UART or LEUART.

Version
5.6.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file retargetserial.c.

#include <stdio.h>
#include "em_device.h"
#include "em_cmu.h"
#include "em_core.h"
#include "em_gpio.h"
#include "retargetserial.h"
#include "retargetserialconfig.h"

Macros

#define _GENERIC_UART_STATUS_IDLE   LEUART_STATUS_TXC
 
#define RXBUFSIZE   8
 

Functions

static void disableRxInterrupt ()
 Disable RX interrupt.
 
static void enableRxInterrupt ()
 Enable RX interrupt.
 
void RETARGET_IRQ_NAME (void)
 UART/LEUART IRQ Handler.
 
int RETARGET_ReadChar (void)
 Receive a byte from USART/LEUART and put into global buffer.
 
void RETARGET_SerialCrLf (int on)
 UART/LEUART toggle LF to CRLF conversion.
 
bool RETARGET_SerialEnableFlowControl (void)
 Enable hardware flow control. (RTS + CTS)
 
void RETARGET_SerialFlush (void)
 Flush UART/LEUART.
 
void RETARGET_SerialInit (void)
 Intializes UART/LEUART.
 
int RETARGET_WriteChar (char c)
 Transmit single byte to USART/LEUART.
 

Variables

static bool initialized = false
 
static uint8_t LFtoCRLF = 0
 
static volatile uint8_t rxBuffer [RXBUFSIZE]
 
static volatile int rxCount = 0
 
static volatile int rxReadIndex = 0
 
static volatile int rxWriteIndex = 0