RTC_Init_TypeDef Struct ReferenceEMLIB > RTC

RTC initialization structure.

Definition at line 60 of file em_rtc.h .

#include < em_rtc.h >

Data Fields

bool comp0Top
bool debugRun
bool enable

Field Documentation

bool RTC_Init_TypeDef::comp0Top

Use compare register 0 as max count value.

Definition at line 63 of file em_rtc.h .

Referenced by RTC_Init() , and UDELAY_Calibrate() .

bool RTC_Init_TypeDef::debugRun

Counter shall keep running during debug halt.

Definition at line 62 of file em_rtc.h .

Referenced by RTC_Init() .

bool RTC_Init_TypeDef::enable

Start counting when initialization is completed.

Definition at line 61 of file em_rtc.h .

Referenced by RTC_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_rtc.h