USB_ConfigurationDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB Configuration Descriptor.
Definition at line
424
of file
em_usb.h
.
#include <
em_usb.h
>
Data Fields |
|
uint8_t | bConfigurationValue |
uint8_t | bDescriptorType |
uint8_t | bLength |
uint8_t | bmAttributes |
uint8_t | bMaxPower |
uint8_t | bNumInterfaces |
uint8_t | iConfiguration |
uint16_t | wTotalLength |
Field Documentation
uint8_t USB_ConfigurationDescriptor_TypeDef::bConfigurationValue |
Value to use as an argument to the SetConfiguration request to select this configuration.
Definition at line
434
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint8_t USB_ConfigurationDescriptor_TypeDef::bDescriptorType |
Constant CONFIGURATION Descriptor Type
Definition at line
426
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint8_t USB_ConfigurationDescriptor_TypeDef::bLength |
Size of this descriptor in bytes
Definition at line
425
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint8_t USB_ConfigurationDescriptor_TypeDef::bmAttributes |
Configuration characteristics.
D7: Reserved (set to one)
D6: Self-powered
D5: Remote Wakeup
D4...0: Reserved (reset to zero)
Definition at line
439
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint8_t USB_ConfigurationDescriptor_TypeDef::bMaxPower |
Maximum power consumption of the USB device, unit is 2mA per LSB
Definition at line
444
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint8_t USB_ConfigurationDescriptor_TypeDef::bNumInterfaces |
Number of interfaces supported by this configuration
Definition at line
432
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint8_t USB_ConfigurationDescriptor_TypeDef::iConfiguration |
Index of string descriptor describing this configuration.
Definition at line
437
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() .
uint16_t USB_ConfigurationDescriptor_TypeDef::wTotalLength |
Total length of data returned for this configuration. Includes the combined length of all descriptors (configuration, interface, endpoint, and class- or vendor-specific) returned for this configuration.
Definition at line
427
of file
em_usb.h
.
Referenced by USBH_PrintConfigurationDescriptor() , and USBH_QueryDeviceB() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
em_usb.h