BURTC_TypeDef Struct ReferenceDevices > EFM32WG_BURTC
Definition at line
48
of file
efm32wg_burtc.h
.
Data Fields |
|
| __IOM uint32_t | CMD |
| __IM uint32_t | CNT |
| __IOM uint32_t | COMP0 |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | FREEZE |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | LFXOFDET |
| __IOM uint32_t | LOCK |
| __IOM uint32_t | LPMODE |
| __IOM uint32_t | POWERDOWN |
| uint32_t | RESERVED0 [48U] |
| BURTC_RET_TypeDef | RET [128U] |
| __IM uint32_t | STATUS |
| __IM uint32_t | SYNCBUSY |
| __IM uint32_t | TIMESTAMP |
Field Documentation
| __IOM uint32_t BURTC_TypeDef::CMD |
Command Register
Definition at line
56
of file
efm32wg_burtc.h
.
| __IM uint32_t BURTC_TypeDef::CNT |
Counter Value Register
Definition at line
51
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::COMP0 |
Counter Compare Value
Definition at line
52
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::CTRL |
Control Register
Definition at line
49
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::FREEZE |
Freeze Register
Definition at line
64
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::IEN |
Interrupt Enable Register
Definition at line
62
of file
efm32wg_burtc.h
.
| __IM uint32_t BURTC_TypeDef::IF |
Interrupt Flag Register
Definition at line
59
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
61
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
60
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::LFXOFDET |
LFXO
Definition at line
54
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::LOCK |
Configuration Lock Register
Definition at line
58
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::LPMODE |
Low power mode configuration
Definition at line
50
of file
efm32wg_burtc.h
.
| __IOM uint32_t BURTC_TypeDef::POWERDOWN |
Retention RAM power-down Register
Definition at line
57
of file
efm32wg_burtc.h
.
| uint32_t BURTC_TypeDef::RESERVED0[48U] |
Reserved registers
Definition at line
67
of file
efm32wg_burtc.h
.
| BURTC_RET_TypeDef BURTC_TypeDef::RET[128U] |
RetentionReg
Definition at line
68
of file
efm32wg_burtc.h
.
| __IM uint32_t BURTC_TypeDef::STATUS |
Status Register
Definition at line
55
of file
efm32wg_burtc.h
.
| __IM uint32_t BURTC_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line
65
of file
efm32wg_burtc.h
.
| __IM uint32_t BURTC_TypeDef::TIMESTAMP |
Backup mode timestamp
Definition at line
53
of file
efm32wg_burtc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/
efm32wg_burtc.h