EBI_Init_TypeDef Struct ReferenceEMLIB > EBI
EBI Initialization structure.
Definition at line 417
of file em_ebi.h
.
#include <
em_ebi.h
>
Data Fields | |
bool | addrHalfALE |
uint32_t | addrHoldCycles |
uint32_t | addrSetupCycles |
EBI_AHigh_TypeDef | aHigh |
EBI_Polarity_TypeDef | alePolarity |
EBI_ALow_TypeDef | aLow |
bool | ardyDisableTimeout |
bool | ardyEnable |
EBI_Polarity_TypeDef | ardyPolarity |
uint32_t | banks |
bool | blEnable |
EBI_Polarity_TypeDef | blPolarity |
uint32_t | csLines |
EBI_Polarity_TypeDef | csPolarity |
bool | enable |
EBI_Location_TypeDef | location |
EBI_Mode_TypeDef | mode |
bool | noIdle |
bool | readHalfRE |
uint32_t | readHoldCycles |
bool | readPageMode |
bool | readPrefetch |
uint32_t | readSetupCycles |
uint32_t | readStrobeCycles |
EBI_Polarity_TypeDef | rePolarity |
EBI_Polarity_TypeDef | wePolarity |
bool | writeBufferDisable |
bool | writeHalfWE |
uint32_t | writeHoldCycles |
uint32_t | writeSetupCycles |
uint32_t | writeStrobeCycles |
Field Documentation
bool EBI_Init_TypeDef::addrHalfALE |
Enable or disables half cycle duration of the ALE strobe in the last address setup cycle.
Definition at line 452
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::addrHoldCycles |
Number of cycles address is driven onto the ADDRDAT bus before ALE is asserted.
Definition at line 449
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::addrSetupCycles |
Number of cycles address is held after Address Latch Enable is asserted.
Definition at line 447
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_AHigh_TypeDef EBI_Init_TypeDef::aHigh |
High address pin limit to enable.
Definition at line 482
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Polarity_TypeDef EBI_Init_TypeDef::alePolarity |
Address Latch Enable pin polarity, active high or low.
Definition at line 423
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_ALow_TypeDef EBI_Init_TypeDef::aLow |
Lower address pin limit to enable.
Definition at line 480
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::ardyDisableTimeout |
Set to turn off 32 cycle timeout ability.
Definition at line 441
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::ardyEnable |
Flag to enable or disable Address Ready support.
Definition at line 439
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Polarity_TypeDef EBI_Init_TypeDef::ardyPolarity |
Address Ready pin polarity, active high or low.
Definition at line 421
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::banks |
Mask of flags which selects address banks to configure EBI_BANK<0-3>.
Definition at line 443
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::blEnable |
Flag to enable or disable Byte Lane support.
Definition at line 434
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Polarity_TypeDef EBI_Init_TypeDef::blPolarity |
Byte Lane pin polarity, active high or low.
Definition at line 432
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::csLines |
Mask of flags which selects chip select lines to configure EBI_CS<0-3>.
Definition at line 445
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Polarity_TypeDef EBI_Init_TypeDef::csPolarity |
Chip Select pin polarity, active high or low.
Definition at line 429
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::enable |
Flag, if EBI should be enabled after configuration.
Definition at line 489
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Location_TypeDef EBI_Init_TypeDef::location |
EBI_Mode_TypeDef EBI_Init_TypeDef::mode |
EBI operation mode, data, and address limits.
Definition at line 419
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::noIdle |
Flag to enable or disable idle state insertion between transfers.
Definition at line 436
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::readHalfRE |
Enabled or disables half cycle duration of the REn signal in the last strobe cycle.
Definition at line 466
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::readHoldCycles |
Number of cycles CSn is held active after REn is deasserted.
Definition at line 459
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::readPageMode |
Enable or disable page mode reads.
Definition at line 462
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::readPrefetch |
Enables or disable prefetching from sequential addresses.
Definition at line 464
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::readSetupCycles |
Number of cycles for address setup before REn is asserted.
Definition at line 455
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::readStrobeCycles |
Number of cycles REn is held active
Definition at line 457
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Polarity_TypeDef EBI_Init_TypeDef::rePolarity |
Read Enable pin polarity, active high or low.
Definition at line 427
of file em_ebi.h
.
Referenced by EBI_Init().
EBI_Polarity_TypeDef EBI_Init_TypeDef::wePolarity |
Write Enable pin polarity, active high or low.
Definition at line 425
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::writeBufferDisable |
Enable or disable the write buffer
Definition at line 476
of file em_ebi.h
.
Referenced by EBI_Init().
bool EBI_Init_TypeDef::writeHalfWE |
Enables or disables half cycle duration of the WEn signal in the last strobe cycle.
Definition at line 478
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::writeHoldCycles |
Number of cycles CSn is held active after WEn is deasserted.
Definition at line 473
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::writeSetupCycles |
Number of cycles for address setup before WEn is asserted.
Definition at line 469
of file em_ebi.h
.
Referenced by EBI_Init().
uint32_t EBI_Init_TypeDef::writeStrobeCycles |
Number of cycles WEn is held active
Definition at line 471
of file em_ebi.h
.
Referenced by EBI_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_ebi.h