ACMP_TypeDef Struct ReferenceDevices > EFM32WG_ACMP

Definition at line 48 of file efm32wg_acmp.h .

Data Fields

__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t INPUTSEL
__IOM uint32_t ROUTE
__IM uint32_t STATUS

Field Documentation

__IOM uint32_t ACMP_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32wg_acmp.h .

Referenced by ACMP_CapsenseInit() , ACMP_Disable() , ACMP_Enable() , ACMP_GPIOSetup() , ACMP_Init() , and ACMP_Reset() .

__IOM uint32_t ACMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 52 of file efm32wg_acmp.h .

Referenced by ACMP_IntDisable() , ACMP_IntEnable() , ACMP_IntGetEnabled() , and ACMP_Reset() .

__IM uint32_t ACMP_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efm32wg_acmp.h .

Referenced by ACMP_IntGet() , and ACMP_IntGetEnabled() .

__IOM uint32_t ACMP_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efm32wg_acmp.h .

Referenced by ACMP_IntClear() , and ACMP_Reset() .

__IOM uint32_t ACMP_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efm32wg_acmp.h .

Referenced by ACMP_IntSet() .

__IOM uint32_t ACMP_TypeDef::INPUTSEL

Input Selection Register

Definition at line 50 of file efm32wg_acmp.h .

Referenced by ACMP_CapsenseChannelSet() , ACMP_CapsenseInit() , ACMP_ChannelSet() , ACMP_Init() , and ACMP_Reset() .

__IOM uint32_t ACMP_TypeDef::ROUTE

I/O Routing Register

Definition at line 56 of file efm32wg_acmp.h .

Referenced by ACMP_GPIOSetup() .

__IM uint32_t ACMP_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32wg_acmp.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/ efm32wg_acmp.h