ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP

ACMP initialization structure.

Definition at line 770 of file em_acmp.h .

#include < em_acmp.h >

Data Fields

uint32_t biasProg
bool enable
bool fullBias
bool halfBias
ACMP_HysteresisLevel_TypeDef hysteresisLevel
bool inactiveValue
bool interruptOnFallingEdge
bool interruptOnRisingEdge
bool lowPowerReferenceEnabled
uint32_t vddLevel
ACMP_WarmTime_TypeDef warmTime

Field Documentation

uint32_t ACMP_Init_TypeDef::biasProg

Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.

Definition at line 785 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::enable

If true, ACMP is enabled after configuration.

Definition at line 860 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::fullBias

Full-bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 774 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::halfBias

Half-bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 780 of file em_acmp.h .

Referenced by ACMP_Init() .

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel

Hysteresis level.

Definition at line 825 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::inactiveValue

Inactive value emitted by ACMP during warmup.

Definition at line 841 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::interruptOnFallingEdge

Enable setting the interrupt flag on the falling edge.

Definition at line 789 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::interruptOnRisingEdge

Enable setting the interrupt flag on the rising edge.

Definition at line 793 of file em_acmp.h .

Referenced by ACMP_Init() .

bool ACMP_Init_TypeDef::lowPowerReferenceEnabled

Low power reference enabled. This setting, if enabled, reduces the power used by the VDD and bandgap references.

Definition at line 846 of file em_acmp.h .

Referenced by ACMP_Init() .

uint32_t ACMP_Init_TypeDef::vddLevel

VDD reference value. VDD_SCALED = VDD * VDDLEVEL * 50 mV/3.8 V. Valid values are in the 0-63 range.

Definition at line 856 of file em_acmp.h .

Referenced by ACMP_Init() .

ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime

Warmup time, which is measured in HFPERCLK cycles and should be about 10 us in wall clock time.

Definition at line 819 of file em_acmp.h .

Referenced by ACMP_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_acmp.h